This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:ad738x [30 Sep 2019 11:20] – Add HDL Design Description, Software Setup, fix HDL link Stanca-Florina Pop | resources:eval:user-guides:ad738x [18 Oct 2019 11:54] – [Overview] jonathan colao | ||
---|---|---|---|
Line 4: | Line 4: | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
Line 10: | Line 13: | ||
===== Overview ===== | ===== Overview ===== | ||
- | The [[adi> | + | The [[adi> |
bit pin compatible family of dual simultaneous sampling, high | bit pin compatible family of dual simultaneous sampling, high | ||
speed, low power, successive approximation analog-to-digital | speed, low power, successive approximation analog-to-digital | ||
converters (ADC) that operate from a 3.3 V power supply and | converters (ADC) that operate from a 3.3 V power supply and | ||
- | features throughput rates up to 4 MSPS for the [[adi> | + | features throughput rates up to 4 MSPS. The analog input type is |
- | [[adi> | + | differential |
- | differential, accept a wide common mode input voltage and are | + | [[adi> |
- | sampled and converted on the falling edge of CS. | + | sampled and converted on the falling edge of CS. The [[adi> |
The [[adi> | The [[adi> | ||
blocks to improve dynamic range and reduce noise at lower | blocks to improve dynamic range and reduce noise at lower | ||
Line 48: | Line 50: | ||
In order to build the HDL design the user has to go through the following steps: | In order to build the HDL design the user has to go through the following steps: | ||
- | - Confirm that you have the right tools (the reference design requires Vivado | + | - Confirm that you have the right tools (the reference design requires Vivado |
- Clone the HDL GitHub repository (the project is located at [[https:// | - Clone the HDL GitHub repository (the project is located at [[https:// | ||
- Build the project (see https:// | - Build the project (see https:// |