This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:ad738x [07 Feb 2019 03:40] – [Overview] jonathan colao | resources:eval:user-guides:ad738x [18 Oct 2019 11:54] – [Overview] jonathan colao | ||
---|---|---|---|
Line 4: | Line 4: | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
Line 10: | Line 13: | ||
===== Overview ===== | ===== Overview ===== | ||
- | The [[adi> | + | The [[adi> |
bit pin compatible family of dual simultaneous sampling, high | bit pin compatible family of dual simultaneous sampling, high | ||
speed, low power, successive approximation analog-to-digital | speed, low power, successive approximation analog-to-digital | ||
converters (ADC) that operate from a 3.3 V power supply and | converters (ADC) that operate from a 3.3 V power supply and | ||
- | features throughput rates up to 4 MSPS for the [[adi> | + | features throughput rates up to 4 MSPS. The analog input type is |
- | [[adi> | + | differential |
- | differential, accept a wide common mode input voltage and are | + | [[adi> |
- | sampled and converted on the falling edge of CS. | + | sampled and converted on the falling edge of CS. The [[adi> |
The [[adi> | The [[adi> | ||
blocks to improve dynamic range and reduce noise at lower | blocks to improve dynamic range and reduce noise at lower | ||
Line 32: | Line 34: | ||
operation specified from −40°C to +125°C. | operation specified from −40°C to +125°C. | ||
- | Applications: | + | ==== Applications |
* Motor control position feedback | * Motor control position feedback | ||
* Motor control current sense | * Motor control current sense | ||
Line 40: | Line 42: | ||
* SONAR | * SONAR | ||
* Power Quality | * Power Quality | ||
+ | |||
+ | ===== HDL Design Description ===== | ||
+ | |||
+ | In the [[: | ||
+ | |||
+ | The reference design uses the standard [[https:// | ||
+ | |||
+ | In order to build the HDL design the user has to go through the following steps: | ||
+ | - Confirm that you have the right tools (the reference design requires Vivado 2018.3) | ||
+ | - Clone the HDL GitHub repository (the project is located at [[https:// | ||
+ | - Build the project (see https:// | ||
+ | |||
+ | ===== Software Setup ===== | ||
+ | |||
+ | In order to perform the software setup the user has to go through the following steps: | ||
+ | - Confirm that you have the right tools (the reference design requires XSDK) | ||
+ | - Clone the No-OS GitHub repository (the project is located at [[https:// | ||
+ | - Follow the instructions provided by [[https:// | ||
===== No-OS Driver Description ===== | ===== No-OS Driver Description ===== | ||
Line 116: | Line 136: | ||
===== HDL Downloads ===== | ===== HDL Downloads ===== | ||
<WRAP round download 50%> | <WRAP round download 50%> | ||
- | * {{https:// | + | * {{https:// |
</ | </ | ||
===== No-OS Downloads ===== | ===== No-OS Downloads ===== |