This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:ad713x:hdl [11 Feb 2022 15:29] – [Overview] sergiu arpadi | resources:eval:user-guides:ad713x:hdl [11 Feb 2022 16:52] – fix bd sergiu arpadi | ||
---|---|---|---|
Line 36: | Line 36: | ||
The design only supports the slave mode for both devices with both DCLK and ODR generated by the FPGA. Each device sends data on 4 of the 8 DIN bits. | The design only supports the slave mode for both devices with both DCLK and ODR generated by the FPGA. Each device sends data on 4 of the 8 DIN bits. | ||
- | {{: | + | {{: |
In order to build the HDL design the user has to go through the following steps: | In order to build the HDL design the user has to go through the following steps: |