Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:user-guides:ad5940 [11 Sep 2019 14:45] – test Ces Pitt | resources:eval:user-guides:ad5940 [11 Sep 2019 14:49] – Micheál Lambe |
---|
The AD594x is a high precision, low power analog front end (AFE) designed for applications requiring high precision, electrochemical-based measurement techniques, such as amperometric, voltametric, or impedance measurements. It is targeted at a number of industries including Healthcare, Industrial and Instrumentation. The AD594x evaluation eco-system is designed to be a versatile development and prototyping vehicle to help customers configure and use the AD594x in their target application. | The AD594x is a high precision, low power analog front end (AFE) designed for applications requiring high precision, electrochemical-based measurement techniques, such as amperometric, voltametric, or impedance measurements. It is targeted at a number of industries including Healthcare, Industrial and Instrumentation. The AD594x evaluation eco-system is designed to be a versatile development and prototyping vehicle to help customers configure and use the AD594x in their target application. |
| |
----- | |
{{ :resources:eval:user-guides:ad5940_wiki_collage.png?nolink&500|}} | {{ :resources:eval:user-guides:ad5940_wiki_collage.png?nolink&500|}} |
| |