This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:ad5758 [04 May 2018 13:36] – Downloads Stefan Popa | resources:eval:user-guides:ad5758 [10 May 2019 14:56] – Add HDL design section Istvan Csomortani | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== AD5758 - No-OS Driver | + | ====== AD5758 - Reference Design |
===== Supported Devices ===== | ===== Supported Devices ===== | ||
* [[adi> | * [[adi> | ||
+ | |||
+ | ===== Supported FPGA carrier board ===== | ||
+ | * [[http:// | ||
===== Overview ===== | ===== Overview ===== | ||
- | The [[adi> | + | The [[adi> |
- | The device uses a versatile 4-wire serial peripheral interface (SPI) that operates at clock rates of up to 50 MHz and is compatible with standard SPI, QSPI™, MICROWIRE™, | + | The device uses a versatile 4-wire serial peripheral interface (SPI) that operates at clock rates of up to 50 MHz and is compatible with standard SPI, QSPI™, MICROWIRE™, |
Applications: | Applications: | ||
Line 14: | Line 17: | ||
* PLC and DCS applications | * PLC and DCS applications | ||
* HART network connectivity | * HART network connectivity | ||
+ | |||
+ | ===== HDL reference design ===== | ||
+ | |||
+ | The HDL project is only needed if the used carrier board is an FPGA board. The project uses a Zedboard and its hardware interfaces. There isn't any custom logic in the programmable side of the Zynq 7000 SoC. | ||
+ | To clone or download the HDL repository, go the Download section of this wiki page. | ||
+ | |||
+ | To find more information about how to create and build the project please visit the [[https:// | ||
+ | |||
+ | To find more information about how to create the application project in Xilinx SDK please visit the following page: https:// | ||
===== Driver Description ===== | ===== Driver Description ===== | ||
Line 116: | Line 128: | ||
RANGE_M5V_5V, | RANGE_M5V_5V, | ||
RANGE_M10V_10V, | RANGE_M10V_10V, | ||
- | RANGE_0mA_20mA, | + | RANGE_0mA_20mA |
RANGE_0mA_24mA, | RANGE_0mA_24mA, | ||
RANGE_4mA_24mA, | RANGE_4mA_24mA, |