This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:user-guides:ad463x:hdl [17 May 2022 16:24] – [HDL Design Description] Jim Catt | resources:eval:user-guides:ad463x:hdl [29 Jul 2022 09:56] – added AD4630-16 content Padraic O Reilly | ||
---|---|---|---|
Line 5: | Line 5: | ||
The HDL reference design for the EVAL-AD4630_FMCZ and EVAL-AD4030_FMCZ provides all the interfaces that are necessary to interact with the device using a Xilinx FPGA development board. | The HDL reference design for the EVAL-AD4630_FMCZ and EVAL-AD4030_FMCZ provides all the interfaces that are necessary to interact with the device using a Xilinx FPGA development board. | ||
- | The design has all the necessary infrastructure to acquire data from the AD4630-24 24-bit dual-channel precision SAR ADC and AD4030-24 single channel ADC, supporting continuous data capture at maximum 2 MSPS data rate. The design targeted to the Zedboard, which is a low cost FPGA carrier board from Digilent, using a Zynq-7000 re-programmable SoC from Xilinx. | + | The design has all the necessary infrastructure to acquire data from the AD4630-24 24-bit dual-channel precision SAR ADC, AD4630-16 16-bit dual channel precision SAR ADC and AD4030-24 single channel ADC, supporting continuous data capture at maximum 2 MSPS data rate. The design targeted to the Zedboard, which is a low cost FPGA carrier board from Digilent, using a Zynq-7000 re-programmable SoC from Xilinx. |
Line 11: | Line 11: | ||
* [[ADI> | * [[ADI> | ||
+ | * [[ADI> | ||
* [[ADI> | * [[ADI> | ||
==== Evaluation board ==== | ==== Evaluation board ==== | ||
* [[adi> | * [[adi> | ||
+ | * [[adi> | ||
* [[adi> | * [[adi> | ||
==== Supported FPGA carrier ==== | ==== Supported FPGA carrier ==== | ||
Line 31: | Line 33: | ||
- | There are three modes in which the system can run. Refer to the [[adi> | + | There are three modes in which the system can run. Refer to the [[adi> |
=== SPI mode - transfer zone 1 === | === SPI mode - transfer zone 1 === |