This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:ad400x [19 Aug 2019 16:32] – [Software Setup] Stanca-Florina Pop | resources:eval:user-guides:ad400x [22 Nov 2019 15:22] – Fix system_bd and HDL links Stanca-Florina Pop | ||
---|---|---|---|
Line 39: | Line 39: | ||
==== Design Configuration ==== | ==== Design Configuration ==== | ||
- | The reference design uses an integrated pulse generator to synchronise the capture events during continuous conversion. The required sampling rate can be set in [[https:// | + | The reference design uses an integrated pulse generator to synchronise the capture events during continuous conversion. The required sampling rate can be set in [[https:// |
1) Reference clock frequency for SPI interface clock | 1) Reference clock frequency for SPI interface clock | ||
Line 60: | Line 60: | ||
In order to perform the software setup the user has to go through the following steps: | In order to perform the software setup the user has to go through the following steps: | ||
- Confirm that you have the right tools (the reference design requires XSDK) | - Confirm that you have the right tools (the reference design requires XSDK) | ||
- | - Clone the HDL GitHub repository (the project is located at [[https:// | + | - Clone the No-OS GitHub repository (the project is located at [[https:// |
- Follow the instructions provided by [[https:// | - Follow the instructions provided by [[https:// | ||
Line 118: | Line 118: | ||
===== HDL Downloads ===== | ===== HDL Downloads ===== | ||
<WRAP round download 50%> | <WRAP round download 50%> | ||
- | * {{https:// | + | * {{https:// |
</ | </ | ||