This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:ad-t1lusb-ebz [08 Dec 2023 14:02] – [Setup Examples] Mihai Ionut Suciu | resources:eval:user-guides:ad-t1lusb-ebz [08 Dec 2023 14:27] (current) – Add another chapter Mihai Ionut Suciu | ||
---|---|---|---|
Line 35: | Line 35: | ||
* {{ : | * {{ : | ||
</ | </ | ||
+ | \\ | ||
+ | |||
+ | ===== Network Testing ===== | ||
+ | When the AD-T1LUSB2.0-EBZ board is connected to a computer via a USB cable, a new network interface should be available. | ||
+ | |||
+ | This can be verified by running on a shell terminal the **'' | ||
+ | |||
+ | The new network configuration which corresponds to the following example: | ||
+ | < | ||
+ | Ethernet adapter Ethernet 3: | ||
+ | |||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | </ | ||
+ | |||
+ | After this we can run the '' | ||
+ | |||
+ | < | ||
+ | Pinging 169.254.193.171 with 32 bytes of data: | ||
+ | Reply from 169.254.193.171: | ||
+ | Reply from 169.254.193.171: | ||
+ | Reply from 169.254.193.171: | ||
+ | Reply from 169.254.193.171: | ||
+ | Reply from 169.254.193.171: | ||
+ | Reply from 169.254.193.171: | ||
+ | Reply from 169.254.193.171: | ||
+ | Reply from 169.254.193.171: | ||
+ | Reply from 169.254.193.171: | ||
+ | Reply from 169.254.193.171: | ||
+ | </ | ||
+ | |||
+ | In this way, we can confirm that the connection between a computer and the AD-T1LUSB2.0-EBZ board works as expected. | ||
+ | |||
\\ | \\ | ||