This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:user-guides:ad-synchrona14-ebz:testing [19 Jul 2022 11:14] – [Required software] Ramona Alexandra Nechita | resources:eval:user-guides:ad-synchrona14-ebz:testing [13 Dec 2022 19:04] – Ciprian Carbunaru | ||
---|---|---|---|
Line 75: | Line 75: | ||
* For channels 11-14, attach the front panel cable to the Twinax to SMA adapter. Use the new probe to test.{{ : | * For channels 11-14, attach the front panel cable to the Twinax to SMA adapter. Use the new probe to test.{{ : | ||
{{ : | {{ : | ||
- | * The next step is testing the inputs, on the back panel. Use the SMA cable for back panel and attach it one at a time to REF IN, PPS, CH2 and CH3. **For CH2 and CH3 inputs you only need to connect to one of the SMA connectors, P or N.** | + | * The next step is testing the inputs, on the back panel. Use the SMA cable for back panel and attach it one at a time to REF IN, PPS, CH2 and CH3. **For CH2 and CH3 inputs you only need to connect to one of the SMA connectors, P or N. On the input (P or N) you are not connecting the SMA cable place a SMA 50 Ohm terminator. ** |
{{ : | {{ : | ||
* In order to test the UART COMM 01, 02 and the SPI Communication, | * In order to test the UART COMM 01, 02 and the SPI Communication, |