This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:ad-synchrona14-ebz:testing [13 Dec 2022 19:04] Ciprian Carbunaru |
resources:eval:user-guides:ad-synchrona14-ebz:testing [15 Dec 2022 22:13] Ciprian Carbunaru |
||
---|---|---|---|
Line 76: | Line 76: | ||
{{ :resources:eval:user-guides:ad-synchrona14-ebz:testt_5.png?|}} | {{ :resources:eval:user-guides:ad-synchrona14-ebz:testt_5.png?|}} | ||
* The next step is testing the inputs, on the back panel. Use the SMA cable for back panel and attach it one at a time to REF IN, PPS, CH2 and CH3. **For CH2 and CH3 inputs you only need to connect to one of the SMA connectors, P or N. On the input (P or N) you are not connecting the SMA cable place a SMA 50 Ohm terminator. ** | * The next step is testing the inputs, on the back panel. Use the SMA cable for back panel and attach it one at a time to REF IN, PPS, CH2 and CH3. **For CH2 and CH3 inputs you only need to connect to one of the SMA connectors, P or N. On the input (P or N) you are not connecting the SMA cable place a SMA 50 Ohm terminator. ** | ||
+ | * | ||
+ | {{ :resources:eval:user-guides:ad-synchrona14-ebz:50ohm.jpg?300 |}} | ||
{{ :resources:eval:user-guides:ad-synchrona14-ebz:backpanel.jpg?|}} | {{ :resources:eval:user-guides:ad-synchrona14-ebz:backpanel.jpg?|}} | ||
+ | |||
+ | |||
+ | |||
* In order to test the UART COMM 01, 02 and the SPI Communication, attach a BR-068851 to the GPIO port on the back panel. | * In order to test the UART COMM 01, 02 and the SPI Communication, attach a BR-068851 to the GPIO port on the back panel. | ||
{{ :resources:eval:user-guides:ad-synchrona14-ebz:gpio.jpg?|}} | {{ :resources:eval:user-guides:ad-synchrona14-ebz:gpio.jpg?|}} |