Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:ad-pzsdr2400tdd-eb [06 Feb 2016 16:29] – [Table of Contents] Neil Wilson | resources:eval:user-guides:ad-pzsdr2400tdd-eb [14 Jan 2021 05:11] (current) – user interwiki links Robin Getz |
---|
====== AD-PZSDR2400TDD-EB User Guide ====== | ====== AD-PZSDR2400TDD-EB User Guide ====== |
| |
The [[adi>AD-PZSDR2400TDD-EB]] is affectionately dubbed the first 'RF personality card'. It plugs into the Avnet [[http://zedboard.org/product/picozed-sdr-som-development-kit|AES-PZSDRCC-FMC-G]] carrier card. 35mm U.FL coaxial cables connect the card to the Avnet [[http://zedboard.org/product/picozed-sdr-som|PicoZed SDR Z7035/AD9361 SOM]] providing access to the transmit and receive inputs of the [[adi>AD9361]]. Information on the card, how to use it, the design package that surrounds it, and the software which can make it work, can be found here. | The [[adi>AD-PZSDR2400TDD-EB]] is affectionately dubbed the first 'RF personality card'. It plugs into the ADRV1CRR-FMC [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/ADRV1CRR-FMC.html]] carrier card. 35mm U.FL coaxial cables connect the card to the ADRV9361-Z7035 [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/ADRV9361-Z7035.html#eb-overview]] providing access to the transmit and receive inputs of the [[adi>AD9361]]. Information on the card, how to use it, the design package that surrounds it, and the software which can make it work, can be found here. |
| |
The purpose of the [[adi>AD-PZSDR2400TDD-EB]] is to provide the user with a tunable path to condition the transmit or receive signals of the [[adi>AD9361]]. Selection of TX or RX path is achieved by the 200MHz to 2.7GHz SPDT switch [[adi>HMC546LP2]] controlled by the FPGA and accompanying software. The transmit path consists of a 2.4GHz filter, half watt driver amplifier [[adi>ADL5324]] and 2 watt power amplifier [[adi>HMC921]]. The receive path consists of the same 2.4GHz filter as well as a low loss LNA [[adi>HMC669]]. | The purpose of the [[adi>AD-PZSDR2400TDD-EB]] is to provide the user with a tunable path to condition the transmit or receive signals of the [[adi>AD9361]]. Selection of TX or RX path is achieved by the 200MHz to 2.7GHz SPDT switch [[adi>HMC546LP2]] controlled by the FPGA and accompanying software. The transmit path consists of a 2.4GHz filter, half watt driver amplifier [[adi>ADL5324]] and 2 watt power amplifier [[adi>HMC921]]. The receive path consists of the same 2.4GHz filter as well as a low loss LNA [[adi>HMC669]]. |
- [[.:ad-pzsdr2400tdd-eb:software|Software]] | - [[.:ad-pzsdr2400tdd-eb:software|Software]] |
- [[.:ad-pzsdr2400TDD-eb:help_and_support|Help and Support]] | - [[.:ad-pzsdr2400TDD-eb:help_and_support|Help and Support]] |
| |
| {{ analogTV>4840956066001 }} |
| |
===== Warning ===== | ===== Warning ===== |
| |
{{page>wiki/common#esd_warning&nofooter&noheader}} | {{page>wiki/common#esd_warning&nofooter&noheader}} |