This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-pqmon-sl [11 Apr 2024 09:53] – [Features] Joyce Velasco | resources:eval:user-guides:ad-pqmon-sl [19 Apr 2024 03:00] (current) – replaced block diagram with updated version Joyce Velasco | ||
---|---|---|---|
Line 5: | Line 5: | ||
Power quality monitoring is becoming important to keep power grids clean despite the harmonics introduced by inverter-based resources. Such activity improves the stability and reliability of the grid and improves equipment health by preventing flickering or blackouts. | Power quality monitoring is becoming important to keep power grids clean despite the harmonics introduced by inverter-based resources. Such activity improves the stability and reliability of the grid and improves equipment health by preventing flickering or blackouts. | ||
- | The [[adi>AD-PQMON-SL]] is a power quality monitoring solution based on the [[adi> | + | The **AD-PQMON-SL** is a power quality monitoring solution based on the [[adi> |
This reference design also has an on-board processor, the [[adi> | This reference design also has an on-board processor, the [[adi> | ||
{{ : | {{ : | ||
+ | |||
+ | {{ : | ||
+ | |||
\\ | \\ | ||
Line 30: | Line 33: | ||
* Intelligent buildings | * Intelligent buildings | ||
+ | \\ | ||
===== Components ===== | ===== Components ===== | ||
==== Metering and Compute Base Board ==== | ==== Metering and Compute Base Board ==== | ||
Line 61: | Line 65: | ||
==== Requirements ==== | ==== Requirements ==== | ||
- | * 1 metering | + | * 1 metering |
* optional 1 add-on board for COMMS and HMI | * optional 1 add-on board for COMMS and HMI | ||
* current transformers (included in the kit) | * current transformers (included in the kit) | ||
Line 69: | Line 73: | ||
\\ | \\ | ||
- | ===== Software | + | ===== Application Development |
==== GUI Scopy – Cross-platform Qt Application ==== | ==== GUI Scopy – Cross-platform Qt Application ==== | ||
- | {{ : | + | {{ : |
- | {{ : | + | {{ : |
- | {{ : | + | {{ : |
\\ | \\ | ||
Line 142: | Line 146: | ||
Functions/ | Functions/ | ||
Screenshot of Sample Readings/ | Screenshot of Sample Readings/ | ||
- | |||
- | |||
</ | </ | ||
+ | |||
---- | ---- | ||
Line 152: | Line 155: | ||
* [[adi> | * [[adi> | ||
- | * [[adi> | + | * [[adi> |
- | * Application notes | + | * [[adi> |
- | * Links to other demo pages using the board | + | * [[adi> |
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | |||
+ | \\ | ||