This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fxtof1-ebz [01 Jul 2021 23:42] – [Introduction] Andrei Cozma | resources:eval:user-guides:ad-fxtof1-ebz [21 Jul 2021 10:48] – Andrei Cozma | ||
---|---|---|---|
Line 54: | Line 54: | ||
<WRAP center round important 100%> | <WRAP center round important 100%> | ||
Some of the AD-FXTOF1-EBZ kits are missing the correct 15 pins cable to connect to Raspberry Pi or the Nvidia platforms. If in your box there is only one 15 pins cable having the contacts on the same side, please get a new cable with contacts on opposite sides (e.g. [[https:// | Some of the AD-FXTOF1-EBZ kits are missing the correct 15 pins cable to connect to Raspberry Pi or the Nvidia platforms. If in your box there is only one 15 pins cable having the contacts on the same side, please get a new cable with contacts on opposite sides (e.g. [[https:// | ||
+ | |||
+ | With the Raspberry Pi or the Nvidia platforms the 15 pins cable with contacts on opposite sides must be used for correct system operation. | ||
</ | </ | ||