This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fxtof1-ebz [13 May 2021 15:44] – [Introduction] Andrei Cozma | resources:eval:user-guides:ad-fxtof1-ebz [01 Jul 2021 23:42] – [Introduction] Andrei Cozma | ||
---|---|---|---|
Line 28: | Line 28: | ||
<WRAP round download 60%> | <WRAP round download 60%> | ||
{{: | {{: | ||
- | \\ | + | {{ : |
{{: | {{: | ||
</ | </ | ||
Line 51: | Line 51: | ||
* USB cable to supply 5V to the system | * USB cable to supply 5V to the system | ||
* One page Quick Start Guide | * One page Quick Start Guide | ||
+ | |||
+ | <WRAP center round important 100%> | ||
+ | Some of the AD-FXTOF1-EBZ kits are missing the correct 15 pins cable to connect to Raspberry Pi or the Nvidia platforms. If in your box there is only one 15 pins cable having the contacts on the same side, please get a new cable with contacts on opposite sides (e.g. [[https:// | ||
+ | </ | ||
+ | |||
<WRAP round info 100%> | <WRAP round info 100%> |