This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fxtof1-ebz:ug_xavier_nx [19 Apr 2021 10:44] – Add fxtof1 demo image Septimiu Vana | resources:eval:user-guides:ad-fxtof1-ebz:ug_xavier_nx [21 Jul 2021 10:50] – [Power on sequence] Andrei Cozma | ||
---|---|---|---|
Line 24: | Line 24: | ||
* Plug the SD card into the Nvidia Xavier NX SD card slot | * Plug the SD card into the Nvidia Xavier NX SD card slot | ||
* Connect the HDMI cable from the monitor to the Jetson HDMI connector | * Connect the HDMI cable from the monitor to the Jetson HDMI connector | ||
- | * Connect the molex cable between the camera and the interposer | + | * Connect the 25 pins flex cable between the camera and the interposer |
- | * Connect the camera cable between the J1 connector of Jetson Xavier NX and the P1 connector of the interposer | + | * Connect the 15 pons camera cable between the J1 connector of Jetson Xavier NX and the P1 connector of the interposer. Make sure to use the cable with contacts on opposite sides. |
* Connect a USB mouse and keyboard to the Xavier NX | * Connect a USB mouse and keyboard to the Xavier NX | ||
* Connect the power supply to the interposer | * Connect the power supply to the interposer |