This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:ad-freqcvt1-ebz:hardware:functional_overview [05 Aug 2016 16:35] Lucian Sin [Downconversion] |
resources:eval:user-guides:ad-freqcvt1-ebz:hardware:functional_overview [08 Nov 2016 11:38] Lucian Sin [LO] add link for ADF4351 |
||
---|---|---|---|
Line 29: | Line 29: | ||
==== LO ==== | ==== LO ==== | ||
- | The LO used in on this board is the ADF4351 which is software programmable. Please refer to the device data sheet for the two LO within this board. The board provides a 25MHz crystal for the ADF4351. | + | The LO used in on this board is the [[adi>ADF4351]] which is software programmable. Please refer to the device data sheet for the two LO within this board. The board provides a 25MHz crystal for the ADF4351. |
==== SPI ==== | ==== SPI ==== |