This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-freqcvt1-ebz:hardware:functional_overview [29 Mar 2016 14:55] – [Power] Charly El-Khoury | resources:eval:user-guides:ad-freqcvt1-ebz:hardware:functional_overview [08 Nov 2016 11:38] (current) – [LO] add link for ADF4351 Lucian Sin | ||
---|---|---|---|
Line 22: | Line 22: | ||
==== Downconversion ==== | ==== Downconversion ==== | ||
- | * Input frequency 1 - 100 MHz | + | * Output |
* Reference impedance 50 ohm | * Reference impedance 50 ohm | ||
* Conversion Gain 14 dB | * Conversion Gain 14 dB | ||
Line 29: | Line 29: | ||
==== LO ==== | ==== LO ==== | ||
- | The LO used in on this board is the ADF4351 which is software programmable. Please refer to the device data sheet for the two LO within this board. The board provides a 25MHz crystal for the ADF4351. | + | The LO used in on this board is the [[adi>ADF4351]] which is software programmable. Please refer to the device data sheet for the two LO within this board. The board provides a 25MHz crystal for the ADF4351. |
==== SPI ==== | ==== SPI ==== |