This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:ad-fmcxmwbr1-ebz [08 Apr 2022 16:08] – Pop Andreea | resources:eval:user-guides:ad-fmcxmwbr1-ebz [16 Jun 2022 14:31] (current) – Pop Andreea | ||
---|---|---|---|
Line 7: | Line 7: | ||
It is powered from the FMC connector but has the option to add an external supply for applications that require higher load currents. This increases flexibility and allows for multiple supply voltages with high current capability. These can be used to bias the X-MW blocks or other IC’s in a prototype design, allowing multiple level translated digital communications paths between the controller board and the front-end. | It is powered from the FMC connector but has the option to add an external supply for applications that require higher load currents. This increases flexibility and allows for multiple supply voltages with high current capability. These can be used to bias the X-MW blocks or other IC’s in a prototype design, allowing multiple level translated digital communications paths between the controller board and the front-end. | ||
- | + | {{: | |
- | {{: | + | |
\\ | \\ | ||