Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:user-guides:ad-fmcomms4-ebz [22 Jul 2015 10:19] – Fix image link. Dragos Bogdan | resources:eval:user-guides:ad-fmcomms4-ebz [22 Jul 2015 11:52] – Fix image link. Dragos Bogdan |
---|
The AD-FMComms4-EBZ board is very similar to the [[AD-FMComms2-EBZ]] and [[AD-FMComms3-EBZ]] boards with only one exception, rather than the [[adi>AD9361]] (which is 2 Rx, 2 Tx), it uses the [[adi>AD9364]], a lower cost 1 Rx, 1 Tx device. The AD-FMComms4-EBZ includes both types of external baluns, one targeted for wider tuning range applications (Minicircuits [[http://www.minicircuits.com/pdfs/TCM1-63AX+.pdf|TCM1-63AX+]]), and ones which provide optimized performance for 2.4 GHz. | The AD-FMComms4-EBZ board is very similar to the [[AD-FMComms2-EBZ]] and [[AD-FMComms3-EBZ]] boards with only one exception, rather than the [[adi>AD9361]] (which is 2 Rx, 2 Tx), it uses the [[adi>AD9364]], a lower cost 1 Rx, 1 Tx device. The AD-FMComms4-EBZ includes both types of external baluns, one targeted for wider tuning range applications (Minicircuits [[http://www.minicircuits.com/pdfs/TCM1-63AX+.pdf|TCM1-63AX+]]), and ones which provide optimized performance for 2.4 GHz. |
| |
{{ :resources:eval:user-guides:ad-fmcomms4-ebz:fmcomms4_top.jpg?350|}} | {{ http://www.analog.com/-/media/analog/en/evaluation-board-images/images/ad-fmcomms4.ashx?.png?350}} |
| |
Since much of the FMCOMMS2/3/4 share a common device/infrastructure, much of the documentation is the same. | Since much of the FMCOMMS2/3/4 share a common device/infrastructure, much of the documentation is the same. |