Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
resources:eval:user-guides:ad-fmcomms4-ebz [22 Jul 2015 10:19] – Fix image link. Dragos Bogdan | resources:eval:user-guides:ad-fmcomms4-ebz [01 Dec 2015 04:21] – add links Robin Getz |
---|
The AD-FMComms4-EBZ board is very similar to the [[AD-FMComms2-EBZ]] and [[AD-FMComms3-EBZ]] boards with only one exception, rather than the [[adi>AD9361]] (which is 2 Rx, 2 Tx), it uses the [[adi>AD9364]], a lower cost 1 Rx, 1 Tx device. The AD-FMComms4-EBZ includes both types of external baluns, one targeted for wider tuning range applications (Minicircuits [[http://www.minicircuits.com/pdfs/TCM1-63AX+.pdf|TCM1-63AX+]]), and ones which provide optimized performance for 2.4 GHz. | The AD-FMComms4-EBZ board is very similar to the [[AD-FMComms2-EBZ]] and [[AD-FMComms3-EBZ]] boards with only one exception, rather than the [[adi>AD9361]] (which is 2 Rx, 2 Tx), it uses the [[adi>AD9364]], a lower cost 1 Rx, 1 Tx device. The AD-FMComms4-EBZ includes both types of external baluns, one targeted for wider tuning range applications (Minicircuits [[http://www.minicircuits.com/pdfs/TCM1-63AX+.pdf|TCM1-63AX+]]), and ones which provide optimized performance for 2.4 GHz. |
| |
{{ :resources:eval:user-guides:ad-fmcomms4-ebz:fmcomms4_top.jpg?350|}} | {{ http://www.analog.com/-/media/analog/en/evaluation-board-images/images/ad-fmcomms4.ashx?.png?350}} |
| |
Since much of the FMCOMMS2/3/4 share a common device/infrastructure, much of the documentation is the same. | Since much of the FMCOMMS2/3/4 share a common device/infrastructure, much of the documentation is the same. |
| |
| - [[adi>ad-fmcomms4-ebz#eb-buy|Purchase]] |
- [[.:ad-fmcomms2-ebz:introduction|Introduction]] | - [[.:ad-fmcomms2-ebz:introduction|Introduction]] |
- [[.:ad-fmcomms4-ebz:hardware|FMCOMMS4 Hardware]]: This provides a brief description of the AD-FMCOMMS4-EBZ board by itself, and is a good reference for those who want to understand a little more about the board. If you just want to use the board, you can skip this section, and come back to it when you want to incorporate the AD9361 into your product. | - [[.:ad-fmcomms4-ebz:hardware|FMCOMMS4 Hardware]]: This provides a brief description of the AD-FMCOMMS4-EBZ board by itself, and is a good reference for those who want to understand a little more about the board. If you just want to use the board, you can skip this section, and come back to it when you want to incorporate the AD9361 into your product. |
- [[.:ad-fmcomms2-ebz:hardware:card_specification|Characteristics & Performance]] | - [[.:ad-fmcomms2-ebz:hardware:card_specification|Characteristics & Performance]] |
- [[.:ad-fmcomms2-ebz:hardware:configuration_options|Configuration options]] | - [[.:ad-fmcomms2-ebz:hardware:configuration_options|Configuration options]] |
| - [[.:ad-fmcomms2-ebz:certification|FCC or CE certification]] |
| - [[.:ad-fmcomms2-ebz:hardware:tuning|Tuning the system]] |
- [[.:ad-fmcomms2-ebz:testing|Production Testing Process]] | - [[.:ad-fmcomms2-ebz:testing|Production Testing Process]] |
- Use the AD-FMCOMMS4-EBZ Board to better understand the AD9364 | - Use the AD-FMCOMMS4-EBZ Board to better understand the AD9364 |