Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:ad-fmcomms4-ebz:hardware [29 Apr 2014 21:32] – [I/O Voltage] Robin Getz | resources:eval:user-guides:ad-fmcomms4-ebz:hardware [14 Mar 2023 06:10] (current) – updated the design files download link Joyce Velasco |
---|
| |
====== AD-FMCOMMS4-EBZ Hardware ====== | ====== AD-FMCOMMS4-EBZ Hardware ====== |
| \\ |
===== Downloads ===== | ===== Schematic, PCB Layout, Bill of Materials ===== |
<WRAP round download 65%> | <WRAP round download 65%> |
<WRAP info>This is the latest and greatest Rev "B" of this board. Note that the Baluns on the Rev B board (T101-T104) are either : | <WRAP info>Note that the Baluns on the Rev C board (T101-T104) are either: |
* Johanson Technology's [[http://www.johansontechnology.com/images/stories/ip/baluns/Balun_2450BL15B050.pdf|2450BL15B050E]] 2.45 GHz Balun. This balun is rated for a operating frequency of 2400~2500 MHz. If you want to evaluate the part outside of this frequency range, an [[../ad-fmcomms2-ebz/hardware/configuration_options|alternative balun]] should be installed. The test results were taken using the Johanson Technology's 2450BL15B050E balun. | * Johanson Technology's [[http://www.johansontechnology.com/datasheets/baluns/JTI_Balun-2450BL15B050_12-03.pdf|2450BL15B050E]] 2.45 GHz Balun. This balun is rated for a operating frequency of 2400~2500 MHz and is connected to RXB Input and TXB Output. If you want to evaluate the part outside of this frequency range, use the other SMA. |
* Mini Circuits [[http://www.minicircuits.com/pdfs/TCM1-63AX+.pdf|TCM1-63AX+]]. They are rated for a operating frequency between 10 MHz and 6 GHz. | * Mini Circuits [[http://www.minicircuits.com/pdfs/TCM1-63AX+.pdf|TCM1-63AX+]]. They are rated for an operating frequency between 70 MHz and 6 GHz, and are connected to the RXA Input and TXB Output. |
</WRAP> | </WRAP> |
* {{:resources:eval:user-guides:ad-fmcomms4-ebz:02_037516b_top.pdf|Rev B Schematics}} | [[adi>media/en/reference-design-documentation/design-integration-files/ad-fmcomms4-ebz-designsupport.zip|AD-FMCOMMS4-EBZ Design & Integration Files]] |
* {{:resources:eval:user-guides:ad-fmcomms4-ebz:08_037516b.7z|Rev B Gerbers}} (This file is [[http://www.7-zip.org/7z.html|compressed]]) | * Schematic |
| * PCB Layout |
* The Epson crystal used on this board, has the generic part number "TSX-3225 40.0000MHZ" - however, the generic part number does not have the specifications needed to meet the AD9361 datasheet specs. ADI has worked with Epson to provide a tighter tolerance part, which can be ordered as the "OUTD-2B-0166" or "X1E000021036701" (either part number will work, depending on which system your Epson contact/distributor has) which meets the requirements that the AD9361 demands. | * Bill of Materials |
| * Allegro Project |
</WRAP> | </WRAP> |
| |
===== I/O Voltage ===== | ===== I/O Voltage ===== |
| |
The AD-FMComms4 (AD9364) assumes a VDD_INTERFACE voltage between 1.71V and 2.625V (1.8 to 2.5 +/- 5%), so on your FPGA carrier board, you should ensure that V<sub>ADJ</sub> is between these levels. Setting things to 3.3V will damage the part. | The [[ADI>AD-FMCOMMS4-EBZ]] (AD9364) assumes a VDD_INTERFACE voltage between 1.71V and 2.625V (1.8 to 2.5 +/- 5%), so on your FPGA carrier board, you should ensure that V<sub>ADJ</sub> is between these levels. Setting things to 3.3V will damage the part. |
| |
| |
{{:resources:eval:user-guides:ad-fmcomms2-ebz:fmcomms2c_layers.png?direct&600|}} | {{:resources:eval:user-guides:ad-fmcomms2-ebz:fmcomms2c_layers.png?direct&600|}} |
| |
{{navigation AD-FMCOMMS2-EBZ#quickstart|Quick Start Guides#.:|Overview#reference_hdl|Reference HDL Design}} | |