Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
resources:eval:user-guides:ad-fmcomms4-ebz:hardware [29 Apr 2014 21:32] – [I/O Voltage] Robin Getz | resources:eval:user-guides:ad-fmcomms4-ebz:hardware [19 May 2021 16:03] – split rev B and C Robin Getz |
---|
| |
<WRAP round download 65%> | <WRAP round download 65%> |
<WRAP info>This is the latest and greatest Rev "B" of this board. Note that the Baluns on the Rev B board (T101-T104) are either : | <WRAP info>Note that the Baluns on the Rev C board (T101-T104) are either : |
* Johanson Technology's [[http://www.johansontechnology.com/images/stories/ip/baluns/Balun_2450BL15B050.pdf|2450BL15B050E]] 2.45 GHz Balun. This balun is rated for a operating frequency of 2400~2500 MHz. If you want to evaluate the part outside of this frequency range, an [[../ad-fmcomms2-ebz/hardware/configuration_options|alternative balun]] should be installed. The test results were taken using the Johanson Technology's 2450BL15B050E balun. | * Johanson Technology's [[http://www.johansontechnology.com/datasheets/baluns/JTI_Balun-2450BL15B050_12-03.pdf|2450BL15B050E]] 2.45 GHz Balun. This balun is rated for a operating frequency of 2400~2500 MHz and is connected to RXB Input and TXB Output. If you want to evaluate the part outside of this frequency range, use the other SMA. |
* Mini Circuits [[http://www.minicircuits.com/pdfs/TCM1-63AX+.pdf|TCM1-63AX+]]. They are rated for a operating frequency between 10 MHz and 6 GHz. | * Mini Circuits [[http://www.minicircuits.com/pdfs/TCM1-63AX+.pdf|TCM1-63AX+]]. They are rated for a operating frequency between 70 MHz and 6 GHz, and are connected to the RXA Input and TXB Output. |
| </WRAP> |
| * {{:resources:eval:user-guides:ad-fmcomms4-ebz:02-037516-01-c-1.pdf|Rev C Schematics}} |
| * {{:resources:eval:user-guides:ad-fmcomms4-ebz:09-037516-01C.zip|Rev C Gerbers}} (This file is [[http://www.7-zip.org/7z.html|compressed]]) |
| * {{:resources:eval:user-guides:ad-fmcomms4-ebz:05-037516-01-c.xls||Rev C BOM}} |
| </WRAP> |
| |
| <WRAP round download 65%> |
| <WRAP info>Note that the Baluns on the Rev B board (T101-T104) are either : |
| * Johanson Technology's [[http://www.johansontechnology.com/datasheets/baluns/JTI_Balun-2450BL15B050_12-03.pdf|2450BL15B050E]] 2.45 GHz Balun. This balun is rated for a operating frequency of 2400~2500 MHz. If you want to evaluate the part outside of this frequency range, an [[../ad-fmcomms2-ebz/hardware/configuration_options|alternative balun]] should be installed. The test results were taken using the Johanson Technology's 2450BL15B050E balun. |
| * Mini Circuits [[http://www.minicircuits.com/pdfs/TCM1-63AX+.pdf|TCM1-63AX+]]. They are rated for a operating frequency between 10 MHz and 6 GHz. |
</WRAP> | </WRAP> |
* {{:resources:eval:user-guides:ad-fmcomms4-ebz:02_037516b_top.pdf|Rev B Schematics}} | * {{:resources:eval:user-guides:ad-fmcomms4-ebz:02_037516b_top.pdf|Rev B Schematics}} |
* {{:resources:eval:user-guides:ad-fmcomms4-ebz:08_037516b.7z|Rev B Gerbers}} (This file is [[http://www.7-zip.org/7z.html|compressed]]) | * {{:resources:eval:user-guides:ad-fmcomms4-ebz:08_037516b.7z|Rev B Gerbers}} (This file is [[http://www.7-zip.org/7z.html|compressed]]) |
| * {{:resources:eval:user-guides:ad-fmcomms4-ebz:fmcomms4_bom.xls||Rev B BOM}} |
| |
* The Epson crystal used on this board, has the generic part number "TSX-3225 40.0000MHZ" - however, the generic part number does not have the specifications needed to meet the AD9361 datasheet specs. ADI has worked with Epson to provide a tighter tolerance part, which can be ordered as the "OUTD-2B-0166" or "X1E000021036701" (either part number will work, depending on which system your Epson contact/distributor has) which meets the requirements that the AD9361 demands. | * The Epson crystal used on this board, has the generic part number "TSX-3225 40.0000MHZ" - however, the generic part number does not have the specifications needed to meet the AD9361 datasheet specs. ADI has worked with Epson to provide a tighter tolerance part, which can be ordered as the "OUTD-2B-0166" or "X1E000021036701" (either part number will work, depending on which system your Epson contact/distributor has) which meets the requirements that the AD9361 demands. |
</WRAP> | </WRAP> |
| |
===== I/O Voltage ===== | ===== I/O Voltage ===== |
| |
{{:resources:eval:user-guides:ad-fmcomms2-ebz:fmcomms2c_layers.png?direct&600|}} | {{:resources:eval:user-guides:ad-fmcomms2-ebz:fmcomms2c_layers.png?direct&600|}} |
| |
{{navigation AD-FMCOMMS2-EBZ#quickstart|Quick Start Guides#.:|Overview#reference_hdl|Reference HDL Design}} | |