This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:ad-fmcomms3-ebz:hardware:configuration_options [08 Jan 2015 00:25] – add some external frequency stuff Robin Getz | resources:eval:user-guides:ad-fmcomms3-ebz:hardware:configuration_options [19 Jan 2018 10:26] (current) – rename xcomm_zynq -> master Alexandru Ardelean | ||
---|---|---|---|
Line 7: | Line 7: | ||
The AD-FMCOMMS2-EBZ and AD-FMCOMMS3-EBZ are both clocked from a 40.000000 MHz Epson crystal. If you want to run from a external source, you need to remove Y101, populate C113 (0.1uF Cap), and provide a low jitter clock source into J105 (SMA connector). If you provide anything but a 40.000000 MHz input, you are required to change the '' | The AD-FMCOMMS2-EBZ and AD-FMCOMMS3-EBZ are both clocked from a 40.000000 MHz Epson crystal. If you want to run from a external source, you need to remove Y101, populate C113 (0.1uF Cap), and provide a low jitter clock source into J105 (SMA connector). If you provide anything but a 40.000000 MHz input, you are required to change the '' | ||
- | <source / | + | <source / |
To change the frequency follow [[[[/ | To change the frequency follow [[[[/ | ||