This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-fmcomms2-ebz:software:datafiles [16 Aug 2017 09:07] – [AD-FMCOMMS2/3/4 Datafiles] Shuai Pei | resources:eval:user-guides:ad-fmcomms2-ebz:software:datafiles [27 Jan 2021 22:20] (current) – use wp> interwiki links Robin Getz | ||
---|---|---|---|
Line 9: | Line 9: | ||
<WRAP round info 65%> | <WRAP round info 65%> | ||
In order to run the models on this page, your MATLAB license needs to include the following components: | In order to run the models on this page, your MATLAB license needs to include the following components: | ||
- | * MATLAB Version 8.2 1 | + | * MATLAB Version 8.2 |
* Simulink Version 8.2 | * Simulink Version 8.2 | ||
* Communications System Toolbox Version 5.5 | * Communications System Toolbox Version 5.5 | ||
Line 77: | Line 77: | ||
=== Model === | === Model === | ||
- | The figure below shows a QPSK transmission model with the pulse shaping filters. Since pulse shaping filters are often distributed as a matched pair between transmitter and receiver, we use the filter shape of ‘Square root’(([[http:// | + | The figure below shows a QPSK transmission model with the pulse shaping filters. Since pulse shaping filters are often distributed as a matched pair between transmitter and receiver, we use the filter shape of ‘Square root’(([[wp>Root-raised-cosine_filter|Root-raised-cosine filter]])). |
{{QPSKwithfilter.png? | {{QPSKwithfilter.png? | ||
Line 208: | Line 208: | ||
===== MSK ===== | ===== MSK ===== | ||
- | MSK stands for minimum shift keying. It is one type of the continuous phase modulation (CPM) schemes (([[http:// | + | MSK stands for minimum shift keying. It is one type of the continuous phase modulation (CPM) schemes (([[wp>Minimum-shift_keying|Minimum-shift keying]])). In this section, we use "MSK Modulator Baseband" |
==== Model ==== | ==== Model ==== | ||
Line 266: | Line 266: | ||
The figure below shows a LTE example according to the specifications developed by the Third Generation Partnership Project (3GPP). It highlights only the downlink physical channel (PDSCH) processing. | The figure below shows a LTE example according to the specifications developed by the Third Generation Partnership Project (3GPP). It highlights only the downlink physical channel (PDSCH) processing. | ||
- | Since LTE is a sophisticated standard, you are encouraged to read the Help Document of this example and its related references to get more information (([[http:// | + | Since LTE is a sophisticated standard, you are encouraged to read the Help Document of this example and its related references to get more information (([[mw>help/ |
{{LTE.png? | {{LTE.png? |