This is an old revision of the document!
In this section, we provide the reference data files of several frequently used digital baseband modulation schemes and their corresponding Simulink models. With these data files, you are ready to transmit them using FMComms2 and test your board. By changing the given Simulink models, you can easily generate your own data files.
In order to run the models on this page, your MATLAB license needs to include the following components:
PSK is one type of the phase modulation (PM) schemes. In this section, two flavors of QPSK data are generated, one with raised cosine pulse shaping filters, and the other one without.
Since we would like to transmit the QPSK at a sample rate of 20M Symbols/s with AD-FMCOMMS2, the sample time specified in “Random-Integer Generator” block is 1/(20e6). The users can specify their own sample rate.
The figure below shows a QPSK transmission model without any pulse shaping filter. Since there are two independent channels on the Tx paths, we model both of them. However, for simplicity, we make them identical. The transmitted signals are saved to workspace.
You can download the Simulink model from below:
In order to observe the transmitted spectrum, we use a “Spectrum Analyzer” block. Since there is no pulse shaping on the Tx path, observe how rectangular-pulse QPSK symbols occupy the entire signal bandwidth in the frequency domain, potentially disturbing adjacent channels in the RF spectrum. Clearly this is not an efficient use of signal bandwidth.
You can download the generated data from below:
The QPSK symbols observed in the previous model cannot be transmitted over the air as perfect rectangular pulses, which would require infinite signal bandwidth. They must first be smoothed in the time domain, in order to limit the signal bandwidth in the frequency domain. Consequently, the first stage of the Tx signal chain is often a pulse-shaping filter, followed by subsequent stages of interpolation filters to increase the sampling rate to the DAC.
In this section, we will employ a root-raised cosine pulse-shaping filter to smooth the QPSK pulses in the time domain, limiting the signal bandwidth to 10 MHz in the frequency domain.
The figure below shows a QPSK transmission model with the pulse shaping filters. Since pulse shaping filters are often distributed as a matched pair between transmitter and receiver, we use the filter shape of ‘Square root’1).
You can download the Simulink model from below:
In order to observe the effect of the pulse shaping filters, we use a “Spectrum Analyzer” block, as well as several “Constellation” blocks.
We have the following observations:
You can download the generated data from below:
It is in the same format as the data in previous section.
Since there is no match filter on FMCOMMS2 receive path, the data obtained from FMCOMMS2 receiver side does not show the constellation of QPSK clearly. Therefore, by looking at the ADI IIO Oscilloscope2)., it is difficult to see whether the received data is valid or not, as shown in the figure below.
(add a figure here to show the IIO scope)
However, with the data capture function of the IIO application, we can now save the received data in MATLAB compatible format (.mat file), let the data pass through a match filter in Simulink, and then verify whether the received data is a QPSK or not. The data capture function can be accessed via “File”-“Save As”, as shown in the figure below.
(add a figure here to show the IIO data capture)
Before you save the data, you need to make sure the sampling rate of ADC and DAC are set properly. Set the sample rate of ADC and DAC 2 times of the generated data rate. Since the generated data rate is 30.72 MSPS, the ADC and DAC rate is 61.44 MSPS here.
In this model, the input I and Q are from the captured .mat file of FMCOMMS2. The received signals from FMCOMMS2 show a 45 degree rotation compared to the transmitted signal, so I add a frequency offset block in the receiver model.
QAM is one type of the amplitude modulation (AM) schemes. In this section, we use “Rectangular QAM Modulator Baseband” block to modulate the input random integer. If you would like a lower or higher order of QAM modulation, you only need to change the “M-ary number” of this block.
The figure below shows a 16-QAM transmission model with the square root raised cosine pulse shaping filters. In order to observe the effect of the pulse shaping filters, we use a “Spectrum Analyzer” block, as well as several “Constellation” blocks on one of the channels.
You can download the Simulink model from below:
You can download the generated 16-QAM data from below:
It is in the same format as the data in previous sections.
MSK stands for minimum shift keying. It is one type of the continuous phase modulation (CPM) schemes 3). In this section, we use “MSK Modulator Baseband” block to modulate the input random binary bits. In other words, the input is either 0 or 1.
The figure below shows a MSK transmission model with the square root raised cosine pulse shaping filters. In order to observe the effect of the pulse shaping filters, we use a “Spectrum Analyzer” block, as well as several “Constellation” blocks on one of the channels.
You can download the Simulink model from below:
You can download the generated MSK data from below:
It is in the same format as the data in previous sections.
Besides the data generated by the basic modulation schemes, it is also possible to transmit the data from some more advanced wireless communication standards. In this section, we will generate some LTE (Long Term Evolution) data from an existing Simulink example.
The figure below shows a LTE example according to the specifications developed by the Third Generation Partnership Project (3GPP). It highlights only the downlink physical channel (PDSCH) processing. In order to obtain the transmitted data, we add a “Signal to Workspace” block on the transmitter side (circled in red). By double clicking the “Model Parameters” block, we can change the model settings such as channel bandwidth, antenna configuration and etc.
Since LTE is a sophisticated standard, you are encouraged to read the Help Document of this example and its related references to get more information 4).
After you run the model, the transmitted data named “Tx” will be saved in workspace. Since it is a Nx2 complex vector, we need to do some processing on it to make the data format compatible with FMComms2 transmission.
You can download the Simulink model and the post-processing m-file from below:
When the data is transmitted and received by real-world hardware, like FMComms2, it is difficult to observe the clear constellation without proper synchronization techniques. However, even with the basic settings, you are still expected to observe the transmit and receive spectrum, which is similar to the following:
Note that the bandwidth shown in the spectrum is approximately 10 MHz, which is consistent with the “Channel bandwidth” setting of the model parameters.
You can download the generated LTE data from below:
It is in the same format as the data in previous sections.