Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:ad-fmcomms2-ebz:software:baremetal [12 Feb 2017 05:33] – [AD9361 No-OS API] nishant kumar | resources:eval:user-guides:ad-fmcomms2-ebz:software:baremetal [18 Sep 2023 09:26] (current) – update build instructions Darius B |
---|
====== AD9361 No-OS Software ====== | ====== AD9361 No-OS Software ====== |
| |
| The AD9361 is a high performance, highly integrated RF Agile Transceiver™. Its programmability and wideband capability make it ideal for a broad range of transceiver applications. The device combines an RF front end with a flexible mixed-signal baseband section and integrated frequency synthesizers, simplifying design-in by providing a configurable digital interface to a processor. |
| |
| ===== Supported Devices ===== |
| |
| * [[adi>AD9361]] |
| * [[adi>AD9363]] |
| * [[adi>AD9364]] |
| |
===== Introduction ===== | ===== Introduction ===== |
|<code c>int32_t ad9361_get_rx_lo_freq | |<code c>int32_t ad9361_get_rx_lo_freq |
(struct ad9361_rf_phy *phy, uint64_t *lo_freq_hz)</code>|Gets current LO frequency. Receives as parameters a structure that contains the AD9361 current state and a variable to store the LO frequency value in Hz. Returns 0 in case of success, negative error code otherwise.| | (struct ad9361_rf_phy *phy, uint64_t *lo_freq_hz)</code>|Gets current LO frequency. Receives as parameters a structure that contains the AD9361 current state and a variable to store the LO frequency value in Hz. Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_set_rx_lo_int_ext(struct ad9361_rf_phy *phy, uint8_t int_ext)</code>|Switches between internal and external LO. Receives as parameters a structure that contains the AD9361 current state and the desired option (INT_LO, EXT_LO). Returns 0 in case of success, negative error code otherwise.| |
|<code c>int32_t ad9361_get_rx_rssi | |<code c>int32_t ad9361_get_rx_rssi |
(struct ad9361_rf_phy *phy, uint8_t ch, struct rf_rssi *rssi)</code>|Gets the RSSI for the selected channel. Receives as parameters a structure that contains the AD9361 current state, the desired channel (0, 1) and a variable to store the RSSI. Returns 0 in case of success, negative error code otherwise.| | (struct ad9361_rf_phy *phy, uint8_t ch, struct rf_rssi *rssi)</code>|Gets the RSSI for the selected channel. Receives as parameters a structure that contains the AD9361 current state, the desired channel (0, 1) and a variable to store the RSSI. Returns 0 in case of success, negative error code otherwise.| |
|<code c>int32_t ad9361_set_rx_fir_config | |<code c>int32_t ad9361_set_rx_fir_config |
(struct ad9361_rf_phy *phy, AD9361_RXFIRConfig fir_cfg)</code>|Sets the FIR filter configuration. Receives as parameters a structure that contains the AD9361 current state and the FIR filter configuration. Returns 0 in case of success, negative error code otherwise.| | (struct ad9361_rf_phy *phy, AD9361_RXFIRConfig fir_cfg)</code>|Sets the FIR filter configuration. Receives as parameters a structure that contains the AD9361 current state and the FIR filter configuration. Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_get_rx_fir_config(struct ad9361_rf_phy *phy, uint8_t rx_ch, AD9361_RXFIRConfig *fir_cfg)</code>|Gets the RX FIR filter configuration. Receives as parameters a structure that contains the AD9361 current state, the desired channel (RX1, RX2) and the location for storing the FIR filter configuration. Returns 0 in case of success, negative error code otherwise.| |
|<code c>int32_t ad9361_set_rx_fir_en_dis | |<code c>int32_t ad9361_set_rx_fir_en_dis |
(struct ad9361_rf_phy *phy, uint8_t en_dis)</code>|Enables/disables the FIR filter. Receives as parameters a structure that contains the AD9361 current state and the option (ENABLE, DISABLE). Returns 0 in case of success, negative error code otherwise.| | (struct ad9361_rf_phy *phy, uint8_t en_dis)</code>|Enables/disables the FIR filter. Receives as parameters a structure that contains the AD9361 current state and the option (ENABLE, DISABLE). Returns 0 in case of success, negative error code otherwise.| |
|<code c>int32_t ad9361_get_rx_quad_track_en_dis | |<code c>int32_t ad9361_get_rx_quad_track_en_dis |
(struct ad9361_rf_phy *phy, uint8_t *en_dis)</code>|Gets the status of the RX Quadrature Tracking. Receives as parameters a structure that contains the AD9361 current state and the enable/disable status buffer.Returns 0 in case of success, negative error code otherwise.| | (struct ad9361_rf_phy *phy, uint8_t *en_dis)</code>|Gets the status of the RX Quadrature Tracking. Receives as parameters a structure that contains the AD9361 current state and the enable/disable status buffer.Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_set_rx_rf_port_input (struct ad9361_rf_phy *phy,uint32_t mode)</code>|Sets the RX RF input port. Receives as parameters a structure that contains the AD9361 current state and the desired port (A_BALANCED, B_BALANCED, C_BALANCED, A_N, A_P, B_N, B_P, C_N, C_P, TX_MON1, TX_MON2, TX_MON1_2). Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_get_rx_rf_port_input (struct ad9361_rf_phy *phy,uint32_t *mode)</code>|Gets the selected RX RF input port. Receives as parameters a structure that contains the AD9361 current state and the location to store the selected port value. Returns 0 in case of success, negative error code otherwise. Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_rx_fastlock_store(struct ad9361_rf_phy *phy, uint32_t profile)</code>|Stores RX fastlock profile. To create a profile tune the synthesizer (ad9361_set_rx_lo_freq()) and then call this function specifying the target profile number. Receives as parameters a structure that contains the AD9361 current state and the profile number (0 - 7). Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_rx_fastlock_recall(struct ad9361_rf_phy *phy, uint32_t profile)</code>|Recalls specified RX fastlock profile. When in fastlock pin select mode (init_param->rx_fastlock_pincontrol_enable), the function needs to be called before then the pin-control can be used. Receives as parameters a structure that contains the AD9361 current state and the profile number (0 - 7). Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_rx_fastlock_load(struct ad9361_rf_phy *phy, uint32_t profile, uint8_t *values)</code>|Recalls specified RX fastlock profile. When in fastlock pin select mode (init_param->rx_fastlock_pincontrol_enable), the function needs to be called before then the pin-control can be used. Receives as parameters a structure that contains the AD9361 current state, the profile number (0 - 7) and the Fastlock profile program data (val0,val1,val2,...,val15). Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_rx_fastlock_save(struct ad9361_rf_phy *phy, uint32_t profile, uint8_t *values)</code>|Saves RX fastlock profile. In order to use more than 8 Profiles, an existing profile can be read back and stored by the user application. Receives as parameters a structure that contains the AD9361 current state, the profile number (0 - 7) and the location for storing the profile data. Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_rx_lo_powerdown(struct ad9361_rf_phy *phy, uint8_t option)</code>|Powers down the RX Local Oscillator. Receives as parameters a structure that contains the AD9361 current state and the option (ON, OFF). Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_get_rx_lo_power(struct ad9361_rf_phy *phy, uint8_t *option)</code>|Gets the RX Local Oscillator power status. Receives as parameters a structure that contains the AD9361 current state and the location to store the selected option. Returns 0 in case of success, negative error code otherwise.| |
^ Transmit Chain Settings ^^ | ^ Transmit Chain Settings ^^ |
|<code c>int32_t ad9361_set_tx_attenuation | |<code c>int32_t ad9361_set_tx_attenuation |
|<code c>int32_t ad9361_get_tx_lo_freq | |<code c>int32_t ad9361_get_tx_lo_freq |
(struct ad9361_rf_phy *phy, uint64_t *lo_freq_hz)</code>|Gets current LO frequency. Receives as parameters a structure that contains the AD9361 current state and a variable to store the LO frequency value in Hz. Returns 0 in case of success, negative error code otherwise.| | (struct ad9361_rf_phy *phy, uint64_t *lo_freq_hz)</code>|Gets current LO frequency. Receives as parameters a structure that contains the AD9361 current state and a variable to store the LO frequency value in Hz. Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_set_tx_lo_int_ext(struct ad9361_rf_phy *phy, uint8_t int_ext)</code>|Switches between internal and external LO. Receives as parameters a structure that contains the AD9361 current state and the desired option (INT_LO, EXT_LO). Returns 0 in case of success, negative error code otherwise.| |
|<code c>int32_t ad9361_set_tx_fir_config | |<code c>int32_t ad9361_set_tx_fir_config |
(struct ad9361_rf_phy *phy, AD9361_TXFIRConfig fir_cfg)</code>|Sets the FIR filter configuration. Receives as parameters a structure that contains the AD9361 current state and the FIR filter configuration. Returns 0 in case of success, negative error code otherwise.| | (struct ad9361_rf_phy *phy, AD9361_TXFIRConfig fir_cfg)</code>|Sets the FIR filter configuration. Receives as parameters a structure that contains the AD9361 current state and the FIR filter configuration. Returns 0 in case of success, negative error code otherwise.| |
| |
| |<code c>int32_t ad9361_get_tx_fir_config(struct ad9361_rf_phy *phy, uint8_t tx_ch, AD9361_TXFIRConfig *fir_cfg)</code>|Gets the TX FIR filter configuration. Receives as parameters a structure that contains the AD9361 current state and the location to store the FIR filter configuration. Returns 0 in case of success, negative error code otherwise.| |
|<code c>int32_t ad9361_set_tx_fir_en_dis | |<code c>int32_t ad9361_set_tx_fir_en_dis |
(struct ad9361_rf_phy *phy, uint8_t en_dis)</code>|Enables/disables the FIR filter. Receives as parameters a structure that contains the AD9361 current state and the option (ENABLE, DISABLE). Returns 0 in case of success, negative error code otherwise.| | (struct ad9361_rf_phy *phy, uint8_t en_dis)</code>|Enables/disables the FIR filter. Receives as parameters a structure that contains the AD9361 current state and the option (ENABLE, DISABLE). Returns 0 in case of success, negative error code otherwise.| |
uint8_t ch, | uint8_t ch, |
uint32_t *rssi_db_x_1000)</code>|Gets the TX RSSI for the selected channel. Receives as parameters a structure that contains the AD9361 current state, the desired channel (0, 1) and a variable to store the RSSI. Returns 0 in case of success, negative error code otherwise.| | uint32_t *rssi_db_x_1000)</code>|Gets the TX RSSI for the selected channel. Receives as parameters a structure that contains the AD9361 current state, the desired channel (0, 1) and a variable to store the RSSI. Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_set_tx_rf_port_output (struct ad9361_rf_phy *phy, uint32_t mode)</code>|Sets the TX RF output port. Receives as parameters a structure that contains the AD9361 current state and the desired port (TXA, TXB). Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_get_tx_rf_port_output (struct ad9361_rf_phy *phy, uint32_t *mode)</code>|Gets the selected TX RF output port. Receives as parameters a structure that contains the AD9361 current state and the location for storing the selected port. Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_set_tx_auto_cal_en_dis (struct ad9361_rf_phy *phy, uint8_t en_dis)</code>|Enables/disables the auto calibration. Receives as parameters a structure that contains the AD9361 current state and the desired mode (ENABLE, DISABLE). Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_get_tx_auto_cal_en_dis (struct ad9361_rf_phy *phy, uint8_t *en_dis)</code>|Gets the status of the auto calibration flag. Receives as parameters a structure that contains the AD9361 current state and the location for storing the selected mode. Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_tx_fastlock_store(struct ad9361_rf_phy *phy, uint32_t profile)</code>|Stores TX fastlock profile. Receives as parameters a structure that contains the AD9361 current state and the profile number (0 - 7). Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_tx_fastlock_recall(struct ad9361_rf_phy *phy, uint32_t profile)</code>|Recalls specified TX fastlock profile. Receives as parameters a structure that contains the AD9361 current state and the profile number (0 - 7). Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_tx_fastlock_load(struct ad9361_rf_phy *phy, uint32_t profile, uint8_t *values)</code>|Loads TX fastlock profile. A previously saved profile can be loaded in any of the 8 available slots. Receives as parameters a structure that contains the AD9361 current state, the profile number (0 - 7) and the Fastlock profile program data (val0,val1,val2,...,val15). Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_tx_fastlock_save(struct ad9361_rf_phy *phy, uint32_t profile, uint8_t *values)</code>|Saves TX fastlock profile. In order to use more than 8 Profiles, an existing profile can be read back and stored by the user application. Receives as parameters a structure that contains the AD9361 current state, the profile number (0 - 7) and the location for storing the profile data. Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_tx_lo_powerdown(struct ad9361_rf_phy *phy, uint8_t option)</code>|Powers down the TX Local Oscillator. Receives as parameters a structure that contains the AD9361 current state and the desired option (ON, OFF). Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_get_tx_lo_power(struct ad9361_rf_phy *phy, uint8_t *option)</code>|Gets the TX Local Oscillator power status. Receives as parameters a structure that contains the AD9361 current state and the location to store the selected option. Returns 0 in case of success, negative error code otherwise.| |
|<code c>int32_t ad9361_set_trx_path_clks | |<code c>int32_t ad9361_set_trx_path_clks |
(struct ad9361_rf_phy *phy, | (struct ad9361_rf_phy *phy, |
|<code c>int32_t ad9361_set_no_ch_mode | |<code c>int32_t ad9361_set_no_ch_mode |
(struct ad9361_rf_phy *phy, uint8_t no_ch_mode)</code>|Set the number of channels mode. Receives as parameters a structure that contains the AD9361 current state and the number of channels mode (1 - 1x1; 2 - 2x2). Returns 0 in case of success, negative error code otherwise.| | (struct ad9361_rf_phy *phy, uint8_t no_ch_mode)</code>|Set the number of channels mode. Receives as parameters a structure that contains the AD9361 current state and the number of channels mode (1 - 1x1; 2 - 2x2). Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_do_mcs(struct ad9361_rf_phy *phy_master, struct ad9361_rf_phy *phy_slave)</code>|Do multi chip synchronization. Receives as parameters a structure that contains the AD9361 master current state and a structure that contains the AD9361 slave current state. Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_set_trx_fir_en_dis (struct ad9361_rf_phy *phy, uint8_t en_dis)</code>|Enables/disables the TRX FIR filters. Receives as parameters a structure that contains the AD9361 current state and the desired option (ENABLE, DISABLE). Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_set_trx_rate_gov (struct ad9361_rf_phy *phy, uint32_t rate_gov)</code>|Set the OSR rate governor. Receives as parameters a structure that contains the AD9361 current state and the desired OSR rate governor (HIGHEST_OSR, NOMINAL_OSR). Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_get_trx_rate_gov (struct ad9361_rf_phy *phy, uint32_t *rate_gov)</code>|Gets the OSR rate governor. Receives as parameters a structure that contains the AD9361 master current state and the location for storing the OSR rate governor. Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_do_calib(struct ad9361_rf_phy *phy, uint32_t cal, int32_t arg)</code>|Performs the selected calibration. Receives as parameters a structure that contains the AD9361 current state, the desired calibration (TX_QUAD_CAL, RFDC_CAL) and for TX_QUAD_CAL, the optional RX phase value overwrite (set to zero). Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_trx_load_enable_fir(struct ad9361_rf_phy *phy, AD9361_RXFIRConfig rx_fir_cfg, AD9361_TXFIRConfig tx_fir_cfg)</code>|Loads and enables TRX FIR filters configurations. Receives as parameters a structure that contains the AD9361 current state, the RX FIR filter configuration and the TX FIR filter configuration. Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_do_dcxo_tune_coarse(struct ad9361_rf_phy *phy, uint32_t coarse)</code>|Does DCXO coarse tuning. Receives as parameters a structure that contains the AD9361 current state and the DCXO coarse tuning value. Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_do_dcxo_tune_fine(struct ad9361_rf_phy *phy, uint32_t fine)</code>|Does DCXO fine tuning. Receives as parameters a structure that contains the AD9361 current state and the DCXO fine tuning value. Returns 0 in case of success, negative error code otherwise.| |
| |<code c>int32_t ad9361_get_temperature(struct ad9361_rf_phy *phy, int32_t *temp)</code>|Gets the temperature. Receives as parameters a structure that contains the AD9361 current state and the location for storing the current temperature (degrees C * 1000). Returns 0 in case of success, negative error code otherwise.| |
| |
**Notes:** | **Notes:** |
| |
<code C> | <code C> |
typedef struct | typedef struct |
{ | { |
/* Identification number */ | /* Device selection */ |
uint8_t id_no; | enum dev_id dev_sel; |
/* Reference Clock */ | /* Identification number */ |
uint32_t reference_clk_rate; | uint8_t id_no; |
/* Base Configuration */ | /* Reference Clock */ |
uint8_t two_rx_two_tx_mode_enable; /* adi,2rx-2tx-mode-enable */ | uint32_t reference_clk_rate; |
uint8_t frequency_division_duplex_mode_enable; /* adi,frequency-division-duplex-mode-enable */ | /* Base Configuration */ |
uint8_t tdd_use_dual_synth_mode_enable; /* adi,tdd-use-dual-synth-mode-enable */ | uint8_t two_rx_two_tx_mode_enable; /* adi,2rx-2tx-mode-enable */ |
uint8_t tdd_skip_vco_cal_enable; /* adi,tdd-skip-vco-cal-enable */ | uint8_t one_rx_one_tx_mode_use_rx_num; /* adi,1rx-1tx-mode-use-rx-num */ |
uint32_t tx_fastlock_delay_ns; /* adi,tx-fastlock-delay-ns */ | uint8_t one_rx_one_tx_mode_use_tx_num; /* adi,1rx-1tx-mode-use-tx-num */ |
uint32_t rx_fastlock_delay_ns; /* adi,rx-fastlock-delay-ns */ | uint8_t frequency_division_duplex_mode_enable; /* adi,frequency-division-duplex-mode-enable */ |
uint8_t rx_fastlock_pincontrol_enable; /* adi,rx-fastlock-pincontrol-enable */ | uint8_t frequency_division_duplex_independent_mode_enable; /* adi,frequency-division-duplex-independent-mode-enable */ |
uint8_t tx_fastlock_pincontrol_enable; /* adi,tx-fastlock-pincontrol-enable */ | uint8_t tdd_use_dual_synth_mode_enable; /* adi,tdd-use-dual-synth-mode-enable */ |
uint8_t external_rx_lo_enable; /* adi,external-rx-lo-enable */ | uint8_t tdd_skip_vco_cal_enable; /* adi,tdd-skip-vco-cal-enable */ |
uint8_t external_tx_lo_enable; /* adi,external-tx-lo-enable */ | uint32_t tx_fastlock_delay_ns; /* adi,tx-fastlock-delay-ns */ |
uint8_t dc_offset_tracking_update_event_mask; /* adi,dc-offset-tracking-update-event-mask */ | uint32_t rx_fastlock_delay_ns; /* adi,rx-fastlock-delay-ns */ |
uint8_t dc_offset_attenuation_high_range; /* adi,dc-offset-attenuation-high-range */ | uint8_t rx_fastlock_pincontrol_enable; /* adi,rx-fastlock-pincontrol-enable */ |
uint8_t dc_offset_attenuation_low_range; /* adi,dc-offset-attenuation-low-range */ | uint8_t tx_fastlock_pincontrol_enable; /* adi,tx-fastlock-pincontrol-enable */ |
uint8_t dc_offset_count_high_range; /* adi,dc-offset-count-high-range */ | uint8_t external_rx_lo_enable; /* adi,external-rx-lo-enable */ |
uint8_t dc_offset_count_low_range; /* adi,dc-offset-count-low-range */ | uint8_t external_tx_lo_enable; /* adi,external-tx-lo-enable */ |
uint8_t tdd_use_fdd_vco_tables_enable; /* adi,tdd-use-fdd-vco-tables-enable */ | uint8_t dc_offset_tracking_update_event_mask; /* adi,dc-offset-tracking-update-event-mask */ |
uint8_t split_gain_table_mode_enable; /* adi,split-gain-table-mode-enable */ | uint8_t dc_offset_attenuation_high_range; /* adi,dc-offset-attenuation-high-range */ |
uint32_t trx_synthesizer_target_fref_overwrite_hz; /* adi,trx-synthesizer-target-fref-overwrite-hz */ | uint8_t dc_offset_attenuation_low_range; /* adi,dc-offset-attenuation-low-range */ |
uint8_t qec_tracking_slow_mode_enable; /* adi,qec-tracking-slow-mode-enable */ | uint8_t dc_offset_count_high_range; /* adi,dc-offset-count-high-range */ |
/* ENSM Control */ | uint8_t dc_offset_count_low_range; /* adi,dc-offset-count-low-range */ |
uint8_t ensm_enable_pin_pulse_mode_enable; /* adi,ensm-enable-pin-pulse-mode-enable */ | uint8_t split_gain_table_mode_enable; /* adi,split-gain-table-mode-enable */ |
uint8_t ensm_enable_txnrx_control_enable; /* adi,ensm-enable-txnrx-control-enable */ | uint32_t trx_synthesizer_target_fref_overwrite_hz; /* adi,trx-synthesizer-target-fref-overwrite-hz */ |
/* LO Control */ | uint8_t qec_tracking_slow_mode_enable; /* adi,qec-tracking-slow-mode-enable */ |
uint64_t rx_synthesizer_frequency_hz; /* adi,rx-synthesizer-frequency-hz */ | /* ENSM Control */ |
uint64_t tx_synthesizer_frequency_hz; /* adi,tx-synthesizer-frequency-hz */ | uint8_t ensm_enable_pin_pulse_mode_enable; /* adi,ensm-enable-pin-pulse-mode-enable */ |
/* Rate & BW Control */ | uint8_t ensm_enable_txnrx_control_enable; /* adi,ensm-enable-txnrx-control-enable */ |
uint32_t rx_path_clock_frequencies[6]; /* adi,rx-path-clock-frequencies */ | /* LO Control */ |
uint32_t tx_path_clock_frequencies[6]; /* adi,tx-path-clock-frequencies */ | uint64_t rx_synthesizer_frequency_hz; /* adi,rx-synthesizer-frequency-hz */ |
uint32_t rf_rx_bandwidth_hz; /* adi,rf-rx-bandwidth-hz */ | uint64_t tx_synthesizer_frequency_hz; /* adi,tx-synthesizer-frequency-hz */ |
uint32_t rf_tx_bandwidth_hz; /* adi,rf-tx-bandwidth-hz */ | uint8_t tx_lo_powerdown_managed_enable; /* adi,tx-lo-powerdown-managed-enable */ |
/* RF Port Control */ | /* Rate & BW Control */ |
uint32_t rx_rf_port_input_select; /* adi,rx-rf-port-input-select */ | uint32_t rx_path_clock_frequencies[6]; /* adi,rx-path-clock-frequencies */ |
uint32_t tx_rf_port_input_select; /* adi,tx-rf-port-input-select */ | uint32_t tx_path_clock_frequencies[6]; /* adi,tx-path-clock-frequencies */ |
/* TX Attenuation Control */ | uint32_t rf_rx_bandwidth_hz; /* adi,rf-rx-bandwidth-hz */ |
int32_t tx_attenuation_mdB; /* adi,tx-attenuation-mdB */ | uint32_t rf_tx_bandwidth_hz; /* adi,rf-tx-bandwidth-hz */ |
uint8_t update_tx_gain_in_alert_enable; /* adi,update-tx-gain-in-alert-enable */ | /* RF Port Control */ |
/* Reference Clock Control */ | uint32_t rx_rf_port_input_select; /* adi,rx-rf-port-input-select */ |
uint8_t xo_disable_use_ext_refclk_enable; /* adi,xo-disable-use-ext-refclk-enable */ | uint32_t tx_rf_port_input_select; /* adi,tx-rf-port-input-select */ |
uint32_t dcxo_coarse_and_fine_tune[2]; /* adi,dcxo-coarse-and-fine-tune */ | /* TX Attenuation Control */ |
uint32_t clk_output_mode_select; /* adi,clk-output-mode-select */ | int32_t tx_attenuation_mdB; /* adi,tx-attenuation-mdB */ |
/* Gain Control */nishant | uint8_t update_tx_gain_in_alert_enable; /* adi,update-tx-gain-in-alert-enable */ |
uint8_t gc_rx1_mode; /* adi,gc-rx1-mode */ | /* Reference Clock Control */ |
uint8_t gc_rx2_mode; /* adi,gc-rx2-mode */ | uint8_t xo_disable_use_ext_refclk_enable; /* adi,xo-disable-use-ext-refclk-enable */ |
uint8_t gc_adc_large_overload_thresh; /* adi,gc-adc-large-overload-thresh */ | uint32_t dcxo_coarse_and_fine_tune[2]; /* adi,dcxo-coarse-and-fine-tune */ |
uint8_t gc_adc_ovr_sample_size; /* adi,gc-adc-ovr-sample-size */ | uint32_t clk_output_mode_select; /* adi,clk-output-mode-select */ |
uint8_t gc_adc_small_overload_thresh; /* adi,gc-adc-small-overload-thresh */ | /* Gain Control */ |
uint16_t gc_dec_pow_measurement_duration; /* adi,gc-dec-pow-measurement-duration */ | uint8_t gc_rx1_mode; /* adi,gc-rx1-mode */ |
uint8_t gc_dig_gain_enable; /* adi,gc-dig-gain-enable */ | uint8_t gc_rx2_mode; /* adi,gc-rx2-mode */ |
uint16_t gc_lmt_overload_high_thresh; /* adi,gc-lmt-overload-high-thresh */ | uint8_t gc_adc_large_overload_thresh; /* adi,gc-adc-large-overload-thresh */ |
uint16_t gc_lmt_overload_low_thresh; /* adi,gc-lmt-overload-low-thresh */ | uint8_t gc_adc_ovr_sample_size; /* adi,gc-adc-ovr-sample-size */ |
uint8_t gc_low_power_thresh; /* adi,gc-low-power-thresh */ | uint8_t gc_adc_small_overload_thresh; /* adi,gc-adc-small-overload-thresh */ |
uint8_t gc_max_dig_gain; /* adi,gc-max-dig-gain */ | uint16_t gc_dec_pow_measurement_duration; /* adi,gc-dec-pow-measurement-duration */ |
/* Gain MGC Control */ | uint8_t gc_dig_gain_enable; /* adi,gc-dig-gain-enable */ |
uint8_t mgc_dec_gain_step; /* adi,mgc-dec-gain-step */ | uint16_t gc_lmt_overload_high_thresh; /* adi,gc-lmt-overload-high-thresh */ |
uint8_t mgc_inc_gain_step; /* adi,mgc-inc-gain-step */ | uint16_t gc_lmt_overload_low_thresh; /* adi,gc-lmt-overload-low-thresh */ |
uint8_t mgc_rx1_ctrl_inp_enable; /* adi,mgc-rx1-ctrl-inp-enable */ | uint8_t gc_low_power_thresh; /* adi,gc-low-power-thresh */ |
uint8_t mgc_rx2_ctrl_inp_enable; /* adi,mgc-rx2-ctrl-inp-enable */ | uint8_t gc_max_dig_gain; /* adi,gc-max-dig-gain */ |
uint8_t mgc_split_table_ctrl_inp_gain_mode; /* adi,mgc-split-table-ctrl-inp-gain-mode */ | /* Gain MGC Control */ |
/* Gain AGC Control */ | uint8_t mgc_dec_gain_step; /* adi,mgc-dec-gain-step */ |
uint8_t agc_adc_large_overload_exceed_counter; /* adi,agc-adc-large-overload-exceed-counter */ | uint8_t mgc_inc_gain_step; /* adi,mgc-inc-gain-step */ |
uint8_t agc_adc_large_overload_inc_steps; /* adi,agc-adc-large-overload-inc-steps */ | uint8_t mgc_rx1_ctrl_inp_enable; /* adi,mgc-rx1-ctrl-inp-enable */ |
uint8_t agc_adc_lmt_small_overload_prevent_gain_inc_enable; /* adi,agc-adc-lmt-small-overload-prevent-gain-inc-enable */ | uint8_t mgc_rx2_ctrl_inp_enable; /* adi,mgc-rx2-ctrl-inp-enable */ |
uint8_t agc_adc_small_overload_exceed_counter; /* adi,agc-adc-small-overload-exceed-counter */ | uint8_t mgc_split_table_ctrl_inp_gain_mode; /* adi,mgc-split-table-ctrl-inp-gain-mode */ |
uint8_t agc_dig_gain_step_size; /* adi,agc-dig-gain-step-size */ | /* Gain AGC Control */ |
uint8_t agc_dig_saturation_exceed_counter; /* adi,agc-dig-saturation-exceed-counter */ | uint8_t agc_adc_large_overload_exceed_counter; /* adi,agc-adc-large-overload-exceed-counter */ |
uint32_t agc_gain_update_interval_us; /* adi,agc-gain-update-interval-us */ | uint8_t agc_adc_large_overload_inc_steps; /* adi,agc-adc-large-overload-inc-steps */ |
uint8_t agc_immed_gain_change_if_large_adc_overload_enable; /* adi,agc-immed-gain-change-if-large-adc-overload-enable */ | uint8_t agc_adc_lmt_small_overload_prevent_gain_inc_enable; /* adi,agc-adc-lmt-small-overload-prevent-gain-inc-enable */ |
uint8_t agc_immed_gain_change_if_large_lmt_overload_enable; /* adi,agc-immed-gain-change-if-large-lmt-overload-enable */ | uint8_t agc_adc_small_overload_exceed_counter; /* adi,agc-adc-small-overload-exceed-counter */ |
uint8_t agc_inner_thresh_high; /* adi,agc-inner-thresh-high */ | uint8_t agc_dig_gain_step_size; /* adi,agc-dig-gain-step-size */ |
uint8_t agc_inner_thresh_high_dec_steps; /* adi,agc-inner-thresh-high-dec-steps */ | uint8_t agc_dig_saturation_exceed_counter; /* adi,agc-dig-saturation-exceed-counter */ |
uint8_t agc_inner_thresh_low; /* adi,agc-inner-thresh-low */ | uint32_t agc_gain_update_interval_us; /* adi,agc-gain-update-interval-us */ |
uint8_t agc_inner_thresh_low_inc_steps; /* adi,agc-inner-thresh-low-inc-steps */ | uint8_t agc_immed_gain_change_if_large_adc_overload_enable; /* adi,agc-immed-gain-change-if-large-adc-overload-enable */ |
uint8_t agc_lmt_overload_large_exceed_counter; /* adi,agc-lmt-overload-large-exceed-counter */ | uint8_t agc_immed_gain_change_if_large_lmt_overload_enable; /* adi,agc-immed-gain-change-if-large-lmt-overload-enable */ |
uint8_t agc_lmt_overload_large_inc_steps; /* adi,agc-lmt-overload-large-inc-steps */ | uint8_t agc_inner_thresh_high; /* adi,agc-inner-thresh-high */ |
uint8_t agc_lmt_overload_small_exceed_counter; /* adi,agc-lmt-overload-small-exceed-counter */ | uint8_t agc_inner_thresh_high_dec_steps; /* adi,agc-inner-thresh-high-dec-steps */ |
uint8_t agc_outer_thresh_high; /* adi,agc-outer-thresh-high */ | uint8_t agc_inner_thresh_low; /* adi,agc-inner-thresh-low */ |
uint8_t agc_outer_thresh_high_dec_steps; /* adi,agc-outer-thresh-high-dec-steps */ | uint8_t agc_inner_thresh_low_inc_steps; /* adi,agc-inner-thresh-low-inc-steps */ |
uint8_t agc_outer_thresh_low; /* adi,agc-outer-thresh-low */ | uint8_t agc_lmt_overload_large_exceed_counter; /* adi,agc-lmt-overload-large-exceed-counter */ |
uint8_t agc_outer_thresh_low_inc_steps; /* adi,agc-outer-thresh-low-inc-steps */ | uint8_t agc_lmt_overload_large_inc_steps; /* adi,agc-lmt-overload-large-inc-steps */ |
uint32_t agc_attack_delay_extra_margin_us; /* adi,agc-attack-delay-extra-margin-us */ | uint8_t agc_lmt_overload_small_exceed_counter; /* adi,agc-lmt-overload-small-exceed-counter */ |
uint8_t agc_sync_for_gain_counter_enable; /* adi,agc-sync-for-gain-counter-enable */ | uint8_t agc_outer_thresh_high; /* adi,agc-outer-thresh-high */ |
/* Fast AGC */ | uint8_t agc_outer_thresh_high_dec_steps; /* adi,agc-outer-thresh-high-dec-steps */ |
uint32_t fagc_dec_pow_measuremnt_duration; /* adi,fagc-dec-pow-measurement-duration */ | uint8_t agc_outer_thresh_low; /* adi,agc-outer-thresh-low */ |
uint32_t fagc_state_wait_time_ns; /* adi,fagc-state-wait-time-ns */ | uint8_t agc_outer_thresh_low_inc_steps; /* adi,agc-outer-thresh-low-inc-steps */ |
/* Fast AGC - Low Power */ | uint32_t agc_attack_delay_extra_margin_us; /* adi,agc-attack-delay-extra-margin-us */ |
uint8_t fagc_allow_agc_gain_increase; /* adi,fagc-allow-agc-gain-increase-enable */ | uint8_t agc_sync_for_gain_counter_enable; /* adi,agc-sync-for-gain-counter-enable */ |
uint32_t fagc_lp_thresh_increment_time; /* adi,fagc-lp-thresh-increment-time */ | /* Fast AGC */ |
uint32_t fagc_lp_thresh_increment_steps; /* adi,fagc-lp-thresh-increment-steps */ | uint32_t fagc_dec_pow_measuremnt_duration; /* adi,fagc-dec-pow-measurement-duration */ |
/* Fast AGC - Lock Level */ | uint32_t fagc_state_wait_time_ns; /* adi,fagc-state-wait-time-ns */ |
uint32_t fagc_lock_level; /* adi,fagc-lock-level */ | /* Fast AGC - Low Power */ |
uint8_t fagc_lock_level_lmt_gain_increase_en; /* adi,fagc-lock-level-lmt-gain-increase-enable */ | uint8_t fagc_allow_agc_gain_increase; /* adi,fagc-allow-agc-gain-increase-enable */ |
uint32_t fagc_lock_level_gain_increase_upper_limit; /* adi,fagc-lock-level-gain-increase-upper-limit */ | uint32_t fagc_lp_thresh_increment_time; /* adi,fagc-lp-thresh-increment-time */ |
/* Fast AGC - Peak Detectors and Final Settling */ | uint32_t fagc_lp_thresh_increment_steps; /* adi,fagc-lp-thresh-increment-steps */ |
uint32_t fagc_lpf_final_settling_steps; /* adi,fagc-lpf-final-settling-steps */ | /* Fast AGC - Lock Level (Lock Level is set via slow AGC inner high threshold) */ |
uint32_t fagc_lmt_final_settling_steps; /* adi,fagc-lmt-final-settling-steps */ | uint8_t fagc_lock_level_lmt_gain_increase_en; /* adi,fagc-lock-level-lmt-gain-increase-enable */ |
uint32_t fagc_final_overrange_count; /* adi,fagc-final-overrange-count */ | uint32_t fagc_lock_level_gain_increase_upper_limit; /* adi,fagc-lock-level-gain-increase-upper-limit */ |
/* Fast AGC - Final Power Test */ | /* Fast AGC - Peak Detectors and Final Settling */ |
uint8_t fagc_gain_increase_after_gain_lock_en; /* adi,fagc-gain-increase-after-gain-lock-enable */ | uint32_t fagc_lpf_final_settling_steps; /* adi,fagc-lpf-final-settling-steps */ |
/* Fast AGC - Unlocking the Gain */ | uint32_t fagc_lmt_final_settling_steps; /* adi,fagc-lmt-final-settling-steps */ |
uint32_t fagc_gain_index_type_after_exit_rx_mode; /* adi,fagc-gain-index-type-after-exit-rx-mode */ | uint32_t fagc_final_overrange_count; /* adi,fagc-final-overrange-count */ |
uint8_t fagc_use_last_lock_level_for_set_gain_en; /* adi,fagc-use-last-lock-level-for-set-gain-enable */ | /* Fast AGC - Final Power Test */ |
uint8_t fagc_rst_gla_stronger_sig_thresh_exceeded_en; /* adi,fagc-rst-gla-stronger-sig-thresh-exceeded-enable */ | uint8_t fagc_gain_increase_after_gain_lock_en; /* adi,fagc-gain-increase-after-gain-lock-enable */ |
uint32_t fagc_optimized_gain_offset; /* adi,fagc-optimized-gain-offset */ | /* Fast AGC - Unlocking the Gain */ |
uint32_t fagc_rst_gla_stronger_sig_thresh_above_ll; /* adi,fagc-rst-gla-stronger-sig-thresh-above-ll */ | uint32_t fagc_gain_index_type_after_exit_rx_mode; /* adi,fagc-gain-index-type-after-exit-rx-mode */ |
uint8_t fagc_rst_gla_engergy_lost_sig_thresh_exceeded_en; /* adi,fagc-rst-gla-engergy-lost-sig-thresh-exceeded-enable */ | uint8_t fagc_use_last_lock_level_for_set_gain_en; /* adi,fagc-use-last-lock-level-for-set-gain-enable */ |
uint8_t fagc_rst_gla_engergy_lost_goto_optim_gain_en; /* adi,fagc-rst-gla-engergy-lost-goto-optim-gain-enable */ | uint8_t fagc_rst_gla_stronger_sig_thresh_exceeded_en; /* adi,fagc-rst-gla-stronger-sig-thresh-exceeded-enable */ |
uint32_t fagc_rst_gla_engergy_lost_sig_thresh_below_ll; /* adi,fagc-rst-gla-engergy-lost-sig-thresh-below-ll */ | uint32_t fagc_optimized_gain_offset; /* adi,fagc-optimized-gain-offset */ |
uint32_t fagc_energy_lost_stronger_sig_gain_lock_exit_cnt; /* adi,fagc-energy-lost-stronger-sig-gain-lock-exit-cnt */ | uint32_t fagc_rst_gla_stronger_sig_thresh_above_ll; /* adi,fagc-rst-gla-stronger-sig-thresh-above-ll */ |
uint8_t fagc_rst_gla_large_adc_overload_en; /* adi,fagc-rst-gla-large-adc-overload-enable */ | uint8_t fagc_rst_gla_engergy_lost_sig_thresh_exceeded_en; /* adi,fagc-rst-gla-engergy-lost-sig-thresh-exceeded-enable */ |
uint8_t fagc_rst_gla_large_lmt_overload_en; /* adi,fagc-rst-gla-large-lmt-overload-enable */ | uint8_t fagc_rst_gla_engergy_lost_goto_optim_gain_en; /* adi,fagc-rst-gla-engergy-lost-goto-optim-gain-enable */ |
uint8_t fagc_rst_gla_en_agc_pulled_high_en; /* adi,fagc-rst-gla-en-agc-pulled-high-enable */ | uint32_t fagc_rst_gla_engergy_lost_sig_thresh_below_ll; /* adi,fagc-rst-gla-engergy-lost-sig-thresh-below-ll */ |
uint32_t fagc_rst_gla_if_en_agc_pulled_high_mode; /* adi,fagc-rst-gla-if-en-agc-pulled-high-mode */ | uint32_t fagc_energy_lost_stronger_sig_gain_lock_exit_cnt; /* adi,fagc-energy-lost-stronger-sig-gain-lock-exit-cnt */ |
uint32_t fagc_power_measurement_duration_in_state5; /* adi,fagc-power-measurement-duration-in-state5 */ | uint8_t fagc_rst_gla_large_adc_overload_en; /* adi,fagc-rst-gla-large-adc-overload-enable */ |
/* RSSI Control */ | uint8_t fagc_rst_gla_large_lmt_overload_en; /* adi,fagc-rst-gla-large-lmt-overload-enable */ |
uint32_t rssi_delay; /* adi,rssi-delay */ | uint8_t fagc_rst_gla_en_agc_pulled_high_en; /* adi,fagc-rst-gla-en-agc-pulled-high-enable */ |
uint32_t rssi_duration; /* adi,rssi-duration */ | uint32_t fagc_rst_gla_if_en_agc_pulled_high_mode; /* adi,fagc-rst-gla-if-en-agc-pulled-high-mode */ |
uint8_t rssi_restart_mode; /* adi,rssi-restart-mode */ | uint32_t fagc_power_measurement_duration_in_state5; /* adi,fagc-power-measurement-duration-in-state5 */ |
uint8_t rssi_unit_is_rx_samples_enable; /* adi,rssi-unit-is-rx-samples-enable */ | /* RSSI Control */ |
uint32_t rssi_wait; /* adi,rssi-wait */ | uint32_t rssi_delay; /* adi,rssi-delay */ |
/* Aux ADC Control */ | uint32_t rssi_duration; /* adi,rssi-duration */ |
uint32_t aux_adc_decimation; /* adi,aux-adc-decimation */ | uint8_t rssi_restart_mode; /* adi,rssi-restart-mode */ |
uint32_t aux_adc_rate; /* adi,aux-adc-rate */ | uint8_t rssi_unit_is_rx_samples_enable; /* adi,rssi-unit-is-rx-samples-enable */ |
/* AuxDAC Control */ | uint32_t rssi_wait; /* adi,rssi-wait */ |
uint8_t aux_dac_manual_mode_enable; /* adi,aux-dac-manual-mode-enable */ | /* Aux ADC Control */ |
uint32_t aux_dac1_default_value_mV; /* adi,aux-dac1-default-value-mV */ | uint32_t aux_adc_decimation; /* adi,aux-adc-decimation */ |
uint8_t aux_dac1_active_in_rx_enable; /* adi,aux-dac1-active-in-rx-enable */ | uint32_t aux_adc_rate; /* adi,aux-adc-rate */ |
uint8_t aux_dac1_active_in_tx_enable; /* adi,aux-dac1-active-in-tx-enable */ | /* AuxDAC Control */ |
uint8_t aux_dac1_active_in_alert_enable; /* adi,aux-dac1-active-in-alert-enable */ | uint8_t aux_dac_manual_mode_enable; /* adi,aux-dac-manual-mode-enable */ |
uint32_t aux_dac1_rx_delay_us; /* adi,aux-dac1-rx-delay-us */ | uint32_t aux_dac1_default_value_mV; /* adi,aux-dac1-default-value-mV */ |
uint32_t aux_dac1_tx_delay_us; /* adi,aux-dac1-tx-delay-us */ | uint8_t aux_dac1_active_in_rx_enable; /* adi,aux-dac1-active-in-rx-enable */ |
uint32_t aux_dac2_default_value_mV; /* adi,aux-dac2-default-value-mV */ | uint8_t aux_dac1_active_in_tx_enable; /* adi,aux-dac1-active-in-tx-enable */ |
uint8_t aux_dac2_active_in_rx_enable; /* adi,aux-dac2-active-in-rx-enable */ | uint8_t aux_dac1_active_in_alert_enable; /* adi,aux-dac1-active-in-alert-enable */ |
uint8_t aux_dac2_active_in_tx_enable; /* adi,aux-dac2-active-in-tx-enable */ | uint32_t aux_dac1_rx_delay_us; /* adi,aux-dac1-rx-delay-us */ |
uint8_t aux_dac2_active_in_alert_enable; /* adi,aux-dac2-active-in-alert-enable */ | uint32_t aux_dac1_tx_delay_us; /* adi,aux-dac1-tx-delay-us */ |
uint32_t aux_dac2_rx_delay_us; /* adi,aux-dac2-rx-delay-us */ | uint32_t aux_dac2_default_value_mV; /* adi,aux-dac2-default-value-mV */ |
uint32_t aux_dac2_tx_delay_us; /* adi,aux-dac2-tx-delay-us */ | uint8_t aux_dac2_active_in_rx_enable; /* adi,aux-dac2-active-in-rx-enable */ |
/* Temperature Sensor Control */ | uint8_t aux_dac2_active_in_tx_enable; /* adi,aux-dac2-active-in-tx-enable */ |
uint32_t temp_sense_decimation; /* adi,temp-sense-decimation */ | uint8_t aux_dac2_active_in_alert_enable; /* adi,aux-dac2-active-in-alert-enable */ |
uint16_t temp_sense_measurement_interval_ms; /* adi,temp-sense-measurement-interval-ms */ | uint32_t aux_dac2_rx_delay_us; /* adi,aux-dac2-rx-delay-us */ |
int8_t temp_sense_offset_signed; /* adi,temp-sense-offset-signed */ | uint32_t aux_dac2_tx_delay_us; /* adi,aux-dac2-tx-delay-us */ |
uint8_t temp_sense_periodic_measurement_enable; /* adi,temp-sense-periodic-measurement-enable */ | /* Temperature Sensor Control */ |
/* Control Out Setup */ | uint32_t temp_sense_decimation; /* adi,temp-sense-decimation */ |
uint8_t ctrl_outs_enable_mask; /* adi,ctrl-outs-enable-mask */ | uint16_t temp_sense_measurement_interval_ms; /* adi,temp-sense-measurement-interval-ms */ |
uint8_t ctrl_outs_index; /* adi,ctrl-outs-index */ | int8_t temp_sense_offset_signed; /* adi,temp-sense-offset-signed */ |
/* External LNA Control */ | uint8_t temp_sense_periodic_measurement_enable; /* adi,temp-sense-periodic-measurement-enable */ |
uint32_t elna_settling_delay_ns; /* adi,elna-settling-delay-ns */ | /* Control Out Setup */ |
uint32_t elna_gain_mdB; /* adi,elna-gain-mdB */ | uint8_t ctrl_outs_enable_mask; /* adi,ctrl-outs-enable-mask */ |
uint32_t elna_bypass_loss_mdB; /* adi,elna-bypass-loss-mdB */ | uint8_t ctrl_outs_index; /* adi,ctrl-outs-index */ |
uint8_t elna_rx1_gpo0_control_enable; /* adi,elna-rx1-gpo0-control-enable */ | /* External LNA Control */ |
uint8_t elna_rx2_gpo1_control_enable; /* adi,elna-rx2-gpo1-control-enable */ | uint32_t elna_settling_delay_ns; /* adi,elna-settling-delay-ns */ |
/* Digital Interface Control */ | uint32_t elna_gain_mdB; /* adi,elna-gain-mdB */ |
uint8_t pp_tx_swap_enable; /* adi,pp-tx-swap-enable */ | uint32_t elna_bypass_loss_mdB; /* adi,elna-bypass-loss-mdB */ |
uint8_t pp_rx_swap_enable; /* adi,pp-rx-swap-enable */ | uint8_t elna_rx1_gpo0_control_enable; /* adi,elna-rx1-gpo0-control-enable */ |
uint8_t tx_channel_swap_enable; /* adi,tx-channel-swap-enable */ | uint8_t elna_rx2_gpo1_control_enable; /* adi,elna-rx2-gpo1-control-enable */ |
uint8_t rx_channel_swap_enable; /* adi,rx-channel-swap-enable */ | uint8_t elna_gaintable_all_index_enable; /* adi,elna-gaintable-all-index-enable */ |
uint8_t rx_frame_pulse_mode_enable; /* adi,rx-frame-pulse-mode-enable */ | /* Digital Interface Control */ |
uint8_t two_t_two_r_timing_enable; /* adi,2t2r-timing-enable */ | uint8_t digital_interface_tune_skip_mode; /* adi,digital-interface-tune-skip-mode */ |
uint8_t invert_data_bus_enable; /* adi,invert-data-bus-enable */ | uint8_t digital_interface_tune_fir_disable; /* adi,digital-interface-tune-fir-disable */ |
uint8_t invert_data_clk_enable; /* adi,invert-data-clk-enable */ | uint8_t pp_tx_swap_enable; /* adi,pp-tx-swap-enable */ |
uint8_t fdd_alt_word_order_enable; /* adi,fdd-alt-word-order-enable */ | uint8_t pp_rx_swap_enable; /* adi,pp-rx-swap-enable */ |
uint8_t invert_rx_frame_enable; /* adi,invert-rx-frame-enable */ | uint8_t tx_channel_swap_enable; /* adi,tx-channel-swap-enable */ |
uint8_t fdd_rx_rate_2tx_enable; /* adi,fdd-rx-rate-2tx-enable */ | uint8_t rx_channel_swap_enable; /* adi,rx-channel-swap-enable */ |
uint8_t swap_ports_enable; /* adi,swap-ports-enable */ | uint8_t rx_frame_pulse_mode_enable; /* adi,rx-frame-pulse-mode-enable */ |
uint8_t single_data_rate_enable; /* adi,single-data-rate-enable */ | uint8_t two_t_two_r_timing_enable; /* adi,2t2r-timing-enable */ |
uint8_t lvds_mode_enable; /* adi,lvds-mode-enable */ | uint8_t invert_data_bus_enable; /* adi,invert-data-bus-enable */ |
uint8_t half_duplex_mode_enable; /* adi,half-duplex-mode-enable */ | uint8_t invert_data_clk_enable; /* adi,invert-data-clk-enable */ |
uint8_t single_port_mode_enable; /* adi,single-port-mode-enable */ | uint8_t fdd_alt_word_order_enable; /* adi,fdd-alt-word-order-enable */ |
uint8_t full_port_enable; /* adi,full-port-enable */ | uint8_t invert_rx_frame_enable; /* adi,invert-rx-frame-enable */ |
uint8_t full_duplex_swap_bits_enable; /* adi,full-duplex-swap-bits-enable */ | uint8_t fdd_rx_rate_2tx_enable; /* adi,fdd-rx-rate-2tx-enable */ |
uint32_t delay_rx_data; /* adi,delay-rx-data */ | uint8_t swap_ports_enable; /* adi,swap-ports-enable */ |
uint32_t rx_data_clock_delay; /* adi,rx-data-clock-delay */ | uint8_t single_data_rate_enable; /* adi,single-data-rate-enable */ |
uint32_t rx_data_delay; /* adi,rx-data-delay */ | uint8_t lvds_mode_enable; /* adi,lvds-mode-enable */ |
uint32_t tx_fb_clock_delay; /* adi,tx-fb-clock-delay */ | uint8_t half_duplex_mode_enable; /* adi,half-duplex-mode-enable */ |
uint32_t tx_data_delay; /* adi,tx-data-delay */ | uint8_t single_port_mode_enable; /* adi,single-port-mode-enable */ |
uint32_t lvds_bias_mV; /* adi,lvds-bias-mV */ | uint8_t full_port_enable; /* adi,full-port-enable */ |
uint8_t lvds_rx_onchip_termination_enable; /* adi,lvds-rx-onchip-termination-enable */ | uint8_t full_duplex_swap_bits_enable; /* adi,full-duplex-swap-bits-enable */ |
uint8_t rx1rx2_phase_inversion_en; /* adi,rx1-rx2-phase-inversion-enable */ | uint32_t delay_rx_data; /* adi,delay-rx-data */ |
/* Tx Monitor Control */ | uint32_t rx_data_clock_delay; /* adi,rx-data-clock-delay */ |
uint32_t low_high_gain_threshold_mdB; /* adi,txmon-low-high-thresh */ | uint32_t rx_data_delay; /* adi,rx-data-delay */ |
uint32_t low_gain_dB; /* adi,txmon-low-gain */ | uint32_t tx_fb_clock_delay; /* adi,tx-fb-clock-delay */ |
uint32_t high_gain_dB; /* adi,txmon-high-gain */ | uint32_t tx_data_delay; /* adi,tx-data-delay */ |
uint8_t tx_mon_track_en; /* adi,txmon-dc-tracking-enable */ | uint32_t lvds_bias_mV; /* adi,lvds-bias-mV */ |
uint8_t one_shot_mode_en; /* adi,txmon-one-shot-mode-enable */ | uint8_t lvds_rx_onchip_termination_enable; /* adi,lvds-rx-onchip-termination-enable */ |
uint32_t tx_mon_delay; /* adi,txmon-delay */ | uint8_t rx1rx2_phase_inversion_en; /* adi,rx1-rx2-phase-inversion-enable */ |
uint32_t tx_mon_duration; /* adi,txmon-duration */ | uint8_t lvds_invert1_control; /* adi,lvds-invert1-control */ |
uint32_t tx1_mon_front_end_gain; /* adi,txmon-1-front-end-gain */ | uint8_t lvds_invert2_control; /* adi,lvds-invert2-control */ |
uint32_t tx2_mon_front_end_gain; /* adi,txmon-2-front-end-gain */ | /* GPO Control */ |
uint32_t tx1_mon_lo_cm; /* adi,txmon-1-lo-cm */ | uint8_t gpo0_inactive_state_high_enable; /* adi,gpo0-inactive-state-high-enable */ |
uint32_t tx2_mon_lo_cm; /* adi,txmon-2-lo-cm */ | uint8_t gpo1_inactive_state_high_enable; /* adi,gpo1-inactive-state-high-enable */ |
/* GPIO definitions */ | uint8_t gpo2_inactive_state_high_enable; /* adi,gpo2-inactive-state-high-enable */ |
int32_t gpio_resetb; /* reset-gpios */ | uint8_t gpo3_inactive_state_high_enable; /* adi,gpo3-inactive-state-high-enable */ |
/* MCS Sync */ | uint8_t gpo0_slave_rx_enable; /* adi,gpo0-slave-rx-enable */ |
int32_t gpio_sync; /* sync-gpios */ | uint8_t gpo0_slave_tx_enable; /* adi,gpo0-slave-tx-enable */ |
int32_t gpio_cal_sw1; /* cal-sw1-gpios */ | uint8_t gpo1_slave_rx_enable; /* adi,gpo1-slave-rx-enable */ |
int32_t gpio_cal_sw2; /* cal-sw2-gpios */ | uint8_t gpo1_slave_tx_enable; /* adi,gpo1-slave-tx-enable */ |
}AD9361_InitParam; | uint8_t gpo2_slave_rx_enable; /* adi,gpo2-slave-rx-enable */ |
| uint8_t gpo2_slave_tx_enable; /* adi,gpo2-slave-tx-enable */ |
| uint8_t gpo3_slave_rx_enable; /* adi,gpo3-slave-rx-enable */ |
| uint8_t gpo3_slave_tx_enable; /* adi,gpo3-slave-tx-enable */ |
| uint8_t gpo0_rx_delay_us; /* adi,gpo0-rx-delay-us */ |
| uint8_t gpo0_tx_delay_us; /* adi,gpo0-tx-delay-us */ |
| uint8_t gpo1_rx_delay_us; /* adi,gpo1-rx-delay-us */ |
| uint8_t gpo1_tx_delay_us; /* adi,gpo1-tx-delay-us */ |
| uint8_t gpo2_rx_delay_us; /* adi,gpo2-rx-delay-us */ |
| uint8_t gpo2_tx_delay_us; /* adi,gpo2-tx-delay-us */ |
| uint8_t gpo3_rx_delay_us; /* adi,gpo3-rx-delay-us */ |
| uint8_t gpo3_tx_delay_us; /* adi,gpo3-tx-delay-us */ |
| /* Tx Monitor Control */ |
| uint32_t low_high_gain_threshold_mdB; /* adi,txmon-low-high-thresh */ |
| uint32_t low_gain_dB; /* adi,txmon-low-gain */ |
| uint32_t high_gain_dB; /* adi,txmon-high-gain */ |
| uint8_t tx_mon_track_en; /* adi,txmon-dc-tracking-enable */ |
| uint8_t one_shot_mode_en; /* adi,txmon-one-shot-mode-enable */ |
| uint32_t tx_mon_delay; /* adi,txmon-delay */ |
| uint32_t tx_mon_duration; /* adi,txmon-duration */ |
| uint32_t tx1_mon_front_end_gain; /* adi,txmon-1-front-end-gain */ |
| uint32_t tx2_mon_front_end_gain; /* adi,txmon-2-front-end-gain */ |
| uint32_t tx1_mon_lo_cm; /* adi,txmon-1-lo-cm */ |
| uint32_t tx2_mon_lo_cm; /* adi,txmon-2-lo-cm */ |
| /* GPIO definitions */ |
| int32_t gpio_resetb; /* reset-gpios */ |
| /* MCS Sync */ |
| int32_t gpio_sync; /* sync-gpios */ |
| int32_t gpio_cal_sw1; /* cal-sw1-gpios */ |
| int32_t gpio_cal_sw2; /* cal-sw2-gpios */ |
| /* External LO clocks */ |
| uint32_t (*ad9361_rfpll_ext_recalc_rate)(struct refclk_scale *clk_priv); |
| int32_t (*ad9361_rfpll_ext_round_rate)(struct refclk_scale *clk_priv, uint32_t rate); |
| int32_t (*ad9361_rfpll_ext_set_rate)(struct refclk_scale *clk_priv, uint32_t rate); |
| }AD9361_InitParam; |
</code> | </code> |
| |
==== AD9361 Doxygen Documentation ==== | ==== AD9361 Doxygen Documentation ==== |
| |
http://analogdevicesinc.github.io/ad9361/ | http://analogdevicesinc.github.io/no-OS/ |
| |
===== Generic Platform ===== | ===== Generic Platform ===== |
| |
==== Required Software ==== | ==== Required Software ==== |
* We're upgrade the Xilinx tools on every release. The supported version number can be found in our [[https://github.com/analogdevicesinc/hdl/tree/master | git repository ]]. | {{page>./../../../../../resources/no-os/build}} |
{{page>./../../../../../resources/fpga/xilinx/software_setup}} | |
==== Console Commands Driver ==== | ==== Console Commands Driver ==== |
| |
* **ZC702 HDL Reference Design for Vivado: **https://github.com/analogdevicesinc/hdl/tree/master/projects/fmcomms2/zc702 | * **ZC702 HDL Reference Design for Vivado: **https://github.com/analogdevicesinc/hdl/tree/master/projects/fmcomms2/zc702 |
* **ZC706 HDL Reference Design for Vivado: **https://github.com/analogdevicesinc/hdl/tree/master/projects/fmcomms2/zc706 | * **ZC706 HDL Reference Design for Vivado: **https://github.com/analogdevicesinc/hdl/tree/master/projects/fmcomms2/zc706 |
* **AC701 HDL Reference Design for Vivado: **https://github.com/analogdevicesinc/hdl/tree/master/projects/fmcomms2/ac701 | |
* **KC705 HDL Reference Design for Vivado: **https://github.com/analogdevicesinc/hdl/tree/master/projects/fmcomms2/kc705 | * **KC705 HDL Reference Design for Vivado: **https://github.com/analogdevicesinc/hdl/tree/master/projects/fmcomms2/kc705 |
* **VC707 HDL Reference Design for Vivado: **https://github.com/analogdevicesinc/hdl/tree/master/projects/fmcomms2/vc707 | * **VC707 HDL Reference Design for Vivado: **https://github.com/analogdevicesinc/hdl/tree/master/projects/fmcomms2/vc707 |
| |
* **ML605 HDL Reference Design for ISE: ** https://github.com/analogdevicesinc/fpgahdl_xilinx/tree/master/cf_ad9361_ml605 | |
</WRAP> | </WRAP> |
| |