This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-fmcomms2-ebz:quickstart [28 May 2019 21:13] – Add networking info Travis Collins | resources:eval:user-guides:ad-fmcomms2-ebz:quickstart [02 Mar 2021 07:48] (current) – [SoCkit + ARRADIO] Stefan-Robert Raus | ||
---|---|---|---|
Line 18: | Line 18: | ||
| [[xilinx> | | [[xilinx> | ||
| [[http:// | | [[http:// | ||
- | | [[http:// | + | | [[http:// |
| [[https:// | | [[https:// | ||
Line 34: | Line 34: | ||
| [[xilinx> | | [[xilinx> | ||
| [[http:// | | [[http:// | ||
- | | [[http:// | + | | [[http:// |
Line 68: | Line 68: | ||
^ ^ MSEL0 ^ MSEL1 ^ MSEL2 ^ MSEL3 ^ MSEL4 ^ CODEC_SEL ^ | ^ ^ MSEL0 ^ MSEL1 ^ MSEL2 ^ MSEL3 ^ MSEL4 ^ CODEC_SEL ^ | ||
- | |**POS**| | + | |**POS**| |
{{: | {{: | ||
Line 90: | Line 90: | ||
| Carrier | | Carrier | ||
+ | For our standard evaluation system most users boot from the SD cards placed either on the SOM or carrier board. For the **ADRV1CRR-BOB** carrier or carriers without SD card slots be sure to set S1 to 0. | ||
===== Networking ===== | ===== Networking ===== | ||
By default, all SD cards for the prototyping platform (not TES) are configured for DHCP networking over their Ethernet interfaces. If you want to change the networking interfaces to use static addresses, which is required for directly connected Ethernet cables without DHCP servers in the loop, a [[https:// | By default, all SD cards for the prototyping platform (not TES) are configured for DHCP networking over their Ethernet interfaces. If you want to change the networking interfaces to use static addresses, which is required for directly connected Ethernet cables without DHCP servers in the loop, a [[https:// | ||
+ | |||
+ | To update the IP address of the board you must be logged into the board over UART or JTAG or Ethernet. | ||
From the development board or SOM itself run the following with the desired IP address: | From the development board or SOM itself run the following with the desired IP address: |