This is an old revision of the document!
The Quick Start Guides provide a simple step by step instruction on how to do an initial system setup for the AD-FMCOMMS2/3/4/5-EBZ boards on various FPGA development boards. They will discuss how to program the bitstream, run a no-OS program or boot a Linux distribution.
The AD-FMCOMMS2/3/4/5-EBZ is, by definition a “FPGA mezzanine card” (FMC), that means it needs a carrier to plug into. The carriers we support are:
The supported OS are:
In most carriers, the AD-FMCOMMS2/3/4-EBZ board connects to the LPC connector (unless otherwise noted). The AD-FMCOMMS5-EBZ board is a dual FMC connector, and requires either FMC connectors (which can be either LPC + LPC). The carrier setup requires power, UART (115200), ethernet (Linux), HDMI (if available) and/or JTAG (no-OS) connections. A few typical setups are shown below.
Early versions of the ZC702 carriers need to work around AR# 51438, PG signal does not assert by default errata.