Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
resources:eval:user-guides:ad-fmcomms2-ebz:quickstart:zynqmp [20 Dec 2017 22:10] – escape // Neil Wilson | resources:eval:user-guides:ad-fmcomms2-ebz:quickstart:zynqmp [06 Sep 2022 14:39] – Update the boot flow and logs Liviu-Mihai Iacob |
---|
| |
* [[resources:eval:user-guides:ad-fmcomms2-ebz:software:linux:zynqmp|Building the ZynqMP / MPSoC Linux kernel and devicetrees from source]] | * [[resources:eval:user-guides:ad-fmcomms2-ebz:software:linux:zynqmp|Building the ZynqMP / MPSoC Linux kernel and devicetrees from source]] |
| * [[resources:tools-software:linux-software:build-the-zynqmp-boot-image|How to build the ZynqMP boot image BOOT.BIN]] |
| |
===== Required Software ===== | ===== Required Software ===== |
</hidden> | </hidden> |
| |
* SD Card 8GB imaged using the instructions here: [[resources:tools-software:linux-software:zynq_images|Zynq & Altera SoC Quick Start Guide]] | * SD Card 16GB or more imaged using the instructions here: [[resources:tools-software:linux-software:zynq_images|Zynq & Altera SoC Quick Start Guide]] |
* A UART terminal (Putty/Tera Term/Minicom, etc.), Baud rate 115200 (8N1). | * A UART terminal (Putty/Tera Term/Minicom, etc.), Baud rate 115200 (8N1). |
| |
==== Setup ==== | ==== Setup ==== |
| |
- Image the SD card with the latest available image | - Image the SD card with the latest available image: [[:resources:tools-software:linux-software:adi-kuiper_images:release_notes]] |
- Download **FMCOMMS2-3 ZCU102 Rev 1.0.zip** | - Copy the following files into the BOOT partition of the SD Card (Replace files if they already exist). |
- Unzip FMCOMMS2-3 ZCU102 Rev 1.0.zip | - **Image** file from **zynqmp-common**. |
- Copy BOOT.BIN, Image, system.dtb and uEnv.txt to the root of the SD Card FAT32 partition. (Replace files if they already exist) | - **BOOT.BIN** from **zynqmp-zcu102-rev10-ad936x-fmcomms2-3-4**. |
| - **system.dtb** from **zynqmp-zcu102-rev10-ad9361-fmcomms2-3**. |
- Safely eject the SD Card | - Safely eject the SD Card |
| |
| |
<WRAP box bggreen><wrap info>This specifies any shell prompt running on the target</wrap> | <WRAP box bggreen><wrap info>This specifies any shell prompt running on the target</wrap> |
<xterm> | <code> |
Xilinx Zynq MP First Stage Boot Loader | Xilinx Zynq MP First Stage Boot Loader |
Release 2017.2 Oct 19 2017 - 09:35:44 | Release 2021.1 Aug 3 2022 - 10:34:27 |
NOTICE: ATF running on XCZU9EG/silicon v4/RTL5.1 at 0xfffea000, with PMU firmware | NOTICE: BL31: v2.4(release):xilinx-v2020.2-2024-g0a69763 |
NOTICE: BL31: Secure code at 0x0 | NOTICE: BL31: Built : 07:48:38, Sep 23 2021 |
NOTICE: BL31: Non secure code at 0x8000000 | PMUFW: v1.1 |
NOTICE: BL31: v1.3(release):f9b244b | |
NOTICE: BL31: Built : 09:35:17, Oct 19 2017 | |
| |
| |
U-Boot 2016.07 (Dec 16 2016 - 15:04:11 -0700) Xilinx ZynqMP ZCU102 revB | U-Boot 2018.01-21439-gd244ce5 (Jul 29 2021 - 16:37:20 +0100) Xilinx ZynqMP ZCU102 revA, Build: jenkins-development-build_uboot-1 |
| |
I2C: ready | I2C: ready |
DRAM: 4 GiB | DRAM: 4 GiB |
EL Level: EL2 | EL Level: EL2 |
Chip ID: xczu9eg | Chip ID: zu9eg |
MMC: sdhci@ff170000: 0 | MMC: sdhci@ff170000: 0 (SD) |
Using default environment | *** Warning - bad CRC, using default environment |
| |
In: serial@ff000000 | In: serial@ff000000 |
Err: serial@ff000000 | Err: serial@ff000000 |
Bootmode: LVL_SHFT_SD_MODE1 | Bootmode: LVL_SHFT_SD_MODE1 |
SCSI: SATA link 0 timeout. | Net: ZYNQ GEM: ff0e0000, phyaddr 15, interface rgmii-id |
SATA link 1 timeout. | |
AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl SATA mode | |
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst | |
scanning bus for devices... | |
Found 0 device(s). | |
Net: ZYNQ GEM: ff0e0000, phyaddr 12, interface rgmii-id | |
| |
Warning: ethernet@ff0e0000 using MAC address from ROM | Warning: ethernet@ff0e0000 using MAC address from ROM |
eth0: ethernet@ff0e0000 | eth0: ethernet@ff0e0000 |
Hit any key to stop autoboot: 0 | Hit any key to stop autoboot: 0 |
switch to partitions #0, OK | switch to partitions #0, OK |
mmc0 is current device | mmc0 is current device |
Device: sdhci@ff170000 | Device: sdhci@ff170000 |
Manufacturer ID: 3 | Manufacturer ID: 89 |
OEM: 5344 | OEM: 303 |
Name: SL08G | Name: NCard |
Tran Speed: 50000000 | Tran Speed: 50000000 |
Rd Block Len: 512 | Rd Block Len: 512 |
SD version 3.0 | SD version 3.0 |
High Capacity: Yes | High Capacity: Yes |
Capacity: 7.4 GiB | Capacity: 14.6 GiB |
Bus Width: 4-bit | Bus Width: 4-bit |
Erase Group Size: 512 Bytes | Erase Group Size: 512 Bytes |
reading uEnv.txt | reading uEnv.txt |
301 bytes read in 9 ms (32.2 KiB/s) | 407 bytes read in 21 ms (18.6 KiB/s) |
Loaded environment from uEnv.txt | Loaded environment from uEnv.txt |
Importing environment from SD ... | Importing environment from SD ... |
Running uenvcmd ... | Running uenvcmd ... |
reading Image | Copying Linux from SD to RAM... |
14209536 bytes read in 991 ms (13.7 MiB/s) | ** No boot file defined ** |
reading system.dtb | |
43396 bytes read in 48 ms (882.8 KiB/s) | |
Wrong Image Format for bootm command | |
ERROR: can't get kernel image! | |
reading system.dtb | reading system.dtb |
43396 bytes read in 49 ms (864.3 KiB/s) | 57875 bytes read in 30 ms (1.8 MiB/s) |
reading Image | reading Image |
14209536 bytes read in 987 ms (13.7 MiB/s) | 32514560 bytes read in 2188 ms (14.2 MiB/s) |
## Flattened Device Tree blob at 04000000 | ## Flattened Device Tree blob at 04000000 |
Booting using the fdt blob at 0x4000000 | Booting using the fdt blob at 0x4000000 |
Loading Device Tree to 000000000fff2000, end 000000000ffff983 ... OK | Loading Device Tree to 000000000ffee000, end 000000000ffff212 ... OK |
| |
Starting kernel ... | Starting kernel ... |
| |
[ 0.000000] Booting Linux on physical CPU 0x0 | [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] |
[ 0.000000] Linux version 4.9.0-12434-g7f38ed6 (michael@mhenneri-D04) (gcc version 4.9.2 20140904 (prerelease) (crosstool-NG linaro-1.13.1-4.9-2014.09 - Linaro GCC 4.9-2014.09) ) #387 SMP Thu Oct 19 10 | [ 0.000000] Linux version 5.10.0-98248-g1bbe32fa5182 (jenkins@romlxbuild1.adlk.analog.com) (aarch64-xilinx-linux-gcc.real (GCC) 10.2.0, GNU ld (GNU Binutils) 2.35.0.20200730) #1143 SMP Wed Aug 3 18:38:55 IST 2022 |
:59:25 CEST 2017 | [ 0.000000] Machine model: ZynqMP ZCU102 Rev1.0 |
[ 0.000000] Boot CPU: AArch64 Processor [410fd034] | |
[ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8') | [ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8') |
[ 0.000000] bootconsole [cdns0] enabled | [ 0.000000] printk: bootconsole [cdns0] enabled |
[ 0.000000] efi: Getting EFI parameters from FDT: | |
[ 0.000000] efi: UEFI not found. | [ 0.000000] efi: UEFI not found. |
[ 0.000000] cma: Reserved 128 MiB at 0x0000000078000000 | [ 0.000000] cma: Reserved 256 MiB at 0x0000000070000000 |
| [ 0.000000] Zone ranges: |
| [ 0.000000] DMA [mem 0x0000000000000000-0x000000003fffffff] |
| [ 0.000000] DMA32 [mem 0x0000000040000000-0x00000000ffffffff] |
| [ 0.000000] Normal [mem 0x0000000100000000-0x000000087fffffff] |
| [ 0.000000] Movable zone start for each node |
| [ 0.000000] Early memory node ranges |
| [ 0.000000] node 0: [mem 0x0000000000000000-0x000000007fffffff] |
| [ 0.000000] node 0: [mem 0x0000000800000000-0x000000087fffffff] |
| [ 0.000000] Initmem setup node 0 [mem 0x0000000000000000-0x000000087fffffff] |
[ 0.000000] psci: probing for conduit method from DT. | [ 0.000000] psci: probing for conduit method from DT. |
[ 0.000000] psci: PSCIv1.0 detected in firmware. | [ 0.000000] psci: PSCIv1.1 detected in firmware. |
[ 0.000000] psci: Using standard PSCI v0.2 function IDs | [ 0.000000] psci: Using standard PSCI v0.2 function IDs |
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported. | [ 0.000000] psci: MIGRATE_INFO_TYPE not supported. |
[ 0.000000] percpu: Embedded 21 pages/cpu @ffffffc87ff62000 s47488 r8192 d30336 u86016 | [ 0.000000] psci: SMC Calling Convention v1.2 |
| [ 0.000000] percpu: Embedded 22 pages/cpu s49496 r8192 d32424 u90112 |
[ 0.000000] Detected VIPT I-cache on CPU0 | [ 0.000000] Detected VIPT I-cache on CPU0 |
[ 0.000000] CPU features: enabling workaround for ARM erratum 845719 | [ 0.000000] CPU features: detected: ARM erratum 845719 |
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 1034240 | [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1034240 |
[ 0.000000] Kernel command line: earlycon=cdns,mmio,0xFF000000,115200n8 console=ttyPS0,115200n8 root=/dev/mmcblk0p2 rw rootwait cma=128M root=/dev/mmcblk0p2 rw rootwait | [ 0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlycon rootfstype=ext4 rootwait clk_ignore_unused cpuidle.off=1 root=/dev/mmcblk0p2 rw rootwait |
[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes) | [ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear) |
[ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes) | [ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) |
[ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes) | [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off |
[ 0.000000] software IO TLB [mem 0x73fff000-0x77fff000] (64MB) mapped at [ffffffc073fff000-ffffffc077ffefff] | [ 0.000000] software IO TLB: mapped [mem 0x000000003bfff000-0x000000003ffff000] (64MB) |
[ 0.000000] Memory: 3918800K/4194304K available (9148K kernel code, 628K rwdata, 3524K rodata, 512K init, 389K bss, 144432K reserved, 131072K cma-reserved) | [ 0.000000] Memory: 3761568K/4194304K available (15488K kernel code, 1672K rwdata, 11952K rodata, 2496K init, 507K bss, 170592K reserved, 262144K cma-reserved) |
[ 0.000000] Virtual kernel memory layout: | [ 0.000000] rcu: Hierarchical RCU implementation. |
[ 0.000000] modules : 0xffffff8000000000 - 0xffffff8008000000 ( 128 MB) | [ 0.000000] rcu: RCU event tracing is enabled. |
[ 0.000000] vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000 ( 250 GB) | [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4. |
[ 0.000000] .text : 0xffffff8008080000 - 0xffffff8008970000 ( 9152 KB) | [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. |
[ 0.000000] .rodata : 0xffffff8008970000 - 0xffffff8008cf0000 ( 3584 KB) | [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 |
[ 0.000000] .init : 0xffffff8008cf0000 - 0xffffff8008d70000 ( 512 KB) | [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 |
[ 0.000000] .data : 0xffffff8008d70000 - 0xffffff8008e0d200 ( 629 KB) | |
[ 0.000000] .bss : 0xffffff8008e0d200 - 0xffffff8008e6e7e0 ( 390 KB) | |
[ 0.000000] fixed : 0xffffffbefe7fd000 - 0xffffffbefec00000 ( 4108 KB) | |
[ 0.000000] PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000 ( 16 MB) | |
[ 0.000000] vmemmap : 0xffffffbf00000000 - 0xffffffc000000000 ( 4 GB maximum) | |
[ 0.000000] 0xffffffbf00000000 - 0xffffffbf1dc00000 ( 476 MB actual) | |
[ 0.000000] memory : 0xffffffc000000000 - 0xffffffc880000000 ( 34816 MB) | |
[ 0.000000] Hierarchical RCU implementation. | |
[ 0.000000] Build-time adjustment of leaf fanout to 64. | |
[ 0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4. | |
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=64, nr_cpu_ids=4 | |
[ 0.000000] NR_IRQS:64 nr_irqs:64 0 | |
[ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000 | [ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000 |
[ 0.000000] GIC: Using split EOI/Deactivate mode | [ 0.000000] GIC: Using split EOI/Deactivate mode |
[ 0.000000] arm_arch_timer: Architected cp15 timer(s) running at 99.99MHz (phys). | [ 0.000000] random: get_random_bytes called from start_kernel+0x31c/0x550 with crng_init=0 |
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x171015c90f, max_idle_ns: 440795203080 ns | [ 0.000000] arch_timer: cp15 timer(s) running at 100.00MHz (phys). |
[ 0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511101ns | [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x171024e7e0, max_idle_ns: 440795205315 ns |
[ 0.008295] Console: colour dummy device 80x25 | [ 0.000003] sched_clock: 56 bits at 100MHz, resolution 10ns, wraps every 4398046511100ns |
[ 0.012559] Calibrating delay loop (skipped), value calculated using timer frequency.. 199.99 BogoMIPS (lpj=399996) | [ 0.008485] Console: colour dummy device 80x25 |
[ 0.022922] pid_max: default: 32768 minimum: 301 | [ 0.012484] Calibrating delay loop (skipped), value calculated using timer frequency.. 200.00 BogoMIPS (lpj=400000) |
[ 0.027604] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes) | [ 0.022841] pid_max: default: 32768 minimum: 301 |
[ 0.034174] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes) | [ 0.027558] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) |
[ 0.041780] ASID allocator initialised with 65536 entries | [ 0.034789] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) |
[ 0.047510] zynqmp_plat_init Power management API v0.3 | [ 0.043434] rcu: Hierarchical SRCU implementation. |
[ 0.052529] EFI services will not be available. | [ 0.047568] EFI services will not be available. |
[ 0.057272] Detected VIPT I-cache on CPU1 | [ 0.051941] smp: Bringing up secondary CPUs ... |
[ 0.057298] CPU1: Booted secondary processor [410fd034] | [ 0.056663] Detected VIPT I-cache on CPU1 |
[ 0.057558] Detected VIPT I-cache on CPU2 | [ 0.056702] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] |
[ 0.057576] CPU2: Booted secondary processor [410fd034] | [ 0.057074] Detected VIPT I-cache on CPU2 |
[ 0.057833] Detected VIPT I-cache on CPU3 | [ 0.057098] CPU2: Booted secondary processor 0x0000000002 [0x410fd034] |
[ 0.057851] CPU3: Booted secondary processor [410fd034] | [ 0.057438] Detected VIPT I-cache on CPU3 |
[ 0.057886] Brought up 4 CPUs | [ 0.057461] CPU3: Booted secondary processor 0x0000000003 [0x410fd034] |
[ 0.088169] SMP: Total of 4 processors activated. | [ 0.057508] smp: Brought up 1 node, 4 CPUs |
[ 0.092846] CPU features: detected feature: 32-bit EL0 Support | [ 0.091780] SMP: Total of 4 processors activated. |
[ 0.098643] CPU: All CPU(s) started at EL2 | [ 0.096452] CPU features: detected: 32-bit EL0 Support |
[ 0.102714] alternatives: patching kernel code | [ 0.101555] CPU features: detected: CRC32 instructions |
[ 0.107781] devtmpfs: initialized | [ 0.106694] CPU: All CPU(s) started at EL2 |
[ 0.116903] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns | [ 0.110736] alternatives: patching kernel code |
[ 0.129064] xor: measuring software checksum speed | [ 0.116198] devtmpfs: initialized |
[ 0.173723] 8regs : 2376.000 MB/sec | [ 0.124524] Registered cp15_barrier emulation handler |
[ 0.213751] 8regs_prefetch: 2170.000 MB/sec | [ 0.124575] Registered setend emulation handler |
[ 0.258121] 32regs : 2632.000 MB/sec | [ 0.128552] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns |
[ 0.298150] 32regs_prefetch: 2459.000 MB/sec | [ 0.138133] futex hash table entries: 1024 (order: 4, 65536 bytes, linear) |
[ 0.302575] xor: using function: 32regs (2632.000 MB/sec) | [ 0.151555] pinctrl core: initialized pinctrl subsystem |
[ 0.308002] pinctrl core: initialized pinctrl subsystem | [ 0.152221] NET: Registered protocol family 16 |
[ 0.313634] NET: Registered protocol family 16 | [ 0.156648] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations |
[ 0.333916] cpuidle: using governor menu | [ 0.162630] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations |
[ 0.338003] Failed to initialise IOMMU /amba/smmu@fd800000 | [ 0.170358] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations |
[ 0.343528] vdso: 2 pages (1 code @ ffffff8008977000, 1 data @ ffffff8008d74000) | [ 0.178166] audit: initializing netlink subsys (disabled) |
[ 0.350728] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. | [ 0.183626] audit: type=2000 audit(0.116:1): state=initialized audit_enabled=0 res=1 |
[ 0.357908] DMA: preallocated 256 KiB pool for atomic allocations | [ 0.183979] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. |
[ 0.378184] reset_zynqmp reset-controller: Xilinx zynqmp reset driver probed | [ 0.197991] ASID allocator initialised with 65536 entries |
[ 0.385780] ARM CCI_400_r1 PMU driver probed[ 0.392280] zynqmp-pinctrl ff180000.pinctrl: zynqmp pinctrl initialized | [ 0.223864] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages |
[ 0.418915] HugeTLB registered 2 MB page size, pre-allocated 0 pages | [ 0.224919] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages |
[ 0.493298] raid6: int64x1 gen() 458 MB/s | [ 0.231589] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages |
[ 0.565380] raid6: int64x1 xor() 478 MB/s | [ 0.238259] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages |
[ 0.637451] raid6: int64x2 gen() 676 MB/s | [ 1.303615] DRBG: Continuing without Jitter RNG |
[ 0.709444] raid6: int64x2 xor() 597 MB/s | [ 1.381660] raid6: neonx8 gen() 2149 MB/s |
[ 0.781506] raid6: int64x4 gen() 981 MB/s | [ 1.449715] raid6: neonx8 xor() 1599 MB/s |
[ 0.853541] raid6: int64x4 xor() 733 MB/s | [ 1.517778] raid6: neonx4 gen() 2189 MB/s |
[ 0.925631] raid6: int64x8 gen() 1021 MB/s | [ 1.585824] raid6: neonx4 xor() 1567 MB/s |
[ 0.997656] raid6: int64x8 xor() 722 MB/s | [ 1.653890] raid6: neonx2 gen() 2072 MB/s |
[ 1.069712] raid6: neonx1 gen() 732 MB/s | [ 1.721945] raid6: neonx2 xor() 1437 MB/s |
[ 1.141750] raid6: neonx1 xor() 755 MB/s | [ 1.790018] raid6: neonx1 gen() 1775 MB/s |
[ 1.213798] raid6: neonx2 gen() 1135 MB/s | [ 1.858055] raid6: neonx1 xor() 1220 MB/s |
[ 1.285853] raid6: neonx2 xor() 1005 MB/s | [ 1.926112] raid6: int64x8 gen() 1438 MB/s |
[ 1.357898] raid6: neonx4 gen() 1507 MB/s | [ 1.994171] raid6: int64x8 xor() 771 MB/s |
[ 1.429929] raid6: neonx4 xor() 1176 MB/s | [ 2.062250] raid6: int64x4 gen() 1599 MB/s |
[ 1.501973] raid6: neonx8 gen() 1541 MB/s | [ 2.130301] raid6: int64x4 xor() 820 MB/s |
[ 1.574022] raid6: neonx8 xor() 1190 MB/s | [ 2.198373] raid6: int64x2 gen() 1399 MB/s |
[ 1.578099] raid6: using algorithm neonx8 gen() 1541 MB/s | [ 2.266418] raid6: int64x2 xor() 749 MB/s |
[ 1.583461] raid6: .... xor() 1190 MB/s, rmw enabled | [ 2.334489] raid6: int64x1 gen() 1031 MB/s |
[ 1.588392] raid6: using intx1 recovery algorithm | [ 2.402538] raid6: int64x1 xor() 517 MB/s |
[ 1.594670] SCSI subsystem initialized | [ 2.402576] raid6: using algorithm neonx4 gen() 2189 MB/s |
[ 1.598408] usbcore: registered new interface driver usbfs | [ 2.406525] raid6: .... xor() 1567 MB/s, rmw enabled |
[ 1.603737] usbcore: registered new interface driver hub | [ 2.411459] raid6: using neon recovery algorithm |
[ 1.609016] usbcore: registered new device driver usb | [ 2.416472] iommu: Default domain type: Translated |
[ 1.614058] media: Linux media interface: v0.10 | [ 2.421095] SCSI subsystem initialized |
[ 1.618517] Linux video capture interface: v2.00 | [ 2.424756] usbcore: registered new interface driver usbfs |
[ 1.623102] pps_core: LinuxPPS API ver. 1 registered | [ 2.430082] usbcore: registered new interface driver hub |
[ 1.628010] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> | [ 2.435360] usbcore: registered new device driver usb |
[ 1.637103] PTP clock support registered | [ 2.440484] mc: Linux media interface: v0.10 |
[ 1.641000] EDAC MC: Ver: 3.0.0 | [ 2.444611] videodev: Linux video capture interface: v2.00 |
[ 1.644344] FPGA manager framework | [ 2.450102] EDAC MC: Ver: 3.0.0 |
[ 1.647673] fpga-region fpga-full: FPGA Region probed | [ 2.453528] zynqmp-ipi-mbox mailbox@ff990400: Registered ZynqMP IPI mbox with TX/RX channels. |
[ 1.652667] Advanced Linux Sound Architecture Driver Initialized. | [ 2.462023] jesd204: found 0 devices and 0 topologies |
[ 1.658903] Bluetooth: Core ver 2.22 | [ 2.466674] FPGA manager framework |
[ 1.662303] NET: Registered protocol family 31 | [ 2.470150] Advanced Linux Sound Architecture Driver Initialized. |
[ 1.666703] Bluetooth: HCI device and connection manager initialized | [ 2.476459] Bluetooth: Core ver 2.22 |
[ 1.673021] Bluetooth: HCI socket layer initialized | [ 2.479633] NET: Registered protocol family 31 |
[ 1.677863] Bluetooth: L2CAP socket layer initialized | [ 2.484033] Bluetooth: HCI device and connection manager initialized |
[ 1.682893] Bluetooth: SCO socket layer initialized | [ 2.490350] Bluetooth: HCI socket layer initialized |
[ 1.688281] clocksource: Switched to clocksource arch_sys_counter | [ 2.495192] Bluetooth: L2CAP socket layer initialized |
[ 1.694241] VFS: Disk quotas dquot_6.6.0 | [ 2.500216] Bluetooth: SCO socket layer initialized |
[ 1.698105] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) | [ 2.505419] clocksource: Switched to clocksource arch_sys_counter |
[ 1.709332] NET: Registered protocol family 2 | [ 2.511214] VFS: Disk quotas dquot_6.6.0 |
[ 1.713813] TCP established hash table entries: 32768 (order: 6, 262144 bytes) | [ 2.515052] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) |
[ 1.721090] TCP bind hash table entries: 32768 (order: 7, 524288 bytes) | [ 2.525762] NET: Registered protocol family 2 |
[ 1.727982] TCP: Hash tables configured (established 32768 bind 32768) | [ 2.526501] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear) |
[ 1.734348] UDP hash table entries: 2048 (order: 4, 65536 bytes) | [ 2.534679] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear) |
[ 1.740351] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes) | [ 2.542709] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear) |
[ 1.746835] NET: Registered protocol family 1 | [ 2.550170] TCP: Hash tables configured (established 32768 bind 32768) |
[ 1.751191] RPC: Registered named UNIX socket transport module. | [ 2.556330] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear) |
[ 1.756924] RPC: Registered udp transport module. | [ 2.562993] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear) |
[ 1.761586] RPC: Registered tcp transport module. | [ 2.570161] NET: Registered protocol family 1 |
[ 1.766257] RPC: Registered tcp NFSv4.1 backchannel transport module. | [ 2.574635] RPC: Registered named UNIX socket transport module. |
[ 1.773094] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available | [ 2.580231] RPC: Registered udp transport module. |
[ 1.781328] futex hash table entries: 1024 (order: 5, 131072 bytes) | [ 2.584895] RPC: Registered tcp transport module. |
[ 1.787442] audit: initializing netlink subsys (disabled) | [ 2.589564] RPC: Registered tcp NFSv4.1 backchannel transport module. |
[ 1.792782] audit: type=2000 audit(1.736:1): initialized | [ 2.596554] PCI: CLS 0 bytes, default 64 |
[ 1.798555] workingset: timestamp_bits=62 max_order=20 bucket_order=0 | [ 2.600273] hw perfevents: no interrupt-affinity property for /pmu, guessing. |
[ 1.805477] NFS: Registering the id_resolver key type | [ 2.607124] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available |
[ 1.810353] Key type id_resolver registered | [ 2.615493] Initialise system trusted keyrings |
[ 1.814492] Key type id_legacy registered | [ 2.619163] workingset: timestamp_bits=62 max_order=20 bucket_order=0 |
[ 1.818475] nfs4filelayout_init: NFSv4 File Layout Driver Registering... | [ 2.626064] NFS: Registering the id_resolver key type |
[ 1.825144] jffs2: version 2.2. (NAND) (SUMMARY) �© 2001-2006 Red Hat, Inc. | [ 2.630493] Key type id_resolver registered |
[ 1.836396] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247) | [ 2.634630] Key type id_legacy registered |
[ 1.843592] io scheduler noop registered | [ 2.638627] nfs4filelayout_init: NFSv4 File Layout Driver Registering... |
[ 1.847483] io scheduler deadline registered | [ 2.645289] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc. |
[ 1.851726] io scheduler cfq registered (default) | [ 2.652460] fuse: init (API version 7.32) |
[ 1.856952] nwl-pcie fd0e0000.pcie: Link is DOWN | [ 2.692910] NET: Registered protocol family 38 |
[ 1.861415] OF: PCI: host bridge /amba/pcie@fd0e0000 ranges: | [ 2.692953] xor: measuring software checksum speed |
[ 1.867017] OF: PCI: MEM 0xe0000000..0xefffffff -> 0xe0000000 | [ 2.700640] 8regs : 2363 MB/sec |
[ 1.872890] OF: PCI: MEM 0x600000000..0x7ffffffff -> 0x600000000 | [ 2.704306] 32regs : 2799 MB/sec |
[ 1.879124] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00 | [ 2.709249] arm64_neon : 2380 MB/sec |
[ 1.885175] pci_bus 0000:00: root bus resource [bus 00-ff] | [ 2.709442] xor: using function: 32regs (2799 MB/sec) |
[ 1.890621] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff] | [ 2.714464] Key type asymmetric registered |
[ 1.897455] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref] | [ 2.718526] Asymmetric key parser 'x509' registered |
[ 1.905185] pci 0000:00:00.0: PCI bridge to [bus 01-0c] | [ 2.723387] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 248) |
[ 1.911528] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed | [ 2.730724] io scheduler mq-deadline registered |
[ 1.918053] Write failed gate address:1000f02 | [ 2.735220] io scheduler kyber registered |
[ 1.922301] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success | [ 2.764706] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled |
[ 1.929279] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success | [ 2.769571] cacheinfo: Unable to detect cache hierarchy for CPU 0 |
[ 1.936192] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success | [ 2.775675] brd: module loaded |
[ 1.943111] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success | [ 2.779959] loop: module loaded |
[ 1.950030] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success | [ 2.780252] Registered mathworks_ip class |
[ 1.956953] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success | [ 2.783724] libphy: Fixed MDIO Bus: probed |
[ 1.963872] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success | [ 2.786672] tun: Universal TUN/TAP device driver, 1.6 |
[ 1.970790] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success | [ 2.790765] CAN device driver interface |
[ 1.977742] zynqmp_pm firmware: Power management API v0.3 | [ 2.795331] usbcore: registered new interface driver asix |
[ 2.015848] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled | [ 2.799893] usbcore: registered new interface driver ax88179_178a |
2.032580] console [ttyPS0] enabled0 at MMIO 0xff000000 (irq = 39, base_baud = 6249999) is a xuartps | [ 2.805922] usbcore: registered new interface driver cdc_ether |
[ 2.032580] console [ttyPS0] enabled | [ 2.811716] usbcore: registered new interface driver net1080 |
[ 2.039540] bootconsole [cdns0] disabled | [ 2.817337] usbcore: registered new interface driver cdc_subset |
[ 2.039540] bootconsole [cdns0] disabled | [ 2.823218] usbcore: registered new interface driver zaurus |
[ 2.047964] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 40, base_baud = 6249999) is a xuartps | [ 2.828771] usbcore: registered new interface driver cdc_ncm |
[ 2.057130] [drm] Initialized | [ 2.835212] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver |
[ 2.060434] [drm] load() is defered & will be called again | [ 2.840850] ehci-pci: EHCI PCI platform driver |
[ 2.066516] xilinx-drm-dp-sub fd4aa000.dp_sub: Xilinx DisplayPort Subsystem is probed | [ 2.845685] usbcore: registered new interface driver uas |
[ 2.074419] Unable to detect cache hierarchy from DT for CPU 0 | [ 2.850564] usbcore: registered new interface driver usb-storage |
[ 2.084703] brd: module loaded | [ 2.856553] usbcore: registered new interface driver usbserial_generic |
[ 2.090388] loop: module loaded | [ 2.863005] usbserial: USB Serial support registered for generic |
[ 2.094184] ahci-ceva fd0c0000.ahci: couldn't get PHY in node ahci: -517 | [ 2.868976] usbcore: registered new interface driver ftdi_sio |
[ 2.100937] mtdoops: mtd device (mtddev=name/number) must be supplied | [ 2.874680] usbserial: USB Serial support registered for FTDI USB Serial Device |
[ 2.108622] m25p80 spi0.0: SPI-NOR-UniqueID 10000023536359160025001817101588af | [ 2.881952] usbcore: registered new interface driver upd78f0730 |
[ 2.115762] m25p80 spi0.0: found n25q512a, expected m25p80 | [ 2.887832] usbserial: USB Serial support registered for upd78f0730 |
[ 2.121340] m25p80 spi0.0: n25q512a (131072 Kbytes) | [ 2.895526] rtc_zynqmp ffa60000.rtc: registered as rtc0 |
[ 2.126148] 4 ofpart partitions found on MTD device spi0.0 | [ 2.899252] rtc_zynqmp ffa60000.rtc: setting system clock to 2022-09-06T11:23:39 UTC (1662463419) |
[ 2.131599] Creating 4 MTD partitions on "spi0.0": | [ 2.908113] i2c /dev entries driver |
[ 2.136376] 0x000000000000-0x000000100000 : "qspi-fsbl-uboot" | [ 2.913394] usbcore: registered new interface driver uvcvideo |
[ 2.142594] 0x000000100000-0x000000600000 : "qspi-linux" | [ 2.917227] USB Video Class driver (1.1.1) |
[ 2.148287] 0x000000600000-0x000000620000 : "qspi-device-tree" | [ 2.922790] Bluetooth: HCI UART driver ver 2.3 |
[ 2.154478] 0x000000620000-0x000000c00000 : "qspi-rootfs" | [ 2.925710] Bluetooth: HCI UART protocol H4 registered |
[ 2.161044] libphy: Fixed MDIO Bus: probed | [ 2.930808] Bluetooth: HCI UART protocol BCSP registered |
[ 2.166010] tun: Universal TUN/TAP device driver, 1.6 | [ 2.936096] Bluetooth: HCI UART protocol LL registered |
[ 2.170974] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com> | [ 2.941187] Bluetooth: HCI UART protocol ATH3K registered |
[ 2.177241] CAN device driver interface | [ 2.946563] Bluetooth: HCI UART protocol Three-wire (H5) registered |
[ 2.184002] macb ff0e0000.ethernet: Not enabling partial store and forward | [ 2.952812] Bluetooth: HCI UART protocol Intel registered |
[ 2.191184] libphy: MACB_mii_bus: probed | [ 2.958151] Bluetooth: HCI UART protocol QCA registered |
[ 2.196867] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 23 (00:0a:35:03:6f:71) | [ 2.963354] usbcore: registered new interface driver bcm203x |
[ 2.206608] TI DP83867 ff0e0000.etherne:0c: attached PHY driver [TI DP83867] (mii_bus:phy_addr=ff0e0000.etherne:0c, irq=-1) | [ 2.968973] usbcore: registered new interface driver bpa10x |
[ 2.218237] usbcore: registered new interface driver asix | [ 2.974512] usbcore: registered new interface driver bfusb |
[ 2.223588] usbcore: registered new interface driver ax88179_178a | [ 2.979961] usbcore: registered new interface driver btusb |
[ 2.229647] usbcore: registered new interface driver cdc_ether | [ 2.985427] usbcore: registered new interface driver ath3k |
[ 2.235462] usbcore: registered new interface driver net1080 | [ 2.990910] EDAC MC: ECC not enabled |
[ 2.241104] usbcore: registered new interface driver cdc_subset | [ 2.994535] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT) |
[ 2.247007] usbcore: registered new interface driver zaurus | [ 3.006844] sdhci: Secure Digital Host Controller Interface driver |
[ 2.252574] usbcore: registered new interface driver cdc_ncm | [ 3.012641] sdhci: Copyright(c) Pierre Ossman |
[ 2.260581] usbcore: registered new interface driver uas | [ 3.016959] sdhci-pltfm: SDHCI platform and OF driver helper |
[ 2.265836] usbcore: registered new interface driver usb-storage | [ 3.023026] ledtrig-cpu: registered to indicate activity on CPUs |
[ 2.272059] mousedev: PS/2 mouse device common for all mice | [ 3.028565] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping .... |
[ 2.277915] rtc_zynqmp ffa60000.rtc: rtc core: registered ffa60000.rtc as rtc0 | [ 3.034994] zynqmp_firmware_probe Platform Management API v1.1 |
[ 2.285081] i2c /dev entries driver | [ 3.040751] zynqmp_firmware_probe Trustzone version v1.0 |
[ 2.290599] usbcore: registered new interface driver uvcvideo | [ 3.078127] zynqmp-pinctrl firmware:zynqmp-firmware:pinctrl: zynqmp pinctrl initialized |
[ 2.296262] USB Video Class driver (1.1.1) | [ 3.124554] zynqmp-aes firmware:zynqmp-firmware:zynqmp-aes: will run requests pump with realtime priority |
[ 2.300823] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer at ffffff800a010000 with timeout 10s | [ 3.140222] alg: No test for xilinx-keccak-384 (zynqmp-keccak-384) |
[ 2.309866] Bluetooth: HCI UART driver ver 2.3 | [ 3.140932] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa) |
[ 2.314223] Bluetooth: HCI UART protocol H4 registered | [ 3.146446] usbcore: registered new interface driver usbhid |
[ 2.319341] Bluetooth: HCI UART protocol BCSP registered | [ 3.151833] usbhid: USB HID core driver |
[ 2.324639] Bluetooth: HCI UART protocol LL registered | [ 3.162357] axi_sysid 85000000.axi-sysid-0: AXI System ID core version (1.01.a) found |
[ 2.329757] Bluetooth: HCI UART protocol ATH3K registered | [ 3.164705] axi_sysid 85000000.axi-sysid-0: [fmcomms2] on [zcu102] git branch <hdl_2021_r1> git <6a6c5acc8ec422c068c7787cdeb5b0ee4ae1aa51> clean [2022-05-20 17:39:13] UTC |
[ 2.335138] Bluetooth: HCI UART protocol Three-wire (H5) registered | [ 3.180217] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered |
[ 2.341424] Bluetooth: HCI UART protocol Intel registered | [ 3.186586] usbcore: registered new interface driver snd-usb-audio |
[ 2.346803] Bluetooth: HCI UART protocol Broadcom registered | [ 3.194020] pktgen: Packet Generator for packet performance testing. Version: 2.75 |
[ 2.352412] Bluetooth: HCI UART protocol QCA registered | [ 3.200241] Initializing XFRM netlink socket |
[ 2.357653] usbcore: registered new interface driver bcm203x | [ 3.204059] NET: Registered protocol family 10 |
[ 2.363292] usbcore: registered new interface driver bpa10x | [ 3.208793] Segment Routing with IPv6 |
[ 2.368849] usbcore: registered new interface driver bfusb | [ 3.212168] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver |
[ 2.374315] usbcore: registered new interface driver btusb | [ 3.218242] NET: Registered protocol family 17 |
[ 2.379755] Bluetooth: Generic Bluetooth SDIO driver ver 0.1 | [ 3.222335] NET: Registered protocol family 15 |
[ 2.385442] usbcore: registered new interface driver ath3k | [ 3.226824] can: controller area network core |
[ 2.390975] EDAC MC: ECC not enabled | [ 3.231087] NET: Registered protocol family 29 |
[ 2.394619] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT) | [ 3.235474] can: raw protocol |
[ 2.407548] sdhci: Secure Digital Host Controller Interface driver | [ 3.238410] can: broadcast manager protocol |
[ 2.413643] sdhci: Copyright(c) Pierre Ossman | [ 3.242565] can: netlink gateway - max_hops=1 |
[ 2.417981] sdhci-pltfm: SDHCI platform and OF driver helper | [ 3.246958] Bluetooth: RFCOMM TTY layer initialized |
[ 2.425963] ledtrig-cpu: registered to indicate activity on CPUs | [ 3.251738] Bluetooth: RFCOMM socket layer initialized |
[ 2.431988] usbcore: registered new interface driver usbhid | [ 3.256847] Bluetooth: RFCOMM ver 1.11 |
[ 2.437479] usbhid: USB HID core driver | [ 3.260557] Bluetooth: BNEP (Ethernet Emulation) ver 1.3 |
[ 2.441982] ad9361 spi32766.0: ad9361_probe : enter (ad9361) | [ 3.265828] Bluetooth: BNEP filters: protocol multicast |
[ 2.451251] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered | [ 3.271022] Bluetooth: BNEP socket layer initialized |
[ 2.458173] xilinx-dp-snd-pcm dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed | [ 3.275949] Bluetooth: HIDP (Human Interface Emulation) ver 1.2 |
[ 2.465416] xilinx-dp-snd-pcm dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed | [ 3.281833] Bluetooth: HIDP socket layer initialized |
[ 2.475104] Write failed to divider address:fd1a007c | [ 3.286900] 9pnet: Installing 9P2000 support |
[ 2.480308] xilinx-dp-snd-codec dp_snd_codec0: Xilinx DisplayPort Sound Codec probed | [ 3.291011] NET: Registered protocol family 36 |
[ 2.488349] xilinx-dp-snd-card dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok | [ 3.295427] Key type dns_resolver registered |
[ 2.498020] xilinx-dp-snd-card dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok | [ 3.299869] registered taskstats version 1 |
[ 2.507912] xilinx-dp-snd-card dp_snd_card: Xilinx DisplayPort Sound Card probed | [ 3.303725] Loading compiled-in X.509 certificates |
[ 2.515314] pktgen: Packet Generator for packet performance testing. Version: 2.75 | [ 3.308834] Btrfs loaded, crc32c=crc32c-generic |
[ 2.523003] Netfilter messages via NETLINK v0.30. | [ 3.321662] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 48, base_baud = 6249999) is a xuartps |
[ 2.527729] ip_tables: (C) 2000-2006 Netfilter Core Team | [ 3.330682] printk: console [ttyPS0] enabled |
[ 2.532999] Initializing XFRM netlink socket | [ 3.330682] printk: console [ttyPS0] enabled |
[ 2.537441] NET: Registered protocol family 10 | [ 3.334977] printk: bootconsole [cdns0] disabled |
[ 2.542258] ip6_tables: (C) 2000-2006 Netfilter Core Team | [ 3.334977] printk: bootconsole [cdns0] disabled |
[ 2.547607] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver | [ 3.344620] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 49, base_baud = 6249999) is a xuartps |
[ 2.553797] NET: Registered protocol family 17 | [ 3.357820] of-fpga-region fpga-full: FPGA Region probed |
[ 2.558167] NET: Registered protocol family 15 | [ 3.364788] nwl-pcie fd0e0000.pcie: host bridge /axi/pcie@fd0e0000 ranges: |
[ 2.562593] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this. | [ 3.371686] nwl-pcie fd0e0000.pcie: MEM 0x00e0000000..0x00efffffff -> 0x00e0000000 |
[ 2.575517] Ebtables v2.0 registered | [ 3.379693] nwl-pcie fd0e0000.pcie: MEM 0x0600000000..0x07ffffffff -> 0x0600000000 |
[ 2.579108] can: controller area network core (rev 20120528 abi 9) | [ 3.387762] nwl-pcie fd0e0000.pcie: Link is DOWN |
[ 2.585265] NET: Registered protocol family 29 | [ 3.392522] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00 |
[ 2.589672] can: raw protocol (rev 20120528) | [ 3.398706] pci_bus 0000:00: root bus resource [bus 00-ff] |
[ 2.593918] can: broadcast manager protocol (rev 20161123 t) | [ 3.404187] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff] |
[ 2.599563] can: netlink gateway (rev 20130117) max_hops=1 | [ 3.411056] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref] |
[ 2.605084] Bluetooth: RFCOMM TTY layer initialized | [ 3.418560] pci 0000:00:00.0: [10ee:d021] type 01 class 0x060400 |
[ 2.609895] Bluetooth: RFCOMM socket layer initialized | [ 3.424617] pci 0000:00:00.0: PME# supported from D0 D1 D2 D3hot |
[ 2.615018] Bluetooth: RFCOMM ver 1.11 | [ 3.435384] pci 0000:00:00.0: PCI bridge to [bus 01-0c] |
[ 2.618745] Bluetooth: BNEP (Ethernet Emulation) ver 1.3 | [ 3.441391] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success |
[ 2.624038] Bluetooth: BNEP filters: protocol multicast | [ 3.448578] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success |
[ 2.629252] Bluetooth: BNEP socket layer initialized | [ 3.455747] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success |
[ 2.634194] Bluetooth: HIDP (Human Interface Emulation) ver 1.2 | [ 3.462922] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success |
[ 2.640099] Bluetooth: HIDP socket layer initialized | [ 3.470090] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success |
[ 2.645194] 9pnet: Installing 9P2000 support | [ 3.477263] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success |
[ 2.649388] Key type dns_resolver registered | [ 3.484430] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success |
[ 2.654078] registered taskstats version 1 | [ 3.491596] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success |
[ 2.658470] Btrfs loaded, crc32c=crc32c-generic | [ 3.498992] xilinx-zynqmp-dpdma fd4c0000.dma-controller: Xilinx DPDMA engine is probed |
[ 2.672950] PLL: shutdown | [ 3.507572] ahci-ceva fd0c0000.ahci: supply ahci not found, using dummy regulator |
[ 2.675574] [drm] load() is defered & will be called again | [ 3.515112] ahci-ceva fd0c0000.ahci: supply phy not found, using dummy regulator |
[ 2.681633] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:8 protocol:4 pll_locked:yes | [ 3.523616] ad9361 spi1.0: ad9361_probe : enter (ad9361) |
[ 2.689628] xilinx-drm-dp fd4a0000.dp: device found, version 4.010 | [ 3.529870] ad9361 spi1.0: No GPIOs defined for ext band ctrl |
[ 2.695724] xilinx-drm-dp fd4a0000.dp: Display Port, version 1.0200 (tx) | [ 3.545027] random: fast init done |
[ 2.702755] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:3 protocol:2 pll_locked:yes | [ 3.760865] ad9361 spi1.0: ad9361_probe : AD936x Rev 0 successfully initialized |
[ 2.710553] ahci-ceva fd0c0000.ahci: AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl platform mode | [ 3.768944] spi-nor spi0.0: SPI-NOR-UniqueID 2eae9700180c001300980596158d |
[ 2.719447] ahci-ceva fd0c0000.ahci: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst | [ 3.775732] spi-nor spi0.0: found mt25qu512a, expected m25p80 |
[ 2.729782] scsi host0: ahci-ceva | [ 3.782144] spi-nor spi0.0: trying to lock already unlocked area |
[ 2.733211] scsi host1: ahci-ceva | [ 3.788148] spi-nor spi0.0: mt25qu512a (131072 Kbytes) |
[ 2.736573] ata1: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x100 irq 36 | [ 3.793311] 4 fixed-partitions partitions found on MTD device spi0.0 |
[ 2.744407] ata2: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x180 irq 36 | [ 3.799654] Creating 4 MTD partitions on "spi0.0": |
[ 2.754766] xilinx-psgtr fd400000.zynqmp_phy: Lane:2 type:0 protocol:3 pll_locked:yes | [ 3.804438] 0x000000000000-0x000000100000 : "qspi-fsbl-uboot" |
[ 2.784444] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller | [ 3.810953] 0x000000100000-0x000000600000 : "qspi-linux" |
[ 2.789857] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1 | [ 3.816918] 0x000000600000-0x000000620000 : "qspi-device-tree" |
[ 2.797694] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x02010810 | [ 3.823419] 0x000000620000-0x000000c00000 : "qspi-rootfs" |
[ 2.806327] xhci-hcd xhci-hcd.0.auto: irq 221, io mem 0xfe200000 | [ 3.832024] macb ff0e0000.ethernet: Not enabling partial store and forward |
[ 2.812401] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 | [ 3.839556] libphy: MACB_mii_bus: probed |
[ 2.819111] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 | [ 3.844359] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 30 (00:0a:35:05:60:78) |
[ 2.826311] usb usb1: Product: xHCI Host Controller | [ 3.854582] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM |
[ 2.831171] usb usb1: Manufacturer: Linux 4.9.0-12434-g7f38ed6 xhci-hcd | [ 3.861146] xilinx-axipmon fd0b0000.perf-monitor: Probed Xilinx APM |
[ 2.837771] usb usb1: SerialNumber: xhci-hcd.0.auto | [ 3.867675] xilinx-axipmon fd490000.perf-monitor: Probed Xilinx APM |
[ 2.842928] hub 1-0:1.0: USB hub found | [ 3.874214] xilinx-axipmon ffa10000.perf-monitor: Probed Xilinx APM |
[ 2.846609] hub 1-0:1.0: 1 port detected | [ 3.884317] pca953x 0-0020: supply vcc not found, using dummy regulator |
[ 2.850655] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller | [ 3.891010] pca953x 0-0020: using no AI |
[ 2.856065] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2 | [ 3.895486] gpio-496 (sel0): hogged as output/low |
[ 2.863810] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003 | [ 3.900390] gpio-497 (sel1): hogged as output/high |
[ 2.870516] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 | [ 3.905378] gpio-498 (sel2): hogged as output/high |
[ 2.877716] usb usb2: Product: xHCI Host Controller | [ 3.910360] gpio-499 (sel3): hogged as output/high |
[ 2.882576] usb usb2: Manufacturer: Linux 4.9.0-12434-g7f38ed6 xhci-hcd | [ 3.915564] pca953x 0-0021: supply vcc not found, using dummy regulator |
[ 2.889172] usb usb2: SerialNumber: xhci-hcd.0.auto | [ 3.922232] pca953x 0-0021: using no AI |
[ 2.894296] hub 2-0:1.0: USB hub found | [ 3.928031] ina2xx 2-0040: power monitor ina226 (Rshunt = 5000 uOhm) |
[ 2.897977] hub 2-0:1.0: 1 port detected | [ 3.935065] ina2xx 2-0041: power monitor ina226 (Rshunt = 5000 uOhm) |
[ 2.902774] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 25 | [ 3.942101] ina2xx 2-0042: power monitor ina226 (Rshunt = 5000 uOhm) |
[ 2.908837] 0-0020 supply vcc not found, using dummy regulator | [ 3.949132] ina2xx 2-0043: power monitor ina226 (Rshunt = 5000 uOhm) |
[ 2.915542] GPIO line 322 (sel0) hogged as output/low | [ 3.956161] ina2xx 2-0044: power monitor ina226 (Rshunt = 5000 uOhm) |
[ 2.920714] GPIO line 323 (sel1) hogged as output/high | [ 3.963199] ina2xx 2-0045: power monitor ina226 (Rshunt = 5000 uOhm) |
[ 2.925971] GPIO line 324 (sel2) hogged as output/high | [ 3.970228] ina2xx 2-0046: power monitor ina226 (Rshunt = 5000 uOhm) |
[ 2.931224] GPIO line 325 (sel3) hogged as output/high | [ 3.977262] ina2xx 2-0047: power monitor ina226 (Rshunt = 5000 uOhm) |
[ 2.936397] pca953x 0-0020: interrupt support not compiled in | [ 3.984347] ina2xx 2-004a: power monitor ina226 (Rshunt = 5000 uOhm) |
[ 2.942137] 0-0021 supply vcc not found, using dummy regulator | [ 3.991379] ina2xx 2-004b: power monitor ina226 (Rshunt = 5000 uOhm) |
[ 2.948496] pca953x 0-0021: interrupt support not compiled in | [ 3.997782] i2c i2c-0: Added multiplexed i2c bus 2 |
[ 2.954961] ina2xx 3-0040: power monitor ina226 (Rshunt = 5000 uOhm) | [ 4.003375] ina2xx 3-0040: power monitor ina226 (Rshunt = 2000 uOhm) |
[ 2.961638] ina2xx 3-0041: power monitor ina226 (Rshunt = 5000 uOhm) | [ 4.010409] ina2xx 3-0041: power monitor ina226 (Rshunt = 5000 uOhm) |
[ 2.968324] ina2xx 3-0042: power monitor ina226 (Rshunt = 5000 uOhm) | [ 4.017451] ina2xx 3-0042: power monitor ina226 (Rshunt = 5000 uOhm) |
[ 2.974997] ina2xx 3-0043: power monitor ina226 (Rshunt = 5000 uOhm) | [ 4.024482] ina2xx 3-0043: power monitor ina226 (Rshunt = 5000 uOhm) |
[ 2.981674] ina2xx 3-0044: power monitor ina226 (Rshunt = 5000 uOhm) | [ 4.031519] ina2xx 3-0044: power monitor ina226 (Rshunt = 5000 uOhm) |
[ 2.988353] ina2xx 3-0045: power monitor ina226 (Rshunt = 5000 uOhm) | [ 4.038557] ina2xx 3-0045: power monitor ina226 (Rshunt = 5000 uOhm) |
[ 2.995026] ina2xx 3-0046: power monitor ina226 (Rshunt = 5000 uOhm) | [ 4.045584] ina2xx 3-0046: power monitor ina226 (Rshunt = 5000 uOhm) |
[ 3.001695] ina2xx 3-0047: power monitor ina226 (Rshunt = 5000 uOhm) | [ 4.052613] ina2xx 3-0047: power monitor ina226 (Rshunt = 5000 uOhm) |
[ 3.008377] ina2xx 3-004a: power monitor ina226 (Rshunt = 5000 uOhm) | [ 4.059015] i2c i2c-0: Added multiplexed i2c bus 3 |
[ 3.015052] ina2xx 3-004b: power monitor ina226 (Rshunt = 5000 uOhm) | [ 4.114980] i2c i2c-0: Added multiplexed i2c bus 4 |
[ 3.021337] i2c i2c-0: Added multiplexed i2c bus 3 | [ 4.119924] i2c i2c-0: Added multiplexed i2c bus 5 |
[ 3.026696] ina2xx 4-0040: power monitor ina226 (Rshunt = 2000 uOhm) | [ 4.124719] pca954x 0-0075: registered 4 multiplexed busses for I2C mux pca9544 |
[ 3.033378] ina2xx 4-0041: power monitor ina226 (Rshunt = 5000 uOhm) | [ 4.132067] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 32 |
[ 3.040062] ina2xx 4-0042: power monitor ina226 (Rshunt = 5000 uOhm) | [ 4.139870] at24 6-0054: supply vcc not found, using dummy regulator |
[ 3.046736] ina2xx 4-0043: power monitor ina226 (Rshunt = 5000 uOhm) | [ 4.146758] at24 6-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write |
[ 3.053408] ina2xx 4-0044: power monitor ina226 (Rshunt = 5000 uOhm) | [ 4.153506] i2c i2c-1: Added multiplexed i2c bus 6 |
[ 3.060088] ina2xx 4-0045: power monitor ina226 (Rshunt = 5000 uOhm) | [ 4.159790] si5341 7-0036: Chip: 5341 Grade: 1 Rev: 1 |
[ 3.066486] ata2: SATA link down (SStatus 0 SControl 330) | [ 4.197775] i2c i2c-1: Added multiplexed i2c bus 7 |
[ 3.066768] ina2xx 4-0046: power monitor ina226 (Rshunt = 5000 uOhm) | [ 4.205453] si570 8-005d: registered, current frequency 300000000 Hz |
[ 3.067173] ina2xx 4-0047: power monitor ina226 (Rshunt = 5000 uOhm) | [ 4.211852] i2c i2c-1: Added multiplexed i2c bus 8 |
[ 3.067191] i2c i2c-0: Added multiplexed i2c bus 4 | [ 4.231656] si570 9-005d: registered, current frequency 148500000 Hz |
[ 3.088296] random: fast init done | [ 4.238059] i2c i2c-1: Added multiplexed i2c bus 9 |
[ 3.092659] ata1: SATA link down (SStatus 0 SControl 330) | [ 4.243109] si5324 10-0069: si5328 probed |
[ 3.097635] i2c i2c-0: Added multiplexed i2c bus 5 | [ 4.309842] si5324 10-0069: si5328 probe successful |
[ 3.097773] i2c i2c-0: Added multiplexed i2c bus 6 | [ 4.314774] i2c i2c-1: Added multiplexed i2c bus 10 |
[ 3.097777] pca954x 0-0075: registered 4 multiplexed busses for I2C mux pca9544 | [ 4.319807] i2c i2c-1: Added multiplexed i2c bus 11 |
[ 3.098668] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 26 | [ 4.324836] i2c i2c-1: Added multiplexed i2c bus 12 |
[ 3.099569] at24 7-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write | [ 4.329872] i2c i2c-1: Added multiplexed i2c bus 13 |
[ 3.099585] i2c i2c-1: Added multiplexed i2c bus 7 | [ 4.334748] pca954x 1-0074: registered 8 multiplexed busses for I2C switch pca9548 |
[ 3.099785] i2c i2c-1: Added multiplexed i2c bus 8 | [ 4.343941] at24 14-0050: supply vcc not found, using dummy regulator |
[ 3.101809] si570 9-005d: registered, current frequency 300000000 Hz | [ 4.350728] at24 14-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write |
[ 3.101826] i2c i2c-1: Added multiplexed i2c bus 9 | [ 4.357475] i2c i2c-1: Added multiplexed i2c bus 14 |
[ 3.115761] si570 10-005d: registered, current frequency 148500000 Hz | [ 4.362511] i2c i2c-1: Added multiplexed i2c bus 15 |
[ 3.115778] i2c i2c-1: Added multiplexed i2c bus 10 | [ 4.367546] i2c i2c-1: Added multiplexed i2c bus 16 |
[ 3.115985] i2c i2c-1: Added multiplexed i2c bus 11 | [ 4.372580] i2c i2c-1: Added multiplexed i2c bus 17 |
[ 3.116117] i2c i2c-1: Added multiplexed i2c bus 12 | [ 4.377614] i2c i2c-1: Added multiplexed i2c bus 18 |
[ 3.116245] i2c i2c-1: Added multiplexed i2c bus 13 | [ 4.382653] i2c i2c-1: Added multiplexed i2c bus 19 |
[ 3.116388] i2c i2c-1: Added multiplexed i2c bus 14 | [ 4.387696] i2c i2c-1: Added multiplexed i2c bus 20 |
[ 3.116392] pca954x 1-0074: registered 8 multiplexed busses for I2C switch pca9548 | [ 4.392735] i2c i2c-1: Added multiplexed i2c bus 21 |
[ 3.117790] at24 15-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write | [ 4.397610] pca954x 1-0075: registered 8 multiplexed busses for I2C switch pca9548 |
[ 3.117806] i2c i2c-1: Added multiplexed i2c bus 15 | [ 4.405217] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 33 |
[ 3.117945] i2c i2c-1: Added multiplexed i2c bus 16 | [ 4.415375] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer with timeout 60s |
[ 3.118081] i2c i2c-1: Added multiplexed i2c bus 17 | [ 4.459408] mmc0: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit |
[ 3.118547] i2c i2c-1: Added multiplexed i2c bus 18 | [ 4.502741] mmc0: new high speed SDHC card at address b368 |
[ 3.118691] i2c i2c-1: Added multiplexed i2c bus 19 | [ 4.508564] mmcblk0: mmc0:b368 NCard 14.6 GiB |
[ 3.118830] i2c i2c-1: Added multiplexed i2c bus 20 | [ 4.514406] mmcblk0: p1 p2 p3 |
[ 3.118974] i2c i2c-1: Added multiplexed i2c bus 21 | [ 5.255248] cf_axi_adc 99020000.cf-ad9361-lpc: ADI AIM (10.01.b) at 0x99020000 mapped to 0x(____ptrval____), probed ADC AD9361 as MASTER |
[ 3.119112] i2c i2c-1: Added multiplexed i2c bus 22 | [ 5.285857] cf_axi_dds 99024000.cf-ad9361-dds-core-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x99024000 mapped to 0x(____ptrval____), probed DDS AD9361 |
[ 3.119117] pca954x 1-0075: registered 8 multiplexed busses for I2C switch pca9548 | [ 5.301580] zynqmp-display fd4a0000.display: vtc bridge property not present |
[ 3.172287] mmc0: SDHCI controller on ff170000.sdhci [ff170000.sdhci] using ADMA 64-bit | [ 5.309785] zynqmp_clk_divider_set_rate() set divider failed for spi1_ref_div1, ret = -13 |
[ 3.172708] ad9361 spi32766.0: ad9361_probe : enter (ad9361) | [ 5.319469] xilinx-dp-snd-codec fd4a0000.display:zynqmp_dp_snd_codec0: Failed to get required clock freq |
[ 3.304741] mmc0: new ultra high speed DDR50 SDHC card at address e624 | [ 5.328966] xilinx-dp-snd-codec: probe of fd4a0000.display:zynqmp_dp_snd_codec0 failed with error -22 |
[ 3.311462] mmcblk0: mmc0:e624 SL08G 7.40 GiB | [ 5.338532] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed |
[ 3.316713] mmcblk0: p1 p2 p3 | [ 5.346700] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed |
[ 3.416956] ad9361 spi32766.0: ad9361_probe : AD936x Rev 2 successfully initialized | [ 5.354967] OF: graph: no port node found in /axi/display@fd4a0000 |
[ 3.435516] cf_axi_dds 99024000.cf-ad9361-dds-core-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.00.b) at 0x99024000 mapped to 0xffffff800a178000, probed DDS AD9361 | [ 5.361363] xlnx-drm xlnx-drm.0: bound fd4a0000.display (ops 0xffffffc010ffd810) |
[ 3.450477] PLL: enable | [ 6.445437] zynqmp-display fd4a0000.display: [drm] Cannot find any crtc or sizes |
[ 3.453191] PLL: shutdown | [ 6.453085] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.display on minor 0 |
[ 3.455891] OF: graph: no port node found in /xilinx_drm | [ 6.460577] zynqmp-display fd4a0000.display: ZynqMP DisplayPort Subsystem driver probed |
[ 3.461122] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). | [ 6.468896] ahci-ceva fd0c0000.ahci: supply ahci not found, using dummy regulator |
[ 3.467715] [drm] No driver support for vblank timestamp query. | [ 6.476444] ahci-ceva fd0c0000.ahci: supply phy not found, using dummy regulator |
[ 3.473635] xilinx-drm xilinx_drm: No connectors reported connected with modes | [ 6.483895] ahci-ceva fd0c0000.ahci: supply target not found, using dummy regulator |
[ 3.480828] [drm] Cannot find any crtc or sizes - going 1024x768 | [ 6.501782] ahci-ceva fd0c0000.ahci: AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl platform mode |
[ 3.492477] Console: switching to colour frame buffer device 128x48 | [ 6.510739] ahci-ceva fd0c0000.ahci: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst |
[ 3.503298] xilinx-drm xilinx_drm: fb0: frame buffer device | [ 6.521288] scsi host0: ahci-ceva |
[ 3.532289] [drm] Initialized xilinx_drm 1.0.0 20130509 on minor 0 | [ 6.524875] scsi host1: ahci-ceva |
[ 4.557574] cf_axi_adc 99020000.cf-ad9361-lpc: ADI AIM (10.00.b) at 0x99020000 mapped to 0xffffff800a4c0000, probed ADC AD9361 as MASTER | [ 6.528305] ata1: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x100 irq 45 |
[ 4.570069] input: gpio-keys as /devices/platform/gpio-keys/input/input0 | [ 6.536221] ata2: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x180 irq 45 |
[ 4.576898] rtc_zynqmp ffa60000.rtc: setting system clock to 2017-04-27 11:03:14 UTC (1493290994) | [ 6.544870] OF: graph: no port node found in /axi/phy@fd400000 |
[ 4.587830] ALSA device list: | [ 6.561006] input: gpio-keys as /devices/platform/gpio-keys/input/input0 |
[ 4.590713] #0: DisplayPort monitor | [ 6.568247] of_cfs_init |
[ 4.595264] EXT4-fs (mmcblk0p2): couldn't mount as ext3 due to feature incompatibilities | [ 6.570705] of_cfs_init: OK |
[ 5.026539] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) | [ 6.573691] cfg80211: Loading compiled-in X.509 certificates for regulatory database |
[ 5.034560] VFS: Mounted root (ext4 filesystem) on device 179:2. | [ 6.712063] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' |
[ 5.045332] devtmpfs: mounted | [ 6.718590] clk: Not disabling unused clocks |
[ 5.048329] Freeing unused kernel memory: 512K (ffffffc000cf0000 - ffffffc000d70000) | [ 6.723122] ALSA device list: |
Mount failed for selinuxfs on /sys/fs/selinux: No such file or directory | [ 6.726081] No soundcards found. |
[ 6.041604] systemd-udevd[2931]: could not open moddep file '/lib/modules/4.9.0-12434-g7f38ed6/modules.dep.bin' | [ 6.729763] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2 |
[ OK ]ting up X socket directories... | [ 6.738370] cfg80211: failed to load regulatory.db |
* STARTDISTCC is set to false in /etc/default/distcc | [ 6.855627] ata2: SATA link down (SStatus 0 SControl 330) |
* /usr/bin/distccd not starting | [ 6.861043] ata1: SATA link down (SStatus 0 SControl 330) |
[ OK ]rting IIO Daemon iiod | [ 7.529447] zynqmp-display fd4a0000.display: [drm] Cannot find any crtc or sizes |
| [ 14.380304] EXT4-fs (mmcblk0p2): warning: mounting fs with errors, running e2fsck is recommended |
| [ 14.492024] EXT4-fs (mmcblk0p2): recovery complete |
| [ 14.578133] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) |
| [ 14.586257] VFS: Mounted root (ext4 filesystem) on device 179:2. |
| [ 14.599775] devtmpfs: mounted |
| [ 14.603610] Freeing unused kernel memory: 2496K |
| [ 14.608263] Run /sbin/init as init process |
| [ 15.227496] systemd[1]: systemd 247.3-7+rpi1 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +ZSTD +SECCOMP +BLKID +ELFUTILS +KMOD +IDN2 -IDN +PCRE2 default-hierarchy=unified) |
| [ 15.250752] systemd[1]: Detected architecture arm64. |
| |
Last login: Thu Apr 27 11:03:18 UTC 2017 on tty1 | Welcome to Kuiper GNU/Linux 11.2 (bullseye)! |
Welcome to Linaro 14.04 (GNU/Linux 4.9.0-12434-g7f38ed6 aarch64) | |
| |
* Documentation: https:%%//%%wiki.analog.com/ https:%%//%%ez.analog.com/ | [ 15.282449] systemd[1]: Set hostname to <analog>. |
| [ 16.855957] systemd[1]: /lib/systemd/system/plymouth-start.service:16: Unit configured to use KillMode=none. This is unsafe, as it disables systemd's process lifecycle management for the service. Please update your service to use a safer KillMode=, such as 'mixed' or 'control-group'. Support for KillMode=none is deprecated and will eventually be removed. |
| [ 17.084624] systemd[1]: Queued start job for default target Graphical Interface. |
| [ 17.093226] random: systemd: uninitialized urandom read (16 bytes read) |
| [ 17.100036] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling. |
| [ 17.112382] systemd[1]: (This warning is only shown for the first unit using IP firewalling.) |
| [ 17.121424] systemd[1]: Created slice system-getty.slice. |
| [ OK ] Created slice system-getty.slice. |
| [ 17.141524] random: systemd: uninitialized urandom read (16 bytes read) |
| [ 17.148512] systemd[1]: Created slice system-modprobe.slice. |
| [ OK ] Created slice system-modprobe.slice. |
| [ 17.169507] random: systemd: uninitialized urandom read (16 bytes read) |
| [ 17.176464] systemd[1]: Created slice system-serial\x2dgetty.slice. |
| [ OK ] Created slice system-serial\x2dgetty.slice. |
| [ 17.197816] systemd[1]: Created slice system-systemd\x2dfsck.slice. |
| [ OK ] Created slice system-systemd\x2dfsck.slice. |
| [ 17.221734] systemd[1]: Created slice User and Session Slice. |
| [ OK ] Created slice User and Session Slice. |
| [ 17.241765] systemd[1]: Started Forward Password Requests to Wall Directory Watch. |
| [ OK ] Started Forward Password R…uests to Wall Directory Watch. |
| [ 17.265740] systemd[1]: Condition check resulted in Arbitrary Executable File Formats File System Automount Point being skipped. |
| [ 17.278165] systemd[1]: Reached target Slices. |
| [ OK ] Reached target Slices. |
| [ 17.293632] systemd[1]: Reached target Swap. |
| [ OK ] Reached target Swap. |
| [ 17.310254] systemd[1]: Listening on Syslog Socket. |
| [ OK ] Listening on Syslog Socket. |
| [ 17.325846] systemd[1]: Listening on fsck to fsckd communication Socket. |
| [ OK ] Listening on fsck to fsckd communication Socket. |
| [ 17.349668] systemd[1]: Listening on initctl Compatibility Named Pipe. |
| [ OK ] Listening on initctl Compatibility Named Pipe. |
| [ 17.376773] systemd[1]: Listening on Journal Audit Socket. |
| [ OK ] Listening on Journal Audit Socket. |
| [ 17.397860] systemd[1]: Listening on Journal Socket (/dev/log). |
| [ OK ] Listening on Journal Socket (/dev/log). |
| [ 17.421888] systemd[1]: Listening on Journal Socket. |
| [ OK ] Listening on Journal Socket. |
| [ 17.445475] systemd[1]: Listening on udev Control Socket. |
| [ OK ] Listening on udev Control Socket. |
| [ 17.465827] systemd[1]: Listening on udev Kernel Socket. |
| [ OK ] Listening on udev Kernel Socket. |
| [ 17.487436] systemd[1]: Mounting Huge Pages File System... |
| Mounting Huge Pages File System... |
| [ 17.503356] systemd[1]: Mounting POSIX Message Queue File System... |
| Mounting POSIX Message Queue File System... |
| [ 17.527103] systemd[1]: Mounting RPC Pipe File System... |
| Mounting RPC Pipe File System... |
| [ 17.543385] systemd[1]: Mounting Kernel Debug File System... |
| Mounting Kernel Debug File System... |
| [ 17.561978] systemd[1]: Condition check resulted in Kernel Trace File System being skipped. |
| [ 17.570631] systemd[1]: Condition check resulted in Kernel Module supporting RPCSEC_GSS being skipped. |
| [ 17.583314] systemd[1]: Starting Restore / save the current clock... |
| Starting Restore / save the current clock... |
| [ 17.609712] systemd[1]: Starting Set the console keyboard layout... |
| Starting Set the console keyboard layout... |
| [ 17.636616] systemd[1]: Condition check resulted in Create list of static device nodes for the current kernel being skipped. |
| [ 17.650210] systemd[1]: Starting Load Kernel Module configfs... |
| Starting Load Kernel Module configfs... |
| [ 17.667701] systemd[1]: Starting Load Kernel Module drm... |
| Starting Load Kernel Module drm... |
| [ 17.687697] systemd[1]: Starting Load Kernel Module fuse... |
| Starting Load Kernel Module fuse... |
| [ 17.708717] systemd[1]: Condition check resulted in Set Up Additional Binary Formats being skipped. |
| [ 17.717983] systemd[1]: Condition check resulted in File System Check on Root Device being skipped. |
| [ 17.729053] systemd[1]: Starting Journal Service... |
| Starting Journal Service... |
| [ 17.750063] systemd[1]: Starting Load Kernel Modules... |
| Starting Load Kernel Modules... |
| [ 17.767598] systemd[1]: Starting Remount Root and Kernel File Systems... |
| Starting Remount Root and Kernel File Systems... |
| [ 17.791561] systemd[1]: Starting Coldplug All udev Devices... |
| Starting Coldplug All udev Devices... |
| [ 17.814846] systemd[1]: Mounted Huge Pages File System. |
| [ OK ] Mounted Huge Pages File System. |
| [ 17.843501] systemd[1]: Mounted POSIX Message Queue File System. |
| [ OK ] Mounted POSIX Message Queue File System. |
| [ 17.866054] systemd[1]: Mounted RPC Pipe File System. |
| [ OK ] Mounted RPC Pipe File System. |
| [ 17.882062] systemd[1]: Mounted Kernel Debug File System. |
| [ OK ] Mounted Kernel Debug File System. |
| [ 17.906458] systemd[1]: Finished Restore / save the current clock. |
| [ OK ] Finished Restore / save the current clock. |
| [ 17.930679] systemd[1]: Finished Set the console keyboard layout. |
| [ OK ] Finished Set the console keyboard layout. |
| [ 17.953966] systemd[1]: Started Journal Service. |
| [ OK ] Started Journal Service. |
| [ OK ] Finished Load Kernel Module configfs. |
| [ OK ] Finished Load Kernel Module drm. |
| [ 17.997740] random: crng init done |
| [ 18.001139] random: 7 urandom warning(s) missed due to ratelimiting |
| [ OK ] Finished Load Kernel Module fuse. |
| [FAILED] Failed to start Load Kernel Modules. |
| See 'systemctl status systemd-modules-load.service' for details. |
| Mounting FUSE Control File System... |
| Mounting Kernel Configuration File System... |
| Starting Apply Kernel Variables... |
| [ OK ] Mounted FUSE Control File System. |
| [ OK ] Mounted Kernel Configuration File System. |
| [ OK ] Finished Apply Kernel Variables. |
| [ OK ] Finished Remount Root and Kernel File Systems. |
| Starting Flush Journal to Persistent Storage... |
| Starting Load/Save Random Seed... |
| Starting Create System Users... |
| [ OK ] Finished Coldplug All udev Devices. |
| Starting Helper to synchronize boot up for ifupdown... |
| Starting Wait for udev To …plete Device Initialization... |
| [* ] (1 of 10) A start job is running fo…d/Save Random Seed (3s / 10min 1s) |
| [ 20.713866] EXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:802: group 32, block bitmap and bg descriptor inconsistent: 8461 vs 10906 free clusters |
| [ 20.731848] EXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:802: group 64, block bitmap and bg descriptor inconsistent: 23266 vs 23260 free clusters |
| [ 20.779729] EXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:802: group 0, block bitmap and bg descriptor inconsistent: 18343 vs 18331 free clusters |
| [ 20.793915] EXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:802: group 25, block [ OK ] Finished Helper to synchronize boot up for ifupdown. |
| [ OK ] Finished Create System Users. |
| Starting Create Static Device Nodes in /dev... |
| [ 20.874353] EXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:802: group 59, block bitmap and bg descriptor inconsistent: 2718 vs 2714 free clusters |
| [ 20.910902] EXT4-fs error (device mmcblk0p2): ext4_lookup:1708: inode #16388: comm systemd-journal: deleted inode referenced: 11882 |
| [ OK ] Finished Load/Save Random Seed. |
| [ OK ] Finished Create Static Device Nodes in /dev. |
| [ OK ] Reached target Local File Systems (Pre). |
| Starting Rule-based Manage…for Device Events and Files... |
| [ *] (3 of 8) A start job is running for…rtuuid/f7eeebee-01 (9s / 1min 30s) |
| [ 27.126343] EXT4-fs error (device mmcblk0p2): ext4_lookup:1708: inode #16388: comm systemd[ **] (3 of 8) A start job is running for…tuuid/f7eeebee-01 (10s / 1min 30s) |
| [ 27.448819] EXT4-fs error (device mmcblk0p2): ext4_lookup:1708: inode #16388: comm systemd[ OK ] Finished Flush Journal to Persistent Storage. |
| [ OK ] Started Rule-based Manager for Device Events and Files. |
| Starting Show Plymouth Boot Screen... |
| [ OK ] Started Show Plymouth Boot Screen. |
| [ OK ] Started Forward Password R…s to Plymouth Directory Watch. |
| [ OK ] Reached target Local Encrypted Volumes. |
| [ OK ] Found device /dev/ttyPS0. |
| [ OK ] Reached target Hardware activated USB gadget. |
| Starting Load Kernel Modules... |
| [FAILED] Failed to start Load Kernel Modules. |
| See 'systemctl status systemd-modules-load.service' for details. |
| [ OK ] Found device /dev/ttyS0. |
| [ OK ] Found device /dev/disk/by-partuuid/f7eeebee-01. |
| [ OK ] Listening on Load/Save RF …itch Status /dev/rfkill Watch. |
| Starting File System Check…isk/by-partuuid/f7eeebee-01... |
| [ OK ] Finished Wait for udev To Complete Device Initialization. |
| [ OK ] Finished File System Check…/disk/by-partuuid/f7eeebee-01. |
| Mounting /boot... |
| [ OK ] Started File System Check Daemon to report status. |
| [ OK ] Mounted /boot. |
| [ OK ] Reached target Local File Systems. |
| Starting Set console font and keymap... |
| Starting Raise network interfaces... |
| Starting Preprocess NFS configuration... |
| Starting Tell Plymouth To Write Out Runtime Data... |
| Starting Create Volatile Files and Directories... |
| [ OK ] Finished Set console font and keymap. |
| [ OK ] Finished Preprocess NFS configuration. |
| [ OK ] Reached target NFS client services. |
| [ OK ] Reached target Remote File Systems (Pre). |
| [ OK ] Reached target Remote File Systems. |
| [ OK ] Finished Tell Plymouth To Write Out Runtime Data. |
| [ OK ] Finished Create Volatile Files and Directories. |
| Starting Update UTMP about System Boot/Shutdown... |
| [ OK ] Finished Update UTMP about System Boot/Shutdown. |
| [ OK ] Reached target System Initialization. |
| [ OK ] Started CUPS Scheduler. |
| [ OK ] Started Daily apt download activities. |
| [ OK ] Started Daily apt upgrade and clean activities. |
| [ OK ] Started Periodic ext4 Onli…ata Check for All Filesystems. |
| [ OK ] Started Discard unused blocks once a week. |
| [ OK ] Started Daily rotation of log files. |
| [ OK ] Started Daily man-db regeneration. |
| [ OK ] Started Daily Cleanup of Temporary Directories. |
| [ OK ] Reached target Paths. |
| [ OK ] Reached target Timers. |
| [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. |
| [ OK ] Listening on CUPS Scheduler. |
| [ OK ] Listening on D-Bus System Message Bus Socket. |
| [ OK ] Listening on Erlang Port Mapper Daemon Activation Socket. |
| [ OK ] Listening on GPS (Global P…ioning System) Daemon Sockets. |
| [ OK ] Listening on triggerhappy.socket. |
| [ OK ] Reached target Sockets. |
| [ OK ] Reached target Basic System. |
| Starting Avahi mDNS/DNS-SD Stack... |
| [ OK ] Started Regular background program processing daemon. |
| [ OK ] Started D-Bus System Message Bus. |
| Starting dphys-swapfile - …unt, and delete a swap file... |
| Starting Remove Stale Onli…t4 Metadata Check Snapshots... |
| Starting Creating IIOD Context Attributes...... |
| Starting Authorization Manager... |
| Starting DHCP Client Daemon... |
| Starting LSB: Switch to on…nless shift key is pressed)... |
| Starting LSB: rng-tools (Debian variant)... |
| Starting System Logging Service... |
| Starting User Login Management... |
| Starting triggerhappy global hotkey daemon... |
| Starting Disk Manager... |
| Starting WPA supplicant... |
| Starting Rotate log files... |
| Starting Daily man-db regeneration... |
| [ OK ] Finished Remove Stale Onli…ext4 Metadata Check Snapshots. |
| [ OK ] Started triggerhappy global hotkey daemon. |
| [ OK ] Started DHCP Client Daemon. |
| [ OK ] Finished Raise network interfaces. |
| [ OK ] Started LSB: rng-tools (Debian variant). |
| [ OK ] Started System Logging Service. |
| [ OK ] Finished dphys-swapfile - …mount, and delete a swap file. |
| [ 32.756194] EXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:802: group 75, block bitmap and bg descriptor inconsistent: 32730 vs 32733 free clusters |
| [FAILED] Failed to start Rotate log files. |
| See 'systemctl status logrotate.service' for details. |
| [ OK ] Started LSB: Switch to ond…(unless shift key is pressed). |
| Starting Online ext4 Metad…a Check for All Filesystems... |
| [ OK ] Finished Online ext4 Metadata Check for All Filesystems. |
| [ OK ] Finished Creating IIOD Context Attributes.... |
| [ OK ] Started User Login Management. |
| [ OK ] Started Avahi mDNS/DNS-SD Stack. |
| [ OK ] Started WPA supplicant. |
| [ OK ] Reached target Network. |
| [ OK ] Reached target Network is Online. |
| Starting CUPS Scheduler... |
| [ OK ] Started Erlang Port Mapper Daemon. |
| Starting Load USB gadget scheme... |
| Starting HTTP based time synchronization tool... |
| [ OK ] Started IIO Daemon. |
| Starting Internet superserver... |
| Starting /etc/rc.local Compatibility... |
| Starting OpenBSD Secure Shell server... |
| Starting Permit User Sessions... |
| [ OK ] Started Unattended Upgrades Shutdown. |
| [ OK ] Started /etc/rc.local Compatibility. |
| [ OK ] Finished Permit User Sessions. |
| Starting Light Display Manager... |
| Starting Hold until boot process finishes up... |
| [ OK ] Started HTTP based time synchronization tool. |
| [ OK ] Started Authorization Manager. |
| Starting Modem Manager... |
| [ OK ] Started Internet superserver. |
| [ OK ] Finished Load USB gadget scheme. |
| Mounting Mount FunctionFS instance... |
| [ OK ] Found device /dev/ttyGS0. |
| [ OK ] Mounted Mount FunctionFS instance. |
| Starting IIO Daemon with USB FFS support... |
| Stopping IIO Daemon... |
| [ OK ] Stopped IIO Daemon. |
| [ OK ] Started IIO Daemon with USB FFS support. |
| Starting Start USB gadget scheme... |
| [ OK ] Started OpenBSD Secure Shell server. |
| |
New release '16.04.3 LTS' available. | Raspbian GNU/Linux 11 analog ttyPS0 |
Run 'do-release-upgrade' to upgrade to it. | |
| |
root@analog:~# | analog login: root (automatic login) |
</xterm></WRAP> | </code></WRAP> |
| |
<WRAP box bggreen><wrap info>This specifies any shell prompt running on the target</wrap> | <WRAP box bggreen><wrap info>This specifies any shell prompt running on the target</wrap> |
<xterm> | <xterm> |
root@analog:~# iio_info | grep iio:device | root@analog:~# iio_info | grep iio:device |
iio:device0: ad7291 | iio:device0: ams |
iio:device1: ad9361-phy | iio:device1: ad9361-phy |
iio:device2: cf-ad9361-dds-core-lpc | iio:device2: ad7291 |
iio:device3: cf-ad9361-lpc | iio:device3: cf-ad9361-lpc (buffer capable) |
| iio:device4: cf-ad9361-dds-core-lpc (buffer capable) |
</xterm></WRAP> | </xterm></WRAP> |
| |
<WRAP box bggreen><wrap info>This specifies any shell prompt running on the target</wrap> | <WRAP box bggreen><wrap info>This specifies any shell prompt running on the target</wrap> |
<xterm> | <xterm> |
root@analog:~# fru-dump -b /sys/bus/i2c/devices/14-0050/eeprom | root@analog:~# fru-dump -b /sys/bus/i2c/devices/14-0050/eeprom |
read 256 bytes from /sys/bus/i2c/devices/14-0050/eeprom | read 256 bytes from /sys/bus/i2c/devices/14-0050/eeprom |
Date of Man : Wed Aug 27 16:42:00 2014 | Date of Man : Wed Jun 18 12:51:00 2014 |
Manufacture : Analog Devices | Manufacturer : Analog Devices |
Product Name : AD9361 Software Development Kit | Product Name : AD9361 RF Hardware Development Kit |
Serial Number : Non-ASCII | Serial Number : 00051 |
Part Number : AD-FMCOMMS3-EBZ | Part Number : AD-FMCOMMS2-EBZ |
FRU File ID : Empty Field | FRU File ID : Empty Field |
PCB Rev : A | PCB Rev : C |
PCB ID : FMCOMMSFMC03A | PCB ID : 9361FMC01A |
BOM Rev : 1 | BOM Rev : 1 |
Uses LVDS : Y | Uses LVDS : Y |