This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fmcomms2-ebz:quickstart:zynq [04 Jun 2021 20:29] – [AD-FMCOMMS2/3/4/5-EBZ Zynq and ZED Quick Start Guide] Robin Getz | resources:eval:user-guides:ad-fmcomms2-ebz:quickstart:zynq [09 Jun 2021 12:11] – Add details to link Iulia Moldovan | ||
---|---|---|---|
Line 19: | Line 19: | ||
===== Creating / Configuring the SD Card ===== | ===== Creating / Configuring the SD Card ===== | ||
- | [[resources/ | + | Create the [[resources/ |
{{page> | {{page> | ||
Line 29: | Line 29: | ||
- Get the [[xilinx> | - Get the [[xilinx> | ||
- {{http:// | - {{http:// | ||
- | | + | - Prepare the SD card with the proper Linux image (from [[: |
- | - Build the devicetree (see [[: | + | |
- | | + | |
- Insert the SD-CARD into the SD Card Interface Connector (J30) | - Insert the SD-CARD into the SD Card Interface Connector (J30) | ||
- Plug the AD-FMCOMMS2-EBZ into the LPC LPC Connector (J5) | - Plug the AD-FMCOMMS2-EBZ into the LPC LPC Connector (J5) | ||
Line 42: | Line 40: | ||
- Wait another ~30 seconds for the HDMI display device to start showing signs of life. | - Wait another ~30 seconds for the HDMI display device to start showing signs of life. | ||
- The follow the instructions for the type of demo that you want to do. | - The follow the instructions for the type of demo that you want to do. | ||
+ | |||
===== Booting the SD Card ===== | ===== Booting the SD Card ===== | ||
Line 59: | Line 58: | ||
- Set the Jumpers and Switches accordingly like shown on the picture. (click on the picture to enlarge) | - Set the Jumpers and Switches accordingly like shown on the picture. (click on the picture to enlarge) | ||
- {{: | - {{: | ||
- | | + | - Prepare the SD card with the proper Linux image (see [[: |
- | - Build the devicetree (see [[: | + | |
- | | + | |
- Insert the SD-CARD into the SD Card Interface Connector (J12) | - Insert the SD-CARD into the SD Card Interface Connector (J12) | ||
- Plug the AD-FMCOMMS2-EBZ or AD-FMCOMMS3-EBZ into the LPC Connector (J1) | - Plug the AD-FMCOMMS2-EBZ or AD-FMCOMMS3-EBZ into the LPC Connector (J1) | ||
Line 75: | Line 72: | ||
- Wait another ~30 seconds for the HDMI display device to start showing signs of life. (Linux TUX top left) | - Wait another ~30 seconds for the HDMI display device to start showing signs of life. (Linux TUX top left) | ||
- Follow the instructions for the type of demo that you want to do on screen. | - Follow the instructions for the type of demo that you want to do on screen. | ||
+ | |||
+ | <note tip> | ||
+ | If you want to manually build the HDL project and make the BOOT.BIN, see [[: | ||
+ | </ | ||
Setup/ | Setup/ | ||
Line 81: | Line 82: | ||
**Note:** For proper robustness shield the ZED board with a plexi-glass cover. Add a " | **Note:** For proper robustness shield the ZED board with a plexi-glass cover. Add a " | ||
- | |||
- | |||