Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:user-guides:ad-fmcomms2-ebz:introduction [14 Oct 2016 13:50] – [Where to go next] remove bottom page links to previous and next section Lucian Sin | resources:eval:user-guides:ad-fmcomms2-ebz:introduction [17 Oct 2016 14:49] – [Introduction to boards based on the AD9361] added LPC type to FMC connectors Lucian Sin |
---|
| |
^ Board ^ AD936x Device ^ Simultaneous \\ Tx / Rx ^ Tx \\ (Ranges) ^ Rx \\ (Ranges) ^ Purpose ^ Connector ^ | ^ Board ^ AD936x Device ^ Simultaneous \\ Tx / Rx ^ Tx \\ (Ranges) ^ Rx \\ (Ranges) ^ Purpose ^ Connector ^ |
| [[../ad-fmcomms2-ebz|AD-FMCOMMS2-EBZ]] | 1 x AD9361 | 2 x 2 | 2 (2400 - 2500 MHz) | 2 (2400 - 2500 MHz) | Best RF performance in a narrow range | FMC | | | [[../ad-fmcomms2-ebz|AD-FMCOMMS2-EBZ]] | 1 x AD9361 | 2 x 2 | 2 (2400 - 2500 MHz) | 2 (2400 - 2500 MHz) | Best RF performance in a narrow range | FMC-LPC | |
| [[../arradio|ARRADIO]] | 1 x AD9361 | 2 x 2 | 2 (2400 - 2500 MHz) | 2 (2400 - 2500 MHz) | Best RF performance in a narrow range | HSMC | | | [[../arradio|ARRADIO]] | 1 x AD9361 | 2 x 2 | 2 (2400 - 2500 MHz) | 2 (2400 - 2500 MHz) | Best RF performance in a narrow range | HSMC | |
| [[../ad-fmcomms3-ebz|AD-FMCOMMS3-EBZ]] | 1 x AD9361 | 2 x 2 | 2 (70 - 6000 MHz) | 2 (70 - 6000 MHz) | Software test and waveform development | FMC | | | [[../ad-fmcomms3-ebz|AD-FMCOMMS3-EBZ]] | 1 x AD9361 | 2 x 2 | 2 (70 - 6000 MHz) | 2 (70 - 6000 MHz) | Software test and waveform development | FMC-LPC | |
| [[../ad-fmcomms4-ebz|AD-FMCOMMS4-EBZ]] | 1 x AD9364 | 1 x 1 | 1 (2400 - 2500 MHz) \\ 1 (70 - 6000 MHz) | 1 (2400 - 2500 MHz) \\ 1 (70 - 6000 MHz) | | FMC | | | [[../ad-fmcomms4-ebz|AD-FMCOMMS4-EBZ]] | 1 x AD9364 | 1 x 1 | 1 (2400 - 2500 MHz) \\ 1 (70 - 6000 MHz) | 1 (2400 - 2500 MHz) \\ 1 (70 - 6000 MHz) | | FMC-LPC | |
| [[../ad-fmcomms5-ebz|AD-FMCOMMS5-EBZ]] | 2 x AD9361 | 4 x 4 | 4 (2400 - 2500 MHz) \\ 4 (70 - 6000 MHz) | 4 (2400 - 2500 MHz) \\ 4 (70 - 6000 MHz) | MIMO test platform, can be synchronized in the RF domain | 2 x FMC | | | [[../ad-fmcomms5-ebz|AD-FMCOMMS5-EBZ]] | 2 x AD9361 | 4 x 4 | 4 (2400 - 2500 MHz) \\ 4 (70 - 6000 MHz) | 4 (2400 - 2500 MHz) \\ 4 (70 - 6000 MHz) | MIMO test platform, can be synchronized in the RF domain | 2 x FMC-LPC | |
| |
<WRAP important>While the AD9361 digital interface supports both LVDS and CMOS mode, all the FMCOMMS boards have been verified in LVDS mode only. Configuring the digital interface in CMOS mode is not tested nor supported on these platforms. This is due to the purposefully weak CMOS drivers (To keep the noise off the part as much as possible) that are part of the digital interface and the large capacitance of the FMC connector. | <WRAP important>While the AD9361 digital interface supports both LVDS and CMOS mode, all the FMCOMMS boards have been verified in LVDS mode only. Configuring the digital interface in CMOS mode is not tested nor supported on these platforms. This is due to the purposefully weak CMOS drivers (To keep the noise off the part as much as possible) that are part of the digital interface and the large capacitance of the FMC connector. |