Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:user-guides:ad-fmcomms2-ebz:hardware [21 May 2015 21:49] – Amberle Zuerlein | resources:eval:user-guides:ad-fmcomms2-ebz:hardware [25 Nov 2015 14:42] – old revision restored (25 Mar 2014 21:27) Lars-Peter Clausen |
---|
====== ARRadio Hardware ====== | ====== AD-FMCOMMS2-EBZ Hardware ====== |
| |
===== Downloads ===== | ===== Downloads ===== |
| |
<WRAP round download 65%> | <WRAP round download 65%> |
<WRAP info> | <WRAP info>This is the latest and greatest Rev "E" of this board. Note that the Baluns on the Rev C board (T101-T104) are Johanson Technology's [[http://www.johansontechnology.com/images/stories/ip/baluns/Balun_2450BL15B050.pdf|2450BL15B050E]] 2.45 GHz Balun. This balun is rated for a operating frequency of 2400~2500 MHz. If you want to evaluate the part outside of this frequency range, an [[./hardware/configuration_options|alternative balun]] should be installed. The test results were taken using the Johanson Technology's 2450BL15B050E balun. |
| |
</WRAP> | </WRAP> |
===== I/O Voltage ===== | ===== I/O Voltage ===== |
| |
The ARRadio (AD9361) assumes a VDD_INTERFACE voltage between 1.71V and 2.625V (1.8 to 2.5 +/- 5%), so on your FPGA carrier board, you should ensure that V<sub>ADJ</sub> is between these levels. Setting things to 3.3V will damage the part. | The AD-FMComms2 (AD9361) assumes a VDD_INTERFACE voltage between 1.71V and 2.625V (1.8 to 2.5 +/- 5%), so on your FPGA carrier board, you should ensure that V<sub>ADJ</sub> is between these levels. Setting things to 3.3V will damage the part. |
| |
| |
===== Picture and Main components ===== | ===== Picture and Main components ===== |
| |
| {{:resources:eval:user-guides:ad-fmcomms2-ebz:fmcomms2_locations.png?direct&600|}} |
| |
===== Outline ===== | ===== Outline ===== |