This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fmcomms2-ebz:hardware:card_specification [15 Jul 2014 08:16] – [EVM] srikanth malipeddi | resources:eval:user-guides:ad-fmcomms2-ebz:hardware:card_specification [15 Oct 2014 01:13] – [Bandwidth] - spelling Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== AD-FMCOMMS2-EBZ Specifications ====== | + | ====== AD-FMCOMMS2-EBZ / AD-FMCOMMS4-EBZ / AD-FMCOMMS5-EBZ Specifications ====== |
|The following equipments were used to generate the following characterization data:| | |The following equipments were used to generate the following characterization data:| | ||
Line 5: | Line 5: | ||
|The Agilent Technology MXA Signal Analyzer and the Rohde& | |The Agilent Technology MXA Signal Analyzer and the Rohde& | ||
+ | These specs are common to any of the boards which use a narrow band balun. | ||
===== Transmit Specs ===== | ===== Transmit Specs ===== | ||
Line 65: | Line 66: | ||
|{{: | |{{: | ||
- | |BW with 2.4GHz LO and -10dBm input and Slow attach | + | |BW with 2.4GHz LO and -10dBm input and Slow attack |
{{navigation AD-FMCOMMS2-EBZ# | {{navigation AD-FMCOMMS2-EBZ# |