This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:ad-fmcomms2-ebz:ad9361 [05 Nov 2021 19:59] – Update PLL wording Travis Collins | resources:eval:user-guides:ad-fmcomms2-ebz:ad9361 [27 Jan 2023 14:37] (current) – Update documentation link for AD9361 Reference Manual Paul Pop | ||
---|---|---|---|
Line 13: | Line 13: | ||
The AD9361 and AD9364 also provide self-calibration and automatic gain control (AGC) systems to maintain a high performance level under varying temperatures and input signal conditions. In addition, the device includes several test modes that allow system designers to insert test tones and create internal loopback modes that can be used by designers to debug their designs during prototyping and optimize their radio configuration for a specific application. | The AD9361 and AD9364 also provide self-calibration and automatic gain control (AGC) systems to maintain a high performance level under varying temperatures and input signal conditions. In addition, the device includes several test modes that allow system designers to insert test tones and create internal loopback modes that can be used by designers to debug their designs during prototyping and optimize their radio configuration for a specific application. | ||
+ | |||
+ | More information can be found in the AD9361 Reference Manual [[https:// | ||
===== Receive Chain ===== | ===== Receive Chain ===== |