Wiki

This version is outdated by a newer approved version.DiffThis version (11 Nov 2022 12:38) was approved by Raluca Chis.The Previously approved version (10 Nov 2022 16:05) is available.Diff

This is an old revision of the document!


Linux on the Xilinx ML605 Virtex6 FPGA development Board

This guide provides some step-by-step instructions on how to build a Microblaze Linux Kernel image for the AD-FMCOMMS1 FMC board connected to an ML605.

Building Linux on ML605 Virtex6 board remains on this website only for legacy purposes. The Linux support for this carrier has been discontinued.

Required Software

Build Linux - Step by Step instructions

Get Microblaze Little Endian Toolchain from Xilinx

This specifies any shell prompt running on the target or development host

Dave@HAL9000:~/fmcomms1$ git clone git://git.xilinx.com/xldk/microblaze_v1.0_le.git
Cloning into 'microblaze_v1.0_le'...
remote: Counting objects: 4, done.
remote: Compressing objects: 100% (4/4), done.
Receiving objects:  75% (3/4), 12.65 MiB | 5 KiB/s
[--snip--]

Untar Toolchain

This specifies any shell prompt running on the target or development host

Dave@HAL9000:~/fmcomms1$ cd microblaze_v1.0_le/
Dave@HAL9000:~/fmcomms1/microblaze_v1.0_le$ tar xzf microblazeel-unknown-linux-gnu.tar.gz

Get Linux kernel source

This specifies any shell prompt running on the target or development host

Dave@HAL9000:~/fmcomms1$ git clone https://github.com/analogdevicesinc/linux.git
Cloning into 'linux'...
remote: Counting objects: 2757163, done.
remote: Compressing objects: 100% (495484/495484), done.
remote: Total 2757163 (delta 2296596), reused 2687337 (delta 2234506)
Receiving objects: 100% (2757163/2757163), 782.04 MiB | 1.39 MiB/s, done.
Resolving deltas: 100% (2296596/2296596), done.
Dave@HAL9000:~/fmcomms1$

Checkout master branch

This specifies any shell prompt running on the target or development host

Dave@HAL9000:~/fmcomms1$ cd linux/
Dave@HAL9000:~/fmcomms1/linux$ git checkout origin/master
Checking out files: 100% (16412/16412), done.
Dave@HAL9000:~/fmcomms1/linux$

Set Environmental Variables

This specifies any shell prompt running on the target or development host

Dave@HAL9000:~/fmcomms1/linux$ export PATH=~/fmcomms1/microblaze_v1.0_le/microblazeel-unknown-linux-gnu/bin/:$PATH
Dave@HAL9000:~/fmcomms1/linux$ export ARCH=microblaze
Dave@HAL9000:~/fmcomms1/linux$ export CROSS_COMPILE=microblazeel-unknown-linux-gnu-

Configure Kernel for ML605 XCOMM platform (aka FMCOMMS1)

This specifies any shell prompt running on the target or development host

Dave@HAL9000:~/fmcomms1/linux$ make ml605_xcomm_defconfig
  HOSTCC  scripts/basic/fixdep
  HOSTCC  scripts/kconfig/conf.o
  SHIPPED scripts/kconfig/zconf.tab.c
  SHIPPED scripts/kconfig/zconf.lex.c
  SHIPPED scripts/kconfig/zconf.hash.c
  HOSTCC  scripts/kconfig/zconf.tab.o
  HOSTLD  scripts/kconfig/conf
#
# configuration written to .config
#
Dave@HAL9000:~/fmcomms1/linux$

Get Root File-System

Root File-system (initramfs)

This specifies any shell prompt running on the target or development host

Dave@HAL9000:~/fmcomms1/linux$ wget http://wiki.analog.com/_media/resources/eval/user-guides/ad-fmcomms1-ebz/software/linux/rootfs.cpio.gz
--2012-12-19 09:25:28--  http://wiki.analog.com/_media/resources/eval/user-guides/ad-fmcomms1-ebz/software/linux/rootfs.cpio.gz
Resolving wiki.analog.com (wiki.analog.com)... 195.170.124.184
Connecting to wiki.analog.com (wiki.analog.com)|195.170.124.184|:80... connected.
HTTP request sent, awaiting response... 200 OK
Length: 2958801 (2.8M) [application/octet-stream]
Saving to: `rootfs.cpio.gz'

100%[=====================================================================================================
=====================================================================>] 2,958,801   1.42M/s   in 2.0s    

2012-12-19 09:25:30 (1.42 MB/s) - `rootfs.cpio.gz' saved [2958801/2958801]
Dave@HAL9000:~/fmcomms1/linux$

Build kernel

This specifies any shell prompt running on the target or development host

Dave@HAL9000:~/fmcomms1/linux$ make -j5 simpleImage.cf_xcomm_ml605
  CHK     include/linux/version.h
  UPD     include/linux/version.h
  HOSTCC  scripts/kallsyms
  HOSTCC  scripts/bin2c
  HOSTCC  scripts/dtc/checks.o
  CC      scripts/mod/empty.o
[--snip--]
  CP      vmlinux arch/microblaze/boot/simpleImage.cf_xcomm_ml605.unstrip
  OBJCOPY arch/microblaze/boot/simpleImage.cf_xcomm_ml605
  UIMAGE  arch/microblaze/boot/simpleImage.cf_xcomm_ml605.ub
Image Name:   Linux-3.5.0-rc4-00817-gbf1afb2
Created:      Tue Dec 18 16:50:37 2012
Image Type:   MicroBlaze Linux Kernel Image (uncompressed)
Data Size:    6178556 Bytes = 6033.75 kB = 5.89 MB
Load Address: c0000000
Entry Point:  c0000000
  STRIP   arch/microblaze/boot/simpleImage.cf_xcomm_ml605
Kernel: arch/microblaze/boot/simpleImage.cf_xcomm_ml605 is ready  (#1)
Dave@HAL9000:~/devel/git/staging_3$

Generate ML605 SysACE Compact Flash File

Following example shows building the System ACE file on a Linux host. Same steps can alternatively performed on a Windows ISE installation.

Create a directory and gather required files

This specifies any shell prompt running on the target or development host

Dave@HAL9000:~/fmcomms1$ mkdir build
Dave@HAL9000:~/fmcomms1$ cd build/
Dave@HAL9000:~/fmcomms1/build$ cp ~/fpgahdl_xilinx/cf_xcomm/implementation/system.bit .
Dave@HAL9000:~/fmcomms1/build$ cp ../linux/arch/microblaze/boot/simpleImage.cf_xcomm_ml605 .

Source Xilinx ISE settings

On Windows open a ISE Design Suite Command Prompt.

This specifies any shell prompt running on the target or development host

Dave@HAL9000:~/fmcomms1/build$ source /opt/Xilinx/14.1/ISE_DS/settings64.sh
. /opt/Xilinx/14.1/ISE_DS/common/.settings64.sh /opt/Xilinx/14.1/ISE_DS/common
. /opt/Xilinx/14.1/ISE_DS/EDK/.settings64.sh /opt/Xilinx/14.1/ISE_DS/EDK
. /opt/Xilinx/14.1/ISE_DS/common/CodeSourcery/.settings64.sh /opt/Xilinx/14.1/ISE_DS/common/CodeSourcery
. /opt/Xilinx/14.1/ISE_DS/PlanAhead/.settings64.sh /opt/Xilinx/14.1/ISE_DS/PlanAhead
. /opt/Xilinx/14.1/ISE_DS/../../Vivado/2012.1/.settings64.sh /opt/Xilinx/14.1/ISE_DS/../../Vivado/2012.1
. /opt/Xilinx/14.1/ISE_DS/ISE/.settings64.sh /opt/Xilinx/14.1/ISE_DS/ISE
. /opt/Xilinx/14.1/ISE_DS/SysGen/.settings64.sh /opt/Xilinx/14.1/ISE_DS/SysGen

Run XMD genace tcl script

This specifies any shell prompt running on the target or development host

Dave@HAL9000:~/fmcomms1/build$ xmd -tcl genace.tcl -hw system.bit -elf simpleImage.cf_xcomm_ml605 -ace linux.ace -board ml605 -target mdm
Xilinx Microprocessor Debugger (XMD) Engine
Xilinx EDK 14.1 Build EDK_P.15xf
Copyright (c) 1995-2009 Xilinx, Inc.  All rights reserved.
Executing xmd script : /opt/Xilinx/14.1/ISE_DS/EDK/data/xmd/genace.tcl

#######################################################################
XMD GenACE utility. Generate SystemACE File from bit/elf/data Files
#######################################################################
Parsing genace option: -hw system.bit -elf simpleImage.cf_xcomm_ml605 -ace linux.ace -board ml605 -target mdm
GenACE Options:
	Board      : ml605
	Jtag Devs  : xc6vlx240t
	FPGA pos   : 1
	JPROG      : false
	HW File    : system.bit
	ACE File   : linux.ace
	nCPUs      : 1

	Processor mdm_1 Information
		Debug opt : -debugdevice devicenr 1 cpunr 1
		ELF files : simpleImage.cf_xcomm_ml605
		Start PC Address : 0xc0000000
Open SVF file

############################################################
Converting Bitstream 'system.bit' to SVF file 'system.svf'

[--snip--]

RUNNING>
############################################################
Converting SVF file 'linux.svf' to SystemACE file 'linux.ace'
Executing 'impact -batch svf2ace.scr'

SystemACE file 'linux.ace' created

The newly created System ACE file can now be transferred to an Compact Flash card. Instructions on how to format and setup the CF Card and configure the ML605 for SysACE boot can be found here:

AD-FMCOMMS1-EBZ ML605 Quick Start Guide

More information

resources/eval/user-guides/ad-fmcomms1-ebz/software/linux/microblaze_ml605.1668166684.txt.gz · Last modified: 11 Nov 2022 12:38 by Raluca Chis