This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-fmcomms1-ebz:iq_correction [28 Oct 2016 11:03] – [With I/Q Correction] change ask help link Lucian Sin | resources:eval:user-guides:ad-fmcomms1-ebz:iq_correction [21 Jan 2022 01:42] (current) – update links Robin Getz | ||
---|---|---|---|
Line 24: | Line 24: | ||
===== Math of I/Q Correction ===== | ===== Math of I/Q Correction ===== | ||
- | We will use the algorithm introduced in S.W. Ellingson' | + | We will use the algorithm introduced in S.W. Ellingson' |
Given a single tone that converts the signal from RF to baseband, ideally, the two baseband signals (in-phase and quadrature) should be orthogonal to each other with the same amplitude. Without loss of generality, we normalize the magnitude and the phase, then the two signals can be expressed as: | Given a single tone that converts the signal from RF to baseband, ideally, the two baseband signals (in-phase and quadrature) should be orthogonal to each other with the same amplitude. Without loss of generality, we normalize the magnitude and the phase, then the two signals can be expressed as: | ||
Line 60: | Line 60: | ||
where <m>I prime(t)</ | where <m>I prime(t)</ | ||
- | Please refer to the S.W. Ellingson' | + | Please refer to the S.W. Ellingson' |
Line 117: | Line 117: | ||
<WRAP round help 80%> | <WRAP round help 80%> | ||
- | * Questions? [[https://ez.analog.com/ | + | * Questions? [[ez>community/ |
</ | </ | ||