This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fmcmotcon1-ebz:quickstart:lv_setup_guide [10 Feb 2014 16:30] – [Getting Started] Andrei Cozma | resources:eval:user-guides:ad-fmcmotcon1-ebz:quickstart:lv_setup_guide [21 Feb 2014 14:53] – add the last step(release P2, then press S1) for starting the motor Lucian Sin | ||
---|---|---|---|
Line 33: | Line 33: | ||
{{ : | {{ : | ||
* Power on the ZedBoard | * Power on the ZedBoard | ||
+ | * After the board is programmed, in order to start the motor, the Emergency Stop button P2 must be released and then the Reset switch S1 must be pressed for a few seconds. | ||
|< 100% 100% >| | |< 100% 100% >| |