This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-fmcmotcon1-ebz:quickstart:chipscope [06 Feb 2014 17:49] – Updated to 14.6 version Adrian Costina | resources:eval:user-guides:ad-fmcmotcon1-ebz:quickstart:chipscope [10 Feb 2021 04:40] (current) – add retired Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== AD-FMCMOTCON1-EBZ ISE Project with Chipscope ====== | ====== AD-FMCMOTCON1-EBZ ISE Project with Chipscope ====== | ||
+ | {{page>/ | ||
This guide provides some quick instructions on how to setup the AD-FMCMOTCON1-EBZ on either: | This guide provides some quick instructions on how to setup the AD-FMCMOTCON1-EBZ on either: | ||
- | * [[xilinx> | ||
- | * [[xilinx> | ||
* [[http:// | * [[http:// | ||
Line 22: | Line 20: | ||
===== System Setup ===== | ===== System Setup ===== | ||
- | To setup the hardware follow the steps described in the [[|Low Voltage Drive Hardware Setup]] section. | + | To setup the hardware follow the steps described in the [[/ |
- | The FPGA must be programmed with the //**top.bit**// bitstream that results after compiling the ISE project. This bitstream | + | The FPGA must be programmed with the **top.bit** bitstream that results after compiling the ISE project. This has already been done, the bitstream was generated and it can be found in the ISE project' |
- | The operation of the system can be controlled and monitored using the Chipscope project from the //Downloads// section. | + | The operation of the system can be controlled and monitored using the Chipscope project from the **Downloads** section. |
===== Chipscope Interface ===== | ===== Chipscope Interface ===== | ||
- | The user interface uses Xilinx Chipscope 14.6. The project is available in the **Downloads** section. | + | The user interface uses Xilinx Chipscope 14.6. The project is available in the **Downloads** section. |
- | {{: | + | \\ {{: |
\\ The A section is used for control. | \\ The A section is used for control. | ||
^ Name ^ Width ^ Description ^ | ^ Name ^ Width ^ Description ^ | ||
- | | PWM | 32 | This registers sets the PWM value for controlling the motor. It must be larger than 0x480 | | + | | PWM | 32 | PWM value for controlling the motor. It must be larger than 0x480 and less than 0x800 | |
- | | GAIN | 2 | Button used change the amplification | + | | GAIN | 2 | Amplification |
- | | RUN_MOTOR | + | | RUN_MOTOR |
+ | | STAR_MOTOR | ||
+ | | CW_DIR | ||
| **Table 1 Section A parameter description** | | **Table 1 Section A parameter description** | ||
Line 52: | Line 52: | ||
| IT | IT current as read on the controller board | | | IT | IT current as read on the controller board | | ||
| VBUS | VBUS voltage as seen on the controller board | | | VBUS | VBUS voltage as seen on the controller board | | ||
+ | | SPEED | Time between a change of the HALL sensors state measured in 100ns units | | ||
+ | | POSITION | ||
| **Table 2 Section B parameter description** | | **Table 2 Section B parameter description** | ||
- | Section C is used to represent graphically the speed . | + | Section C is used to represent graphically the speed of the motor. |
^ Name ^ Description^ | ^ Name ^ Description^ | ||
- | | SPEED | + | | SPEED |
| **Table 3 Section C parameter description** | | **Table 3 Section C parameter description** | ||
- | Section D is used to plot the currents described in section B. | + | Section D is used to plot the currents |
{{navigation AD-FMCMOTCON1-EBZ# | {{navigation AD-FMCMOTCON1-EBZ# |