This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fmcmotcon1-ebz:quickstart:chipscope [21 Feb 2014 13:16] – [System Setup] Lucian Sin | resources:eval:user-guides:ad-fmcmotcon1-ebz:quickstart:chipscope [09 Jan 2021 00:32] – user interwiki links Robin Getz | ||
---|---|---|---|
Line 20: | Line 20: | ||
===== System Setup ===== | ===== System Setup ===== | ||
- | To setup the hardware follow the steps described in the [[http:// | + | To setup the hardware follow the steps described in the [[/ |
The FPGA must be programmed with the **top.bit** bitstream that results after compiling the ISE project. This has already been done, the bitstream was generated and it can be found in the ISE project' | The FPGA must be programmed with the **top.bit** bitstream that results after compiling the ISE project. This has already been done, the bitstream was generated and it can be found in the ISE project' | ||
Line 35: | Line 35: | ||
^ Name ^ Width ^ Description ^ | ^ Name ^ Width ^ Description ^ | ||
- | | PWM | 32 | This registers sets the PWM value for controlling the motor. It must be larger than 0x480 | | + | | PWM | 32 | PWM value for controlling the motor. It must be larger than 0x480 and less than 0x800 | |
- | | GAIN | 2 | Button used change the amplification | + | | GAIN | 2 | Amplification |
- | | RUN_MOTOR | + | | RUN_MOTOR |
+ | | STAR_MOTOR | ||
+ | | CW_DIR | ||
| **Table 1 Section A parameter description** | | **Table 1 Section A parameter description** | ||
Line 50: | Line 52: | ||
| IT | IT current as read on the controller board | | | IT | IT current as read on the controller board | | ||
| VBUS | VBUS voltage as seen on the controller board | | | VBUS | VBUS voltage as seen on the controller board | | ||
+ | | SPEED | Time between a change of the HALL sensors state measured in 100ns units | | ||
+ | | POSITION | ||
| **Table 2 Section B parameter description** | | **Table 2 Section B parameter description** | ||
- | Section C is used to represent graphically the speed . | + | Section C is used to represent graphically the speed of the motor. |
^ Name ^ Description^ | ^ Name ^ Description^ | ||
- | | SPEED | + | | SPEED |
| **Table 3 Section C parameter description** | | **Table 3 Section C parameter description** | ||
- | Section D is used to plot the currents described in section B. | + | Section D is used to plot the currents |
{{navigation AD-FMCMOTCON1-EBZ# | {{navigation AD-FMCMOTCON1-EBZ# |