This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-fmcmotcon1-ebz:introduction [29 Dec 2013 22:50] – update Andrei Cozma | resources:eval:user-guides:ad-fmcmotcon1-ebz:introduction [10 Feb 2021 04:39] (current) – add retired Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== ADI FMC Motor Control | + | ====== ADI FMC Motor Drive System |
+ | {{page>/ | ||
- | **The ADI FMC motor control solutions | + | **The ADI FMC motor drive solution solution |
- | * [[resources/ | + | |
- | * [[resources/ | + | |
+ | * **[[resources/ | ||
+ | |||
+ | |< 100% 33% 33% 34% >| | ||
+ | ^ AD-FMCMOTCON1-EBZ | ||
+ | | {{ : | ||
**Purpose** | **Purpose** | ||
- | * Provide an efficient | + | * Provide an efficient |
* Address power and isolation challenges encountered in motor control applications | * Address power and isolation challenges encountered in motor control applications | ||
* Provide accurate measurement of motor feedback signals | * Provide accurate measurement of motor feedback signals | ||
- | * FPGA interfacing capability | + | * Achieve flexible control with FPGA/SoC interface |
+ | * High speed industrial Ethernet interface | ||
**Added Value** | **Added Value** | ||
Line 20: | Line 27: | ||
* Increased versatility to be able to control different types of motors | * Increased versatility to be able to control different types of motors | ||
* Example reference designs showing how to use the control solution with Xilinx FPGAs and Simulink from Mathworks | * Example reference designs showing how to use the control solution with Xilinx FPGAs and Simulink from Mathworks | ||
+ | |||
+ | ===== Where to Buy ===== | ||
+ | |||
+ | <WRAP round box 90%> | ||
+ | **[[http:// | ||
+ | </ | ||
{{navigation AD-FMCMOTCON1-EBZ# | {{navigation AD-FMCMOTCON1-EBZ# | ||