Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:ad-fmcmotcon1-ebz:introduction:dc_control [28 Dec 2013 21:50]
Andrei Cozma Added navigation pane
resources:eval:user-guides:ad-fmcmotcon1-ebz:introduction:dc_control [18 Feb 2014 14:18]
Lucian Sin syntax error
Line 1: Line 1:
 ====== Brushed DC Motor Control ====== ====== Brushed DC Motor Control ======
  
-The Brushed DC motor is the simplest type of motor to control, all tht needs to be done is to vary the supply voltage and the motor'​s speed will vary proportional to the voltage. The most common technique used to vary the applied voltage is called **Pulse Width Modulation (PWM)**, where constant amplitude voltage pulses of varying widths are provided to the motor - the wider the pulse, the more energy transferred to the motor. ​If The frequency of the pulses is high enough that the motor’s inductance averages them, and it runs smooth.+The Brushed DC motor is the simplest type of motor to control, all that needs to be done is to vary the supply voltage and the motor'​s speed will vary proportional to the voltage. The most common technique used to vary the applied voltage is called **Pulse Width Modulation (PWM)**, where constant amplitude voltage pulses of varying widths are provided to the motor - the wider the pulse, the more energy transferred to the motor. The frequency of the pulses is high enough that the motor’s inductance averages them, and it runs smooth.
  
 A single transistor and diode can control the speed of a dc motor. ​ A single transistor and diode can control the speed of a dc motor. ​
resources/eval/user-guides/ad-fmcmotcon1-ebz/introduction/dc_control.txt · Last modified: 18 Feb 2014 14:18 by Lucian Sin