This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:ad-fmcdaq2-ebz:quickstart:a10soc [10 May 2018 10:32] – J29 Lars-Peter Clausen | resources:eval:user-guides:ad-fmcdaq2-ebz:quickstart:a10soc [05 Feb 2021 15:16] (current) – [IIO Oscilloscope Remote] Michael Hennerich | ||
---|---|---|---|
Line 334: | Line 334: | ||
If the Arria 10 SoC Development Kit is connected to a network with a DHCP server the IP address assigned to the board appears on the LCD. Alternatively you can query the IP address by running `ifconfig eth0` on the command line. To manually assign an IP address run `ifconfig eth0 // | If the Arria 10 SoC Development Kit is connected to a network with a DHCP server the IP address assigned to the board appears on the LCD. Alternatively you can query the IP address by running `ifconfig eth0` on the command line. To manually assign an IP address run `ifconfig eth0 // | ||
- | ===== IIO Oscilloscope Remote ===== | + |