This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fmcdaq2-ebz:quickstart:a10gx [10 Dec 2021 11:12] – [Required Software] Liviu Adace | resources:eval:user-guides:ad-fmcdaq2-ebz:quickstart:a10gx [16 Dec 2021 15:17] – [Nios II Terminal] Liviu Adace | ||
---|---|---|---|
Line 85: | Line 85: | ||
To start the Nios II Terminal use the following **nios2-terminal.exe** command. | To start the Nios II Terminal use the following **nios2-terminal.exe** command. | ||
Example of console: | Example of console: | ||
+ | <hidden Complete kernel boot log (Click to expand)> | ||
+ | <WRAP box bggreen> | ||
< | < | ||
ceshu@LADACE-L02:/ | ceshu@LADACE-L02:/ | ||
Line 180: | Line 182: | ||
Welcome to Buildroot | Welcome to Buildroot | ||
buildroot login: | buildroot login: | ||
- | </ | + | </code></ |
+ | </hidden> | ||
===== IIO Oscilloscope ===== | ===== IIO Oscilloscope ===== | ||
Line 211: | Line 214: | ||
To plot the captured waveforms go to **File** menu then click **New Plot**. Select the channels to plot and then click **Capture / Stop** button. | To plot the captured waveforms go to **File** menu then click **New Plot**. Select the channels to plot and then click **Capture / Stop** button. | ||
- | {{ resources: | + | {{ resources: |
===== More Information ===== | ===== More Information ===== | ||
* [[: | * [[: |