Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:ad-fmcdaq2-ebz:clocking [12 Sep 2017 14:22] – [Linux] Lars-Peter Clausenresources:eval:user-guides:ad-fmcdaq2-ebz:clocking [19 Jan 2018 10:14] (current) – rename xcomm_zynq -> master Alexandru Ardelean
Line 1: Line 1:
 ====== AD-FMCDAQ2-EBZ Clocking ====== ====== AD-FMCDAQ2-EBZ Clocking ======
  
-The AD9523-1 is responsible for generating and distributing all clock signals used on the AD-FMCDAQ2-EBZ platform.+===== Overview =====
  
-The AD-FMCDAQ2-EBZ platform only uses the second PLL of the AD9523-1 with the reference for the PLL being sourced from a external 125 MHz crystal. The PLL2 VCO has a locking range of 2910 MHz to 3100 MHz, with the external reference being 125 MHz the nominal output frequency of the VCO is 3000 MHz.+The [[adi>AD9523-1]] is responsible for generating and distributing all clock signals used on the AD-FMCDAQ2-EBZ platform. 
 + 
 +The AD-FMCDAQ2-EBZ platform only uses the second PLL of the AD9523-1 with the reference for the PLL being sourced from a external 125 MHz crystal. The PLL2 VCO has a locking range of 2940 MHz to 3100 MHz, with the external reference being 125 MHz the nominal output frequency of the VCO is 3000 MHz.
  
 The output of the PLL VCO is down divided to the target frequencies in two steps. First it is divided by either 3, 4 or 5, which gives a frequency of 1000 MHz, 750 MHz or 600 MHz respectively. This is the master clock frequency for the data converter system and shared between the DAC and ADC data path, all generated clocks are based of this master clock. The output of the PLL VCO is down divided to the target frequencies in two steps. First it is divided by either 3, 4 or 5, which gives a frequency of 1000 MHz, 750 MHz or 600 MHz respectively. This is the master clock frequency for the data converter system and shared between the DAC and ADC data path, all generated clocks are based of this master clock.
Line 22: Line 24:
 The ADC and DAC converter clocks are the reference clock for the ADC and DAC respectively and determine the sampling rate of the converter. If a deterministic latency relationship between the DAC and ADC datapath is required the DAC and ADC clock need to be in a (sub-)harmonic relationship to each other, otherwise their relationship can be chosen freely. The ADC and DAC converter clocks are the reference clock for the ADC and DAC respectively and determine the sampling rate of the converter. If a deterministic latency relationship between the DAC and ADC datapath is required the DAC and ADC clock need to be in a (sub-)harmonic relationship to each other, otherwise their relationship can be chosen freely.
  
-The ADC FPGA reference clock is the reference clock for the JESD204 clock-data-recovery (CDR) circuit as well the ADC data path inside the FPGASimilarly the DAC FPGA reference clock is the reference clock for the JESD204 transmit PLL and the DAC data path inside the FPGA.+The DAC has built-in interpolation filters that allow interpolation by a factor of 2, 4 or 8The interpolation factor and the DAC converter sample-rate decide the DAC data-input-rate. The data-input-rate is equal to the sample-rate divided by the interpolation factor.
  
-The SYSREF clocks are used for synchronization and to establish deterministic latency between the different components. The SYSREF clock must be a integer multiple of the local-multi-frame-clock (LMFC). The LMFC is a clock that is generated internally in the converters and FPGA and on the AD-FMCDAQ2-EBZ platform it's rate is 1/32 of the converter samplerate. This means the SYSREF clock frequency must be integer down divided of the converter samplerate / 32 (I.e. samplerate / {32, 64, 96, 128, ...}).+The ADC has built-in decimation filters that allow interpolation by a factor of 2, 4, 8 or 16. The decimation factor and the ADC converter sample-rate decide the ADC data-output-rate. The data-output-rate is equal to the sample-rate divided by the decimation factor. 
 + 
 +The JESD204 lane rates depend on the data-output/input-rates. On the AD-FMCDAQ2-EBZ both for the ADC and the DAC the lane-rate is equal to 10 times the data-rate. 
 + 
 +The ADC FPGA reference clock is the reference clock for the JESD204 clock-data-recovery (CDR) circuit as well the ADC data path inside the FPGA. Similarly the DAC FPGA reference clock is the reference clock for the JESD204 transmit PLL and the DAC data path inside the FPGA. These clocks should be set to the JESD204 lane-rate divided by 20. 
 + 
 +The SYSREF clocks are used for synchronization and to establish deterministic latency between the different components. The SYSREF clock must be a integer multiple of the local-multi-frame-clock (LMFC). The LMFC is a clock that is generated internally in the converters and FPGA and on the AD-FMCDAQ2-EBZ platform it's rate is 1/32 of the converter data-input/output-rate. This means the SYSREF clock frequency must be integer down divided of the converter data-rate / 32 (I.e. data-rate / {32, 64, 96, 128, ...}).
  
 The SYSREF clocks going to the converter and the FPGA must be configured for the same frequency. If a deterministic latency relationship between the DAC and ADC datapath is required the DAC and ADC SYSREF signals must be configured for the same frequency, otherwise the DAC and ADC datapath SYSREF clocks can be configured with different frequencies. The SYSREF clocks going to the converter and the FPGA must be configured for the same frequency. If a deterministic latency relationship between the DAC and ADC datapath is required the DAC and ADC SYSREF signals must be configured for the same frequency, otherwise the DAC and ADC datapath SYSREF clocks can be configured with different frequencies.
  
 ^ Clock ^ Frequency range ^ Comments ^ ^ Clock ^ Frequency range ^ Comments ^
-| PLL2 VCO | 3000 MHz | Tuning range of 2910 MHz to 3100 MHz |+| PLL2 VCO | 3000 MHz | Tuning range of 2940 MHz to 3100 MHz |
 | Master clock | 1000 MHz, 750 MHz, 600 MHz | PLL2 VCO divided by 3, 4 or 5 | | Master clock | 1000 MHz, 750 MHz, 600 MHz | PLL2 VCO divided by 3, 4 or 5 |
 | ADC converter clock | ≥ 312.5 MHz, ≤ 1000 MHz, Master clock / N<sub>ADC</sub> | | ADC converter clock | ≥ 312.5 MHz, ≤ 1000 MHz, Master clock / N<sub>ADC</sub> |
Line 35: Line 43:
 | DAC converter clock | ≥ 200 MHz, ≤ 1000 MHz, Master clock / N<sub>DAC</sub> | | DAC converter clock | ≥ 200 MHz, ≤ 1000 MHz, Master clock / N<sub>DAC</sub> |
 | DAC SYSREF clock | DAC converter clock / (N<sub>DAC_SYSREF</sub> * 32) | | DAC SYSREF clock | DAC converter clock / (N<sub>DAC_SYSREF</sub> * 32) |
-| ADC JESD204 lane rate | ADC converter clock * 1000 +| ADC JESD204 lane rate | ADC converter clock / ADC decimation factor 10 
-| DAC JESD204 lane rate | DAC converter clock * 1000 |+| DAC JESD204 lane rate | DAC converter clock / DAC interpolation factor 10 |
  
 ===== Examples ===== ===== Examples =====
Line 46: Line 54:
 ^ Clock ^ Frequency ^ Divider setting ^ ^ Clock ^ Frequency ^ Divider setting ^
 | Master clock | 1000 MHz | 3 | | Master clock | 1000 MHz | 3 |
-| ADC converter clock | 1000 MHZ | 1 | +| ADC converter clock | 1000 MHz | 1 | 
-| ADC FPGA reference clock | 500 MHZ | 2 | +| ADC FPGA reference clock | 500 MHz | 2 | 
-| ADC SYSREF clock | 7.8125 MHZ | 128 | +| ADC SYSREF clock | 7.8125 MHz | 128 | 
-| ADC FPGA SYSREF clock | 7.8125 MHZ | 128 |+| ADC FPGA SYSREF clock | 7.8125 MHz | 128 |
 | ADC JESD204 lane rate | 10 Gbps |  | | ADC JESD204 lane rate | 10 Gbps |  |
-| DAC converter clock | 1000 MHZ | 1 | +| DAC converter clock | 1000 MHz | 1 | 
-| DAC FPGA reference clock | 500 MHZ | 2 | +| DAC FPGA reference clock | 500 MHz | 2 | 
-| DAC SYSREF clock | 7.8125 MHZ | 128 | +| DAC SYSREF clock | 7.8125 MHz | 128 | 
-| DAC FPGA SYSREF clock | 7.8125 MHZ | 128 |+| DAC FPGA SYSREF clock | 7.8125 MHz | 128 |
 | DAC JESD204 lane rate | 10 Gbps |  | | DAC JESD204 lane rate | 10 Gbps |  |
  
Line 63: Line 71:
 ^ Clock ^ Frequency ^ Divider setting ^ ^ Clock ^ Frequency ^ Divider setting ^
 | Master clock | 750 MHz | 4 | | Master clock | 750 MHz | 4 |
-| ADC converter clock | 375 MHZ | 2 | +| ADC converter clock | 375 MHz | 2 | 
-| ADC FPGA reference clock | 187.5 MHZ | 4 | +| ADC FPGA reference clock | 187.5 MHz | 4 | 
-| ADC SYSREF clock | 2.9296875 MHZ | 256 | +| ADC SYSREF clock | 2.9296875 MHz | 256 | 
-| ADC FPGA SYSREF clock | 2.9296875 MHZ | 256 |+| ADC FPGA SYSREF clock | 2.9296875 MHz | 256 |
 | ADC JESD204 lane rate | 3.75 Gbps |  | | ADC JESD204 lane rate | 3.75 Gbps |  |
-| DAC converter clock | 250 MHZ | 3 | +| DAC converter clock | 250 MHz | 3 | 
-| DAC FPGA reference clock | 125 MHZ | 6 | +| DAC FPGA reference clock | 125 MHz | 6 | 
-| DAC SYSREF clock | 1.953125 MHZ | 384 | +| DAC SYSREF clock | 1.953125 MHz | 384 | 
-| DAC FPGA SYSREF clock | 1.953125 MHZ | 384 |+| DAC FPGA SYSREF clock | 1.953125 MHz | 384 |
 | DAC JESD204 lane rate | 2.5 Gbps |  | | DAC JESD204 lane rate | 2.5 Gbps |  |
 +
 +===== Replacing the Crystal Oscillator =====
 +
 +On the AD-FMCDAQ2-EBZ platform the reference clock signal for the AD9523-1 PLL2 is provided by a crystal oscillator (XO). The default populated crystal oscillator has a output frequency of 125 MHz, this results in a nominal AD9523-1 VCO frequency of 3 GHz, all other clock signals are integer down-divided versions of the signal.
 +
 +Other VCO frequencies are possible by replacing the XO with a suitable replacement producing a different frequency. Replacing the XO might require changing the VCO feedback divider settings to produce a valid VCO frequency. The VCO frequency must be in the range of 2940 MHz to 3100 MHz, otherwise the PLL2 will not lock.
 +
 +{{ :resources:eval:user-guides:ad-fmcdaq2-ebz:ad9523_pll2.png|}}
 +
 +The reference frequency can optionally be divided by the R2 (1-32) reference divider or multiplied by 2 using the frequency doubler. The result of this is the phase-frequency-detector (PFD) input frequency. The maximum PFD input frequency is 259 MHz. If the reference frequency exceeds this value the reference divider must be used to bring it into a valid range.
 +
 +''fPFD'' = ''fReference'' / ''R2'' * ''frequency_doubler''
 +
 +The VCO frequency is the PFD input frequency multiplied by the VCO feedback divider (N2).
 +
 +''fVCO'' = ''fPFD'' * ''N2''
 +
 +The feedback divider is the combination of two counters, the A and B counter. These are the settings that are programmed to the AD9523-1 configuration registers.
 +
 +''N2'' = ''4'' * ''B'' + ''A''
 +
 +Rearranging these formulas it is possible to compute the A and B counter settings from a known reference and a desired VCO frequency.
 +
 +''N2'' = ''fVCO'' / ''fPFD'' \\
 +''A'' = ''N2'' % ''4'' \\
 +''B'' = ''N2'' / ''4''
 +
 +==== Example: fXO = 122.88 MHz, fVCO = 2949.12 MHz ====
 +
 +In this example the frequency doubler is bypassed and the reference divider is set to 1. That means the PFD input frequency is equal to the reference frequency.
 +
 +''N2'' = ''fVCO'' / ''fPFD'' => ''N2'' = ''2949.12'' / ''122.88'' = ''24'' \\
 +''A'' = ''N2'' % ''4'' => ''A'' = ''24'' % ''4'' = ''0'' \\
 +''B'' = ''N2'' / ''4'' => ''B'' = ''24'' / ''4'' = ''6''
 +
 +^ Configuration Parameter ^ Setting ^
 +| PLL2 reference divider (R2) | 1 |
 +| PLL2 reference frequency doubler | Disabled |
 +| PLL2 feedback A divider | 0 |
 +| PLL2 feedback B divider | 6 |
  
 ===== Modifying the Clock Configuration ===== ===== Modifying the Clock Configuration =====
Line 80: Line 128:
 On Linux the default clock configuration is supplied through the [[https://www.devicetree.org/|devicetree]]. On Linux the default clock configuration is supplied through the [[https://www.devicetree.org/|devicetree]].
  
-The devicetree file that is used for the AD-FMCDAQ2-EBZ and contains the clock configuration is called [[linux.github>xcomm_zynq?arch/arm/boot/dts/adi-daq2.dtsi|adi-daq2.dtsi]]. This file contains nodes for the [[linux.github>xcomm_zynq?arch/arm/boot/dts/adi-daq2.dtsi#L8|AD9523-1]], the [[linux.github>xcomm_zynq?arch/arm/boot/dts/adi-daq2.dtsi#L105|AD9144]] and the [[linux.github>xcomm_zynq?arch/arm/boot/dts/adi-daq2.dtsi#L120|AD9680]]. Each node contains properties that describe the hardware setup and provide default configuration parameters. For information on how to edit devicetree please see [[:resources:eval:user-guides:ad-fmcomms2-ebz:software:linux:zynq_tips_tricks#customizing_the_device_tree_on_the_target|Tips & Tricks - Customizing the device tree on the target]].+The devicetree file that is used for the AD-FMCDAQ2-EBZ and contains the clock configuration is called [[linux.github>master?arch/arm/boot/dts/adi-daq2.dtsi|adi-daq2.dtsi]]. This file contains nodes for the [[linux.github>master?arch/arm/boot/dts/adi-daq2.dtsi#L8|AD9523-1]], the [[linux.github>master?arch/arm/boot/dts/adi-daq2.dtsi#L105|AD9144]] and the [[linux.github>master?arch/arm/boot/dts/adi-daq2.dtsi#L120|AD9680]]. Each node contains properties that describe the hardware setup and provide default configuration parameters. For information on how to edit devicetree please see [[:resources:eval:user-guides:ad-fmcomms2-ebz:software:linux:zynq_tips_tricks#customizing_the_device_tree_on_the_target|Tips & Tricks - Customizing the device tree on the target]].
  
 To change the clocking configuration the properties of the AD9523-1 node can be modified. The following lists the most important properties for the AD-FMCDAQ2-EBZ and their corresponding hardware setting. The function of each of these settings and how to choose their value has been discussed above. For more information refer to the [[:resources:tools-software:linux-drivers:iio-pll:ad9523|AD9523-1 driver documenation]]. To change the clocking configuration the properties of the AD9523-1 node can be modified. The following lists the most important properties for the AD-FMCDAQ2-EBZ and their corresponding hardware setting. The function of each of these settings and how to choose their value has been discussed above. For more information refer to the [[:resources:tools-software:linux-drivers:iio-pll:ad9523|AD9523-1 driver documenation]].
Line 87: Line 135:
 | Frequency of the external VCXO | ''adi,vcxo-freq'' | | Frequency of the external VCXO | ''adi,vcxo-freq'' |
 | PLL2 reference divider (R2) | ''adi,pll2-r2-div'' | | PLL2 reference divider (R2) | ''adi,pll2-r2-div'' |
-| PLL2 feedback divider | ''adi,pll2-ndiv-a-cnt''+| PLL2 feedback divider A counter | ''adi,pll2-ndiv-a-cnt''
-| PLL2 feedback divider | ''adi,pll2-ndiv-b-cnt'' |+| PLL2 feedback divider B counter | ''adi,pll2-ndiv-b-cnt'' |
 | PLL2 VCO output divider (M1) | ''adi,pll2-vco-diff-m1'' | | PLL2 VCO output divider (M1) | ''adi,pll2-vco-diff-m1'' |
  
Line 112: Line 160:
  
 Based on the data output and input rates the converter drivers will automatically calculate the JESD204 lane rate and propagate the configuration to the JESD204 receiver and transmitter drivers. These drivers will update the high-speed transceiver configuration accordingly. This means no additional manual configuration is necessary to setup the JESD204 link. Based on the data output and input rates the converter drivers will automatically calculate the JESD204 lane rate and propagate the configuration to the JESD204 receiver and transmitter drivers. These drivers will update the high-speed transceiver configuration accordingly. This means no additional manual configuration is necessary to setup the JESD204 link.
-==== No-OS ====+ 
resources/eval/user-guides/ad-fmcdaq2-ebz/clocking.txt · Last modified: 19 Jan 2018 10:14 by Alexandru Ardelean