This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fmcadc5-ebz [28 Jun 2017 13:59] – Add no-OS drivers link Dragos Bogdan | resources:eval:user-guides:ad-fmcadc5-ebz [06 Mar 2018 14:42] – changed the branch used Adrian Costina | ||
---|---|---|---|
Line 30: | Line 30: | ||
The HDL reference design is built around a processor as in an embedded system. You may use either Linux or No-OS software to demonstrate the design (details in the downloads section). In order to run the HDL with the No-OS application, | The HDL reference design is built around a processor as in an embedded system. You may use either Linux or No-OS software to demonstrate the design (details in the downloads section). In order to run the HDL with the No-OS application, | ||
- | At the time of this writing, we are using the ' | + | The [[https:// |
Once the bit file is ready, follow these instructions to build the elf file. This assumes you are following our directory structures. If you are not, just get the idea from here and port it to your environment. However you have to figure out things on your own. | Once the bit file is ready, follow these instructions to build the elf file. This assumes you are following our directory structures. If you are not, just get the idea from here and port it to your environment. However you have to figure out things on your own. | ||
- Clone [[https:// | - Clone [[https:// | ||
- | - **Checkout the ' | + | - **Checkout the latest release |
- Change the directory to `ad-fmcadc5-ebz/ | - Change the directory to `ad-fmcadc5-ebz/ | ||
- Make the elf file by running `make HDF-FILE=< | - Make the elf file by running `make HDF-FILE=< |