Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:user-guides:ad-fmcadc5-ebz [20 Mar 2018 17:03] – Cleanup Adrian Costina | resources:eval:user-guides:ad-fmcadc5-ebz [14 Feb 2019 10:21] – Fixed broken links Adrian Costina |
---|
| |
===== Introduction ===== | ===== Introduction ===== |
{{ :resources:eval:user-guides:ad-fmcadc5-ebz:ad-fmcadc5-ebz.jpg?400|}} The [[http://www.xilinx.com/products/boards-and-kits/1-5l1boj.html|AD-FMCADC5-EBZ]] is a high speed single channel data acquisition board featuring two [[adi>AD9625]] ADCs. The board is provisioned to sample the single input at an effective sampling rate of 5GSPS, with both the ADCs running at 2.5GHz and sampling at both edges (the clocks are 180 out of phase to each other). The board is a variant of [[http://www.fidus.com/analog-digital-converters|FSF-AD15000A]] from Fidus Systems Inc. | {{ :resources:eval:user-guides:ad-fmcadc5-ebz:ad-fmcadc5-ebz.jpg?400|}} The [[adi>AD-FMCADC5-EBZ|AD-FMCADC5-EBZ]] is a high speed single channel data acquisition board featuring two [[adi>AD9625]] ADCs. The board is provisioned to sample the single input at an effective sampling rate of 5GSPS, with both the ADCs running at 2.5GHz and sampling at both edges (the clocks are 180 out of phase to each other). The board is a variant of [[https://fidus.com/fmcs/|FSF-AD15000A]] from Fidus Systems Inc. |
| |
Although this board does meet most of the FMC specifications, it is not meant as a [[wp>Commercial_off-the-shelf|commercial off the shelf]] (COTS) board. If a commercial, ready to go integrate product is required, please refer to one of the many FMC manufacturers. | Although this board does meet most of the FMC specifications, it is not meant as a [[wp>Commercial_off-the-shelf|commercial off the shelf]] (COTS) board. If a commercial, ready to go integrate product is required, please refer to one of the many FMC manufacturers. |
| |
The AD-FMCADC5-EBZ uses a 2.5GHz crystal. The two AD9625 devices are clocked from the same clock source, but 180 degrees out of phase. | The AD-FMCADC5-EBZ uses a 2.5GHz crystal. The two AD9625 devices are clocked from the same clock source, but 180 degrees out of phase. |
| |
==== Analog Front End ==== | |
| |
===== Running No-OS Application & Achieving Interleaving at 5GSPS ===== | ===== Running No-OS Application & Achieving Interleaving at 5GSPS ===== |
- Make the elf file by running `make HDF-FILE=<HDL-REPO>/projects/fmcadc5/vc707/fmcadc5_vc707.sdk/system_top.hdf` | - Make the elf file by running `make HDF-FILE=<HDL-REPO>/projects/fmcadc5/vc707/fmcadc5_vc707.sdk/system_top.hdf` |
| |
The make will build the default 'hello-world', but we only need the bsp and I am no fan of eclipse, hence this method. If you are more comfortable with the GUI, import all the files (or folders) that the make uses. | The make will build the default 'hello-world', but we only need the bsp and I am no fan of eclipse, therefore this method. If you are more comfortable with the GUI, import all the files (or folders) that the make uses. |
| |
A typical run looks like this: | A typical run looks like this: |
| |
<WRAP center round download> | <WRAP center round download> |
* AD-FMCADC5-EBZ No-OS - https://github.com/analogdevicesinc/no-OS/tree/master/ad-fmcadc5-ebz | * AD-FMCADC5-EBZ No-OS - https://github.com/analogdevicesinc/no-OS/tree/master/fmcadc5 |
</WRAP> | </WRAP> |
| |
| |