This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fmcadc2-ebz [14 May 2015 00:05] – old revision restored (15 Apr 2015 21:38) Robin Getz | resources:eval:user-guides:ad-fmcadc2-ebz [17 Jul 2015 09:04] – change ADP1753 link Lucian Sin | ||
---|---|---|---|
Line 12: | Line 12: | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
- | * [[adi>ADP1753A]] is a low dropout linear regulators that operate from 1.6 V to 3.6 V and provide up to 800mA of output current. | + | * [[adi>ADP1753]] is a low dropout linear regulators that operate from 1.6 V to 3.6 V and provide up to 800mA of output current. |
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> |