This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:eval:user-guides:ad-96tof1-ebz:ug_host_system_setup [28 Nov 2019 09:33] – created Andrei Cozma | resources:eval:user-guides:ad-96tof1-ebz:ug_host_system_setup [03 Jan 2021 21:46] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 2: | Line 2: | ||
==== Required hardware ==== | ==== Required hardware ==== | ||
- | * [[https:// | + | * [[adi>en/ |
* [[https:// | * [[https:// | ||
* DragonBoard410c 12V power supply (e.g. AK-ND-49) | * DragonBoard410c 12V power supply (e.g. AK-ND-49) | ||
Line 8: | Line 8: | ||
==== Power on sequence ==== | ==== Power on sequence ==== | ||
- | * Plug the SD card that came in the AD-96TOF1-EBZ box into the DragonBoard410c SD card slot. To benefit from the most recent software updates it is higly recommended to update the SD card with the [[https:// | + | * Plug the SD card that came in the AD-96TOF1-EBZ box into the DragonBoard410c SD card slot. To benefit from the most recent software updates it is highly |
* Make sure that switch S6 on the DragonBoard410C is set to SD BOOT (position 2 ON, all others OFF) | * Make sure that switch S6 on the DragonBoard410C is set to SD BOOT (position 2 ON, all others OFF) | ||
* Connect USB cable to the host PC | * Connect USB cable to the host PC | ||
* Connect the 5V power supply to the camera board and set the camera power switch S2 to on. Once the camera board is powered up the DS1 LED will turn on | * Connect the 5V power supply to the camera board and set the camera power switch S2 to on. Once the camera board is powered up the DS1 LED will turn on | ||
* Connect the 12V power supply to the DragonBoard 410c. Once power is connected to the DragonBoard the system will boot the Linux OS from the SD card | * Connect the 12V power supply to the DragonBoard 410c. Once power is connected to the DragonBoard the system will boot the Linux OS from the SD card | ||
- | * Wait for the board to finish booting. The booting progress can be monitored by observing the user leds 1, 2, 3 and 4 on the DragonBoard410c which are placed between the two USB type A connectors. During boot the leds (especially led 3 and 1) will blink very rapidly. When led 1 is the only one left bliking | + | * Wait for the board to finish booting. The booting progress can be monitored by observing the user leds 1, 2, 3 and 4 on the DragonBoard410c which are placed between the two USB type A connectors. During boot the leds (especially led 3 and 1) will blink very rapidly. When led 1 is the only one left blinking |
{{ : | {{ : |