This shows you the differences between two versions of the page.
Previous revisionNext revision | |||
— | resources:eval:user-guide:adskpmb10-ev-fmcz [02 Jun 2023 04:04] – [Schematic, PCB Layout, Bill of Materials] Chelsea Faye Aure | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== ADSKPMB10-EV-FMCZ User Guide ====== | ||
+ | ===== Features ===== | ||
+ | * Fully Isolated PMOD-to-FMC interposer board | ||
+ | * Software programmable bipolar input ranges (±1.1 V to ±11.0 V) \\ | ||
+ | * GΩ input impedance allows direct interface with sensors | ||
+ | * On-board 5 V reference and buffer | ||
+ | * Complete power management solution | ||
+ | * SPI-/ | ||
+ | * PC software for control and data analysis of time and frequency domain | ||
+ | |||
+ | ===== Evaluation Kit Contents ===== | ||
+ | * Fully Isolated PMOD-to-FMC Board | ||
+ | * PGIA+ADAQ4003 Data Acquisition Board | ||
+ | |||
+ | ===== Equipment Needed ===== | ||
+ | * System Demonstration Platform Board: [[adi> | ||
+ | * DC/AC signal source (Audio Precision or similar high performance signal source) | ||
+ | * SMA cables | ||
+ | * XLR-SMA interposer board | ||
+ | * Standard USB A to USB mini-B | ||
+ | * PC running Windows 7, 8, or 10 with USB 2.0 port | ||
+ | |||
+ | ===== Software Required ===== | ||
+ | * [[ADI> | ||
+ | |||
+ | ===== General Description ===== | ||
+ | The [[ADI> | ||
+ | |||
+ | The Precision Medium Bandwidth Data Acquisition Solution features a discrete programmable gain instrumentation amplifier (PGIA) that was built using a 30V, High Speed, Low Noise, Low Bias Current, JFET Operational Amplifier, the [[adi> | ||
+ | |||
+ | The Fully Isolated PMOD-to-FMC interposer board was designed using a Low Noise, 1A, 1MHz Push-Pull DC/DC Driver with Duty Cycle Control, the [[adi> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | // | ||
+ | |||
+ | ===== Getting Started ===== | ||
+ | The following section contains the installation instructions for the ADSKPMB10-EV-FMCZ Evaluation Software and the drivers for the SDP hardware required for operation of the software. The evaluation software provides a graphical user interface (GUI) for quick evaluation of the ADSKPMB10-EV-FMCZ. | ||
+ | |||
+ | ==== Software Installation Procedures ==== | ||
+ | Download the evaluation board software from the [[ADI> | ||
+ | To install the software, take the following steps: | ||
+ | * Run the [[ADI> | ||
+ | * Run the [[ADI> | ||
+ | |||
+ | === Warning === | ||
+ | <note warning> | ||
+ | |||
+ | |||
+ | === Installing the ADSKPMB10-EV-FMCZ Evaluation Software === | ||
+ | ++++ Click here to see the complete installation instructions. | | ||
+ | To install the ADSKPMB10-EV-FMCZ Evaluation Software, follow these steps: | ||
+ | - Start the Windows operating system and download the software from the ADSKPMB10-EV-FMCZ product page on the Analog Devices website. | ||
+ | - Unzip the downloaded file. <WRAP centeralign> | ||
+ | - Double-click the **setup.exe** file to begin the evaluation board software installation (see Figure 3). <WRAP centeralign> | ||
+ | - Select a location to install the software and click **Next**. The default location is **C: | ||
+ | - A license agreement appears. Read the agreement, and then select **I accept the License Agreement**, | ||
+ | - An installation summary displays. Click **Next** to continue. <WRAP centeralign> | ||
+ | - A dialog box shows the installation progress. <WRAP centeralign> | ||
+ | - The dialog box informs the user when the installation is complete. Click **Finish**. <WRAP centeralign> | ||
+ | - The setup for the installation of the SDP-H1 board drivers automatically loads. | ||
+ | ++++ | ||
+ | |||
+ | |||
+ | === Installing the SDP-H1 Board Drivers === | ||
+ | ++++ Click here to see the complete installation instructions. | | ||
+ | After installation of the evaluation board software completes, a welcome window displays for the installation of the SDP-H1 system demonstration platform board drivers. Then, take the following steps: | ||
+ | - Ensure all other applications are closed and click **Next**. <WRAP centeralign> | ||
+ | - A license agreement appears. Read the agreement, and then click **I Agree**. <WRAP centeralign> | ||
+ | - Make sure to select the **Pre-Requisites** checkbox, then click **Next**< | ||
+ | - Select a location to install the drivers and click **Install**. <WRAP centeralign> | ||
+ | - Installation of the SDP drivers begins. <WRAP centeralign> | ||
+ | - A dialog box appears asking to install the SDP software available with the SDP-H1. Click **Install**. <WRAP centeralign> | ||
+ | - To complete the drivers installation, | ||
+ | - After installing the drivers, restart the PC prior to using the ADSKPMB10-EV-FMCZ Evaluation Software. A dialog box opens, giving the following options: **Restart**, | ||
+ | Later**. Click **Restart**. <WRAP centeralign> | ||
+ | |||
+ | |||
+ | |||
+ | ++++ | ||
+ | ==== Hardware Connection ==== | ||
+ | The ADSKPMB10-EV-FMCZ connects to the SDP-H1. The SDP-H1 board serves as the communication link between the PC and ADSKPMB10-EV-FMCZ. Figure 17 shows the connections between the ADSKPMB10-EV-FMCZ and the SDP-H1 board. | ||
+ | |||
+ | |||
+ | === Connecting ADSKPMB10-EV-FMCZ and SDP-H1 to a PC === | ||
+ | After installing the ACE software, follow these steps to set up the ADSKPMB10-EV-FMCZ and SDP-H1, as shown in Figure 18. | ||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | - Ensure all configuration links are in the appropriate positions, as detailed in Table 1. | ||
+ | - Connect the ADSKPMB10-EV-FMCZ securely to the 160-way connector on the SDP-H1. The ADSKPMB10-EV-FMCZ does not require an external power supply adapter. | ||
+ | - Connect the SDP-H1 to the PC through the USB cable and power it up with the 12 V wall adapter included in the SDP-H1 kit. | ||
+ | |||
+ | |||
+ | |||
+ | ===Verifying the Board Connection=== | ||
+ | After completing Software Installation Procedures and Evaluation Board Setup, follow these steps to verify the board connection: | ||
+ | - Run the **Found New Hardware Wizard** after the SDP-H1 system demonstration platform board is plugged into the PC. If using Windows XP, search for the SDP-H1 drivers. Automatically search for the drivers of the SDP-H1 system demonstration platform board, if prompted by the operating system. | ||
+ | - Check the evaluation board is connecting to the PC correctly using the **Device Manager** of the PC. Access the **Device Manager** as follows: | ||
+ | - Right click **My Computer** and then click **Manage**. | ||
+ | - A dialog box appears seeking permission to allow the program to make changes to the computer. Click **Yes**. | ||
+ | - The **Computer Management** window appears. Click **Device Manager** from the list of System Tools (see Figure 18) | ||
+ | - If the SDP-H1 system demonstration platform board appears under **ADI Development Tools**, the driver software is installed and the evaluation board is connecting to the PC correctly. <WRAP centeralign> | ||
+ | |||
+ | |||
+ | === Disconnecting ADSKPMB10-EV-FMCZ === | ||
+ | Disconnect the ADSKPMB10-EV-FMCZ from the SDP-H1 by either: | ||
+ | - Turning off the power from the SDP-H1 by unplugging the 12 V wall wart adapter. | ||
+ | - Pressing the reset tact switch located alongside the mini-USB port on the SDP-H1. | ||
+ | ===== Hardware Description and Performance ===== | ||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | Figure 19 shows the simplified block diagram of the [[adi> ADSKPMB10-EV-FMCZ]], | ||
+ | |||
+ | The PMOD-to-FMC interposer board consists of the digital isolators, [[adi> ADuM152N]] (U1) and [[adi> ADuM120N]] (U7), the DC/DC regulator [[adi> LT3999]] (U6), and lastly, the LDO regulators, [[adi> ADP7105]] (U2) and [[adi> ADP150N]] (U4). | ||
+ | |||
+ | The PGIA + ADAQ4003 Data Acquisition Board consists of the [[adi> | ||
+ | |||
+ | ==== Power Supplies ==== | ||
+ | |||
+ | === Fully Isolated PMOD-to-FMC Interposer Board === | ||
+ | The Fully Isolated PMOD-to-FMC interposer board was designed using a Low Noise, 1A, 1MHz Push-Pull DC/DC Driver with Duty Cycle Control, the [[adi> | ||
+ | |||
+ | The interposer board was designed to cater multiple VIO voltage levels. The user has 3 options on the FMC VIO side and by default, the VIO is connected or set by FMC's VADJ pin. 3.3 V and 1.8 V is also available in case other VIO voltage level is needed as shown in Figure 20 below. <WRAP centeralign> | ||
+ | |||
+ | On the PMOD side, the user has an option to connect the VCC pin of the PMOD Data Acquisition device directly to LT3999' | ||
+ | <WRAP centeralign> | ||
+ | |||
+ | === PGIA + ADAQ4003 Data Acquisition Board === | ||
+ | The SDP-H1 supplies 3.3 V to power the rails for the different components on the PGIA + ADAQ4003 Data Acquisition Board. The ADAQ4003 µModule use four power supply pins: the ADC driver positive supply (VS+), the ADC driver negative supply (VS−), the core ADC supply (VDD), and the digital input and output interface supply (VIO). The VIO pin allows the direct interface with any logic between 1.8 V and 5.5 V. A combination of the ADP5070 (dual, high-performance dc-to-dc switching regulator), the LT3032 (dual, low noise, positive and negative low dropout voltage linear regulator), and the LT3023 (dual, micropower, low noise, low dropout regulator) can generate independently regulated positive and negative rails for all four power supply pins, including ±15 V rails for any additional signal conditioning. | ||
+ | |||
+ | |||
+ | <WRAP centeralign> | ||
+ | {{ : | ||
+ | |||
+ | |||
+ | Each supply is decoupled at the PGIA + ADAQ4003 Data Acquisition Board entrance and device connection. A single, on-board ground plane minimizes the effect of the high frequency noise interference. | ||
+ | |||
+ | In addition, the PGIA + ADAQ4003 Data Acquisition Board can be powered from a benchtop power supply of ±16 V. The +16 V, −16 V, and GND test points are available on board to support this function. When bench power is used, the on-board power supplies are no longer required, and the link between the output pin of the ADP5070 must be removed, that is, uninstall R65 and R66. | ||
+ | |||
+ | Take the following steps to set up the PGIA + ADAQ4003 Data Acquisition Board when using a benchtop power supply of ±16 V: | ||
+ | - Connect the PGIA + ADAQ4003 Data Acquisition Board to the Isolated PMOD-to-FMC interposer board at the P1 header (see Figure 17). | ||
+ | - Connect the Isolated PMOD-to-FMC interposer board to the SDP-H1 via the 160-pin FMC connector. | ||
+ | - Connect the USB and a 12 V power adapter to the SDP-H1. Ensure that the software and drivers are installed. | ||
+ | - Connect the +16 V and −16 V bench supplies to the +16 V and −16 V test points on the PGIA + ADAQ4003 Data Acquisition Board. Connect also the bench supply ground to the GND test point (see Figure 22). | ||
+ | - Power up the benchtop supply. The +16 V supply rail draws approximately 25 mA, and the −16 V supply rail draws approximately 20 mA. <WRAP centeralign> | ||
+ | |||
+ | The evaluation kit is now ready to use. Note that by default, the PGIA + ADAQ4003 Data Acquisition Board are set up to accept a differential input with a 22 V range. | ||
+ | |||
+ | |||
+ | |||
+ | ==== SDP-H1 Controller Board ==== | ||
+ | The [[adi> | ||
+ | |||
+ | The SDP-H1 has an FMC low pin count (LPC) connector with full differential LVDS and singled-ended LVCMOS support. It also features the 160-pin connector, found on the [[adi> | ||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | ==== Analog Inputs ==== | ||
+ | The analog input signals of the board are the Subminiature Version A (SMA) connectors, J3 and J4, by default. Similarly, an option for the Subminiature Version B (SMB) connectors, J1 and J2 are also available. These analog inputs are fed to the dedicated amplifier circuitry, [[adi> | ||
+ | |||
+ | The analog inputs are fully differential by default, with both inputs floating with high impedance. Thus, ensure the signal source is properly biased to a common-mode voltage. See Table 2 for input range configuration and control. | ||
+ | |||
+ | Measure the true dynamic range of the board by connecting the two inputs to the board’s ground reference by using SMA terminators (see Figure 23). | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | For dynamic performance, | ||
+ | |||
+ | ==== Hardware Link Options ==== | ||
+ | Set the multiple link options correctly for the appropriate operating setup before applying the power and signal to the ADSKPMB10-EV-FMCZ. Table 1 shows the default link positions for the ADSKPMB10-EV-FMCZ. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | {{ : | ||
+ | |||
+ | |||
+ | |||
+ | |||
+ | ==== Precision Medium Bandwidth Data Acquisition Solution ==== | ||
+ | This Data Acquisition Solution has 4 gain options, as shown in Table 2. The gain of the signal chain can be controlled by changing the logic levels of the ADG1209 A0 and A1 pins. This can be done through the software or by adjusting the jumpers JA0 and JA1. | ||
+ | \\ | ||
+ | <WRAP centeralign> | ||
+ | \\ | ||
+ | Figure 24 shows the Dynamic Range vs. Gain Performance of the data acquisition solution. | ||
+ | \\ | ||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | \\ | ||
+ | Figure 25 shows the Signal-to-Noise Ratio (SNR) vs. Frequency vs. Gain Performance of the data acquisition solution. | ||
+ | \\ | ||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | \\ | ||
+ | Figure 26 shows the Total Harmonic Distortion (THD) vs. Frequency vs. Gain Performance of the data acquisition solution. | ||
+ | \\ | ||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | \\ | ||
+ | |||
+ | ===== Software GUI Setup ===== | ||
+ | |||
+ | |||
+ | ==== Launching the Software ==== | ||
+ | After installing the ADSKPMB10-EV-FMCZ Evaluation Software Installer (see the Software Installation Procedures section), run the software with either of the following methods: | ||
+ | * Navigate to the destination folder of the ADSKPMB10-EV-FMCZ Evaluation Software Installer selected during the installation procedure and run the **ADSKPMB10-EV-FMCZ.exe** file. | ||
+ | * Click **Start > All Programs > Analog Devices > ADSKPMB10-EV-FMCZ**. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | ==== Establishing Hardware Connection ==== | ||
+ | After the ADSKPMB10-EV-FMCZ Evaluation Software initializes, | ||
+ | |||
+ | If the software does not detect a valid ADSKPMB10-EV-FMCZ evaluation board, a connectivity error dialog box appears (see Figure 28). Clicking the **Rescan** button instructs the software to try to detect the hardware again. Clicking the **Cancel** button causes the software to boot in offline mode. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | ==== Navigating the Evaluation Software ==== | ||
+ | <WRAP centeralign> | ||
+ | |||
+ | === Front Panel Overview === | ||
+ | The ADSKPMB10-EV-FMCZ Evaluation Software front panel is shown in Figure 29. The following sections describe the various software controls accessible on the front panel. | ||
+ | |||
+ | //**File Menu**// | ||
+ | |||
+ | The **File** menu (Label 1 in Figure 29) provides the following options: | ||
+ | * **Save Captured Data (Ctrl + S):** saves the current session in a **.csv** file. The user is prompted to either choose or enter the path of the file in the **Save As** dialog box. This saved file can be loaded by the software at a future time to display previously captured data. | ||
+ | * **Load Captured Data (Ctrl + O):** opens the **Load File** dialog box and the user is prompted to load the previously saved evaluation software session files (**.csv**). Don't forget to click **Single Capture** to view the saved session files. | ||
+ | * **Take Screenshot: | ||
+ | * **Print Screenshot: | ||
+ | * **Exit:** closes the front panel and exits the software. | ||
+ | |||
+ | |||
+ | //** Edit Menu **// | ||
+ | |||
+ | The **Edit** menu (Label 1 in Figure 29) provides the following options: | ||
+ | * **Reinitialize Default Values:** resets a subset of the evaluation software front panel controls to the default state. | ||
+ | |||
+ | //** Help Menu **// | ||
+ | |||
+ | The **Help** menu (Label 1 in Figure 29) provides the following options: | ||
+ | * **Analog Devices Website:** opens the [[adi> ]] Analog Devices webpage in the default browser of the PC. | ||
+ | * **ADAQ4003 Evaluation Hardware Info:** opens the [[adi> ADAQ4003]] product page in the default browser of the PC. | ||
+ | * **Context Help (Ctrl + H):** displays a context help dialog box, which displays information about the various software controls when the mouse hovers over them. | ||
+ | * **About (Ctrl + A):** displays version and copyright information of the evaluation software in a dialog box. | ||
+ | |||
+ | |||
+ | //** Display Tabs **// | ||
+ | |||
+ | The following five tabs are located at the top of the front panel (Label 2 in Figure 29): **Configure, | ||
+ | |||
+ | //** Single Capture Button **// | ||
+ | |||
+ | Click **Single Capture** (Label 3 in Figure 29) to perform a single set of conversions. The number of conversions performed is set with the **Samples** dropdown list, which is located to the left of the **Single Capture** control. | ||
+ | |||
+ | //** Continuous Capture Button **// | ||
+ | |||
+ | Click **Continuous Capture** (Label 4 in Figure 29) to perform repeated sets of conversions. The number of conversions performed per set is set with the **Samples** dropdown list. | ||
+ | |||
+ | //** Samples Dropdown List **// | ||
+ | |||
+ | The **Samples** dropdown list (Label 5 in Figure 29) sets the number of conversions that are performed when **Single Capture** or **Continuous Capture** is clicked. | ||
+ | |||
+ | //** Status Bar **// | ||
+ | |||
+ | The status bar (Label 6 in Figure 29) displays information about the current process being completed by the evaluation software. The **Status Bar** includes a **Busy** indicator, which displays if the software is busy performing a task such as performing conversions, | ||
+ | |||
+ | |||
+ | ---- | ||
+ | |||
+ | |||
+ | === Configure Tab View=== | ||
+ | |||
+ | |||
+ | Figure 29 shows the **Configure** tab view. The **Configure** tab provides controls for configuring the connected device and software settings. The Configure tab view contains the following controls and indicators: | ||
+ | |||
+ | * **Eval Board Connected** (Label 6 in Figure 29): indicates that the evaluation board is connected to the software. | ||
+ | * **Oversampling Ratio** (Label 7 in Figure 29): sets the oversampling ratio applied to the captured data. After this control is set to any value other than **None**, the software sums up the consecutive conversion results together to increase effective resolution. The number of conversions summed together is set by the **Oversampling Ratio** control. | ||
+ | * **Throughput (kSPS)** (Label 8 in Figure 29): sets the throughput of the connected device. The maximum value of this control is automatically set to reflect the maximum achievable throughput of the connected device, given the state of the **Status Bits** and **Turbo Mode** controls. See the relevant [[adi> | ||
+ | * **Gain Control** (Label 8 in Figure 29): sets the PGIA Front-end Gain of the device. The user can choose from 1, 2, 5, or 10. | ||
+ | * **Voltage Reference (VREF)** (Label 10 in Figure 29): sets the VREF used in data analysis such as when calculating LSB Size (see Label 2 in Figure 30), or measured voltage in the waveform graph (see the Waveform Tab View section. This control must be set to match the VREF used on the connected evaluation board. | ||
+ | * **Device Config Settings** (Label 11 in Figure 29): configures the connected device user configuration register settings. See the relevant ADAQ4003 device data sheet for a detailed description of the user configuration register and the device features. | ||
+ | * **Status Bits:** enables or disables the status bits for the connected device. | ||
+ | * **Span Compression: | ||
+ | * **High-Z Mode:** enables or disables high-Z mode. | ||
+ | * **Turbo Mode:** enables or disables turbo mode for the connected device. | ||
+ | * **Read Register** (Label 12 in Figure 29): reads the device user register. When **Read Register** is clicked, the contents of the connected device register are read to update the **Device Config Settings** items accordingly. | ||
+ | * Device configuration settings display (Label 13 in Figure 29): displays the status of the user register when **Read Register** is clicked. Each of the following indicators displays the state of the corresponding settings: | ||
+ | * **Status Bits, Span Compression, | ||
+ | * **Overvoltage Clamp Flag:** indicates the status of the OV clamp flag in the user configuration register of the connected device. When this indicator is red, the OV flag is low, indicating the presence of an overvoltage event. | ||
+ | * **Status Bits Indicators** (Label 14 in Figure 29): displays the configuration settings of the device as indicated by the status bits. The status bits are enabled with the **Status Bits** control in the **Device Config Settings** pane (Label 11 in Figure 29). The **Status Bits Indicators** are only updated after conversions are performed with the **Single Capture** or **Continuous Capture** controls when the status bits are enabled on the connected device. The status bit functionality is described in the relevant ADAQ4003 device data sheet. | ||
+ | * The **Span Compression, | ||
+ | * **Overvoltage Clamp Flag:** displays whether the OV clamp flag in the status bits indicated an overvoltage event in any of the conversions in the most recently displayed results. When this indicator is red, the OV flag is low, indicating the presence of an overvoltage event. See the ADAQ4003 datasheet for more details on the OV clamp flag. | ||
+ | |||
+ | |||
+ | ----------------- | ||
+ | === Waveform Tab View === | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | Figure 30 shows the **Waveform** tab view. The **Waveform** tab view shows the time domain representation of the conversion results from the connected device, as well as several analysis items. The **Waveform** tab view contains the following controls and indicators: | ||
+ | * **Waveform graph** (Label 1 in Figure 30): displays the time domain plot of the most recently captured or loaded conversion results. The scale and range of the waveform graph can be set in the **Waveform Analysis** box by double clicking on the **Minimum Value** and **Maximum Value** fields and entering the desired values. The waveform graph also includes viewing tools that are described in Graph Viewing Controls section. | ||
+ | * **Waveform Analysis** (Label 2 in Figure 30): shows the following analysis items for the currently displayed data. | ||
+ | * **Pk-Pk Amplitude: | ||
+ | * **Max Amplitude: | ||
+ | * **Min Amplitude: | ||
+ | * **Mean:** displays the arithmetic mean of the captured data. | ||
+ | * **Standard Deviation: | ||
+ | * **Frequency: | ||
+ | |||
+ | |||
+ | ----------------- | ||
+ | === Histogram Tab View === | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | |||
+ | Figure 31 shows the **Histogram** tab view. The **Histogram** tab is useful for performing statistical analysis of the device conversion results, especially when measuring DC signals. The histogram graph shows the distribution of the conversion results as well as various statistical analysis items. The **Histogram** tab contains the following controls and indicators: | ||
+ | * **Histogram graph** (Label 1 in Figure 31): displays histogram of the most recently captured or loaded conversion results. The scale and range of the histogram graph can be set by double-clicking on the minimum and maximum axis values and entering the desired values. The histogram graph also includes viewing tools, described in Table 5. | ||
+ | * **Histogram Analysis** (Label 2 in Figure 31): shows the following analysis items for the currently displayed data. | ||
+ | * **Max Value:** displays the maximum value measured in the captured data. | ||
+ | * **Min Value:** displays the minimum value measured in the captured data. | ||
+ | * **DC Offset/ | ||
+ | * **Transition Noise:** displays the transition noise of the captured data. | ||
+ | * **Pk-Pk Amplitude: | ||
+ | * **RMS:** displays the measured RMS voltage. | ||
+ | * **LSB:** displays the effective size (in μV) of each LSB given the resolution of the connected device, and the **Voltage Reference (VREF)** and **Oversampling Ratio** values selected in the Configure tab. | ||
+ | * **Histogram Width:** displays the size of the bins in the histogram graph x-axis. | ||
+ | |||
+ | ----------------- | ||
+ | === FFT Tab View === | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | Figure 32 shows the **FFT** tab view. The **FFT** tab displays the calculated FFT representation of the conversions results from the connected device and common AC performance metrics. The **FFT** tab contains the following controls and indicators: | ||
+ | * **FFT graph** (Label 1 in Figure 32): displays an FFT of the most recently captured or loaded conversion results. Set the scale and range of the FFT graph by double clicking on the minimum and maximum values along the x-axis and y-axis and entering the desired values. The FFT graph also includes viewing tools that described in Table 5. | ||
+ | * **FFT Analysis** (Label 2 in Figure 32): displays common ac performance metrics of the captured data. Results are calculated from the FFT spectrum, typically ignoring the first six frequency bins. | ||
+ | * **Max Amplitude: | ||
+ | * **Min Amplitude: | ||
+ | * **Pk-Pk Amplitude: | ||
+ | * **DC:** displays the DC value of the captured data. | ||
+ | * **Fund. Frequency: | ||
+ | * **Fund. Amplitude: | ||
+ | * **Dynamic Range:** displays the calculated dynamic range. | ||
+ | * **RMS:** displays the measured RMS voltage. | ||
+ | * **SNR:** displays the calculated signal-to-noise ratio (SNR). | ||
+ | * **THD:** displays calculated total harmonic distortion (THD), up to the fifth harmonic. | ||
+ | * **SINAD:** displays the calculated single-to-noise and distortion ratio (SINAD). | ||
+ | * **Noise Floor:** displays the average amplitude of noise frequency bins, more specifically, | ||
+ | * **Bin Width:** displays the size of the frequency bins in the FFT graph x-axis. The bin width is a function of both the **Throughput (kSPS)** control (Label 8 in Figure 29) and the number of samples in the captured data. | ||
+ | * **SFDR:** displays the calculated spurious-free dynamic range (SFDR). | ||
+ | * **Show Harmonic Content:** contains Frequency and Amplitude information for the fundamental and harmonic tones identified in the FFT. These displays are only visible when toggled by the Show Harmonic Content control and are not displayed in Figure 32. | ||
+ | * **Frequency: | ||
+ | * **Amplitude: | ||
+ | |||
+ | |||
+ | ----------------- | ||
+ | === Summary Tab View === | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | Figure 33 shows the Summary tab view. The Summary tab simultaneously displays the waveform, histogram, and FFT graphs and analysis for the device conversion results on the screen. The Summary tab contains the following controls and indicators: | ||
+ | * **Waveform graph** (Label 1 in Figure 33): displays the time domain plot of the most recently captured or loaded conversion results. The scale and range of the waveform graph can be set by double-clicking on the minimum and maximum axis values along the x-axis and y-axis and entering the desired values. The waveform graph also includes viewing tools that are described in Graph Viewing Controls section. | ||
+ | * **Histogram graph** (Label 2 in Figure 33): displays the histogram of the most recently captured or loaded conversion results. The scale and range of the histogram graph can be set by double-clicking on the minimum and maximum values along the x-axis and y-axis and entering the desired values. The histogram graph also includes viewing tools that are described in Graph Viewing Controls section. | ||
+ | * **FFT graph** (Label 3 in Figure 33): displays an FFT of the most recently captured or loaded conversion results. The scale and range of the FFT graph can be set by double clicking on the minimum and maximum axis values and entering the desired values. The FFT graph also includes viewing tools that are described in Graph Viewing Controls section. | ||
+ | * **Analysis Summary** (Label 4 in Figure 33): shows the following analysis items for the currently displayed data. | ||
+ | * **Pk-Pk Amp:** displays the peak-to-peak amplitude of the captured data. | ||
+ | * **DC Offset/ | ||
+ | * **Transition Noise:** displays the transition noise of the captured data. | ||
+ | * **Fund. Freq.:** displays frequency identified as the fundamental (the frequency bin with the largest signal). | ||
+ | * **Fund. Amp.:** displays the amplitude of the Fund. Freq. | ||
+ | * **RMS:** displays the measured RMS voltage of the captured data. | ||
+ | * **Dynamic Range:** displays the calculated dynamic range of the captured data. | ||
+ | * **SNR:** displays the calculated SNR of the captured data. | ||
+ | * **THD:** displays the calculated THD of the captured data (up to the fifth harmonic). | ||
+ | * **SINAD:** displays the calculated SINAD of the captured data. | ||
+ | * **LSB:** displays the effective size (in μV) of each LSB. The LSB size is a function of the resolution of the connected device, the Reference Voltage (VREF), and Oversampling Ratio values selected in the Configure tab. | ||
+ | * **SFDR:** displays the calculated SFDR of the captured data. | ||
+ | |||
+ | |||
+ | |||
+ | ----------------- | ||
+ | === Graph Viewing Controls === | ||
+ | The tools described below allow users to control the different chart displays within any of the chart panels in the graphical user interface (GUI) tabs. | ||
+ | |||
+ | ^ Symbol | ||
+ | | {{ : | ||
+ | | {{ : | ||
+ | | {{ : | ||
+ | |||
+ | |||
+ | === Saving and Loading Sessions === | ||
+ | The ADSKPMB10-EV-FMCZ Evaluation Software allows users to save and load data to quickly recall previous results. | ||
+ | Clicking **File > Save Captured Data** or using the shortcut **Ctrl + S** saves the capture data and relevant sampling parameters for the currently displayed device in a .csv file. These saved files can be loaded at a later time by clicking **File > Load Captured Data** or using the shortcut **Ctrl + O**. Upon loading these **.csv** files, the evaluation software displays the data in the **Waveform, Histogram, FFT,** and **Summary** tabs. | ||
+ | |||
+ | The evaluation software also allows the user to export the raw data of any of the graphs into a generic text file by right clicking them and selecting **Export > Export Data to Excel**, as shown in Figure 34. The exported data can be used for additional postprocessing, | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
+ | |||
+ | <WRAP round 80% download> | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | * Schematics | ||
+ | * {{ : | ||
+ | * {{ : | ||
+ | * PCB Layout | ||
+ | * Bill of Materials | ||
+ | * Allegro Project | ||
+ | </ | ||
+ | |||
+ | ===== Troubleshooting ===== | ||
+ | ==== Software ==== | ||
+ | To troubleshoot the software, take the following steps: | ||
+ | - Always install the software before connecting the hardware to the PC. | ||
+ | - Make sure to completely finish the installation (the software is a two-part installation, | ||
+ | - When the user initially plugs in the SDP-H1 via the provided USB cable, allow the Found New Hardware Wizard to run, which can take several seconds. Allow this to happen first before starting the software. | ||
+ | - If the ADSKPMB10-EV-FMCZ or SDP-H1 board are connected to the PC via the USB port, but are not detected by the software, ensure that the board is being recognized in the Device Manager, as shown in Figure 18. | ||
+ | - If connected to a slower USB port where the SDP-H1 cannot read as quickly as it needs to, a timeout error can result. In this case, it is advised not to read continuously, | ||
+ | |||
+ | |||
+ | ==== Hardware ==== | ||
+ | To troubleshoot the hardware, take the following steps: | ||
+ | - If the software does not read back any data, do the following: | ||
+ | * Check that the power is applied within the power ranges described in the Power Supplies section. | ||
+ | * Using a voltmeter, measure the voltage present at each of the test points: P15V, N15V, N1V, 1V8, and 5V5. Note that the LED1 on the SDP-H1 must be lit. | ||
+ | * Launch the software and read the data. If nothing happens, exit the software. | ||
+ | * Power down the board and relaunch the software. | ||
+ | * If no data is read back, confirm that the evaluation board is connected to the SDP-H1, and that the SDP-H1 is being recognized in the Device Manager, as shown in Figure 18. | ||
+ | - When the user is working with the software in standalone/ | ||
+ | |||
+ | |||
+ | |||
+ | |||
+ | ===== Additional Information and Useful Links ===== | ||
+ | |||
+ | |||
+ | * [[adi> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | |||
+ | ===== Software Projects and Platforms ===== | ||
+ | * N/A | ||
+ | |||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ | ||
+ | |||
+ | //End of Document// |