This is an old revision of the document!
The manual consists of:
Thank you for purchasing the EVAL-SDP-CB1Z System Demonstration Platform (SDP) from Analog Devices, Inc. The SDP is used as part of the evaluation system for many ADI components. The SDP board is designed to be used in conjunction with various ADI component evaluation boards as part of a customer evaluation environment. The SDP provides USB connectivity through a USB 2.0 high speed connection to the computer allowing users to evaluate components on this platform from a PC application. The SDP is based on ADSP-BF527 Blackfin processor, with the Blackfin processor peripheral communication lines available to the component daughter board through the two identical 120-pin small footprint connectors
The board features:
For more information, go to The ADI web site.
The SDP User Guide provides instructions for installing the SDP hardware (EVAL-SDP-CB1Z board) and software onto your computer. The necessary installation files are provided with the evaluation daughter board package.
The primary audience for this manual is a system engineer who seeks to understand how to set up the SDP board and begin USB communications to the computer.